metaonly module xdc.tools.Cmdr

Command line tool context

XDCscript usage meta-domain sourced in xdc/tools/Cmdr.xdc
var Cmdr = xdc.useModule('xdc.tools.Cmdr');
module-wide constants & types
    values of type Cmdr.Context// 
        const Cmdr.SHELL;
        const Cmdr.SCRIPT;
per-instance config parameters
    var params = new Cmdr.Params// Instance config-params object;
        params.tid//  = Int 0;
per-instance creation
    var inst = Cmdr.create// Create an instance-object(Any cmdmod, params);
per-instance functions
    inst.getopts// Parse command-line arguments into config params(Any inst, Any args) returns Any
    inst.verbose// Set verbose flag as specified(Any flag) returns Any
 
 
enum Cmdr.Context
XDCscript usage meta-domain
values of type Cmdr.Context
    const Cmdr.SHELL;
    const Cmdr.SCRIPT;
 
Instance Config Parameters

XDCscript usage meta-domain
var params = new Cmdr.Params;
// Instance config-params object
    params.tid = Int 0;
    // 
 
config Cmdr.tid  // instance
XDCscript usage meta-domain
var params = new Cmdr.Params;
  ...
params.tid = Int 0;
 
Instance Creation

XDCscript usage meta-domain
var params = new Cmdr.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = Cmdr.create(Any cmdmod, params);
// Create an instance-object
 
Cmdr.error()  // instance

Throw an error exception with the specified message

XDCscript usage meta-domain
inst.error(Any msg) returns Any
 
DETAILS
If msg is null or the empty string (""), the message "fatal error" is used.
 
Cmdr.getopts()  // instance

Parse command-line arguments into config params

XDCscript usage meta-domain
inst.getopts(Any inst, Any args) returns Any
 
ARGUMENTS
inst — instance with config parameters to set
args — an array of command-line arguments
DETAILS
This function accepts an array of command-line arguments, and uses them to set the values of config parameters in a module instance. Parsing is controlled by the XDC declarations of the instance config params.
USAGE
The following command-line argument syntaxes are supported, following the syntax supported by GNU getopt() and getopt_long():
    -f                a boolean flag with short name
    -f value          a number or string with short name
    -fvalue
    -f=value
    --longname        a boolean flag with long name
    --longname value  a number or string with long name
    --longname=value  a number or string with long name
In addition the following non-standard syntaxes are supported:
    -f:value
    --longnamevalue
    --longname:value
DECLARATION
The long and short names of the config parameter are declared by the @CommandOption() attribute of the XDC spec language. For example to declare a boolean flag with a short name of "-f" and a long name of "--flag", and a default value of false:
     @ CommandOption("f,flag")
     config Bool myFlag = false;
Options of type Bool with no argument are assigned the value "true". The types String and Int can also be used, and always require an argument to be given on the command line.
COMBINING SHORT FLAGS
Short-name options can be combined on the command line where there is no ambiguity, for example the following usages are equivalent:
    -a -b -c -f filename
    -abcf filename
MULTIPLE OCCURRENCES
If the config param is declared as an array, the option may be used multiple times on the command line and each occurence will be recorded. For example the following records all -I options, in order:
    @ CommandOption("I")
    config String includeDirs[] = [];
REQUIRED OPTIONS
If the config param has no default value declared, then it is required on the command line.
RETURNS
The following return values are used to determine whether or not to proceed with the command and, if not, what the exit status of the command should be.
undefined
the command options have been successfully parsed and the command should be run.
0 (zero)
the command options have been successfully parsed and the command does not need to be run and should exit with a successful exit status (0).
non-zero integral value
an error occured in the parsing the options and the command should not be run and should exit with a non-zero exit status.
 
Cmdr.info()  // instance

Output informational message to stdout

XDCscript usage meta-domain
inst.info(Any msg) returns Any
 
 
Cmdr.time()  // instance

Output elapsed time since command start to stderr

XDCscript usage meta-domain
inst.time(Any msg) returns Any
 
 
Cmdr.usage()  // instance

Output command usage message to stderr

XDCscript usage meta-domain
inst.usage(Any msg) returns Any
 
DETAILS
If msg is defined and non-empty, the command name and msg are output before the usage information.
 
Cmdr.verbose()  // instance

Set verbose flag as specified

XDCscript usage meta-domain
inst.verbose(Any flag) returns Any
 
 
Cmdr.warning()  // instance

Output specified warning message to stderr

XDCscript usage meta-domain
inst.warning(Any msg) returns Any
 
generated on Thu, 16 Jun 2011 22:53:00 GMT