typedef SysUart_GetLineFxn |
![](../../../../Arrow_up.png) |
Input a single line
typedef Void (*SysUart_GetLineFxn)(Char[],Int);
config SysUart_getLineFxn // module-wide |
![](../../../../Arrow_up.png) |
User suplied character input function
DETAILS
If this parameter is set to a non-null value, the specified
function will be called to input a line of chars received by
SysUart.
For example, if you define a function named myGetLineFxn, the
following configuration fragment will cause SysUart to call
myGetLineFxn whenever a line is received.
var SysUart = xdc.useModule("xdc.runtime.SysUart");
SysUart.getLineFxn = "&myGetLineFxn";
If this parameter is not set, a default function will be used which
simply drops the input.
SEE
config SysUart_lineSize // module-wide |
![](../../../../Arrow_up.png) |
The maximum line buffer size
extern const Int SysUart_lineSize;
DETAILS
The maximum number of characters to buffer before calling
getLineFxn. If set to zero, no buffering occurs and each
character received triggers getLineFxn (if it's defined).
SysUart_abort() // module-wide |
![](../../../../Arrow_up.png) |
Backend for System.abort()
Void SysUart_abort(String str);
ARGUMENTS
str
message to output just prior to aborting
If non-NULL, this string should be output just prior to
terminating.
DETAILS
This function is called by
System.abort() prior to calling
the ANSI C Standard library function
abort(). So, to ensure the
abort processing of the system's ANSI C Standard library completes,
this function should return to its caller.
SysUart_exit() // module-wide |
![](../../../../Arrow_up.png) |
Backend for System.exit()
Void SysUart_exit(Int stat);
ARGUMENTS
stat
status value passed to all "atexit" handlers
This value is passed to all "atexit" handles bound via
System.atexit(). If the application exits via the
ANSI C Standard
exit() function rather than via System_exit(),
stat will be equal to
System.STATUS_UNKNOWN.
DETAILS
This function is called as part the normal "atexit" processing
performed by the ANSI C Standard Library's
exit() function;
System.exit() directly calls ANSI
exit().
This function is called after all "atexit" handlers bound via
System.atexit() are run and it
is always called while "inside" the the
System gate.
To ensure that all exit processing of the system's ANSI C
Standard Library completes, this function should return to its caller.
Exit handlers bound using the ANSI C Standard Library atexit()
function may run before or after this function.
SEE
SysUart_flush() // module-wide |
![](../../../../Arrow_up.png) |
Backend for System.flush()
DETAILS
This function is simply called by
System_flush
to output any characters buffered by the underlying
SystemSupport
module to an output device.
SysUart_putch() // module-wide |
![](../../../../Arrow_up.png) |
Backend for System.printf() and System.putch()
Void SysUart_putch(Char ch);
ARGUMENTS
ch
character to output
DETAILS
Output a single character. This function is called by
System_printf() to write each character
of formated output specified by its arguments.
SysUart_ready() // module-wide |
![](../../../../Arrow_up.png) |
Test if character output can proceed
DETAILS
This function is called by
System prior to performing
any character output. If this function returns
FALSE, the
System
functions that would normally call
putch() simply return
(with an appropriate error status) without ever calling
putch.
Module-Wide Built-Ins |
![](../../../../Arrow_up.png) |
// Get this module's unique id
Bool SysUart_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SysUart_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SysUart_Module_getMask();
// Returns the diagnostics mask for this module
Void SysUart_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module