module ti.mcu.msp430.runtime.GateGIE

Global interrupt disable/enable implementation of IGateProvider

Instances of this gate implementation disable all interrupts and should only be used for modules in which the data structures protected by module-level gates are held for fixed short durations.
C synopsis target-domain sourced in ti/mcu/msp430/runtime/GateGIE.xdc
#include <ti/mcu/msp430/runtime/GateGIE.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
IArg 
Void 
Bool 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef GateGIE_Object *
typedef struct
typedef struct
typedef struct
 
 
const GateGIE_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GateGIE_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GateGIE_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GateGIE_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
GateGIE_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GateGIE_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GateGIE_Module_id();
// Get this module's unique id
 
Bool GateGIE_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GateGIE_Module_heap();
// The heap from which this module allocates memory
 
Bool GateGIE_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GateGIE_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GateGIE_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GateGIE_Object GateGIE_Object;
// Opaque internal representation of an instance object
 
typedef GateGIE_Object *GateGIE_Handle;
// Client reference to an instance object
 
typedef struct GateGIE_Struct GateGIE_Struct;
// Opaque client structure large enough to hold an instance object
 
GateGIE_Handle GateGIE_handle(GateGIE_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GateGIE_Struct *GateGIE_struct(GateGIE_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GateGIE_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} GateGIE_Params;
 
Void GateGIE_Params_init(GateGIE_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
Instance Creation

C synopsis target-domain
GateGIE_Handle GateGIE_create(const GateGIE_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GateGIE_construct(GateGIE_Struct *structP, const GateGIE_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion

C synopsis target-domain
Void GateGIE_delete(GateGIE_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GateGIE_destruct(GateGIE_Struct *structP);
// Finalize the instance object inside the provided structure
 
GateGIE_enter()  // instance

Enter this gate

C synopsis target-domain
IArg GateGIE_enter(GateGIE_Handle handle);
 
ARGUMENTS
handle — handle of a previously-created GateGIE instance object
DETAILS
Each gate provider can implement mutual exclusion using different algorithms; e.g., disabling all scheduling, disabling the scheduling of all threads below a specified "priority level", suspending the caller when the gate has been entered by another thread and re-enabling it when the the other thread leaves the gate. However, in all cases, after this method returns that caller has exclusive access to the data protected by this gate.
A thread may reenter a gate without blocking or failing.
RETURNS
Returns a "key" that is used to leave this gate; this value is used to restore thread preemption to the state that existed just prior to entering this gate.
 
GateGIE_leave()  // instance

Leave this gate

C synopsis target-domain
Void GateGIE_leave(GateGIE_Handle handle, IArg key);
 
ARGUMENTS
handle — handle of a previously-created GateGIE instance object
key — the value returned by a matching call to enter
DETAILS
This method is only called by threads that have previously entered this gate via enter. After this method returns, the caller must not access the data structure protected by this gate (unless the caller has entered the gate more than once and other calls to leave remain to balance the number of previous calls to enter).
Instance Convertors

C synopsis target-domain
IGateProvider_Handle GateGIE_Handle_upCast(GateGIE_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GateGIE_Handle GateGIE_Handle_downCast(IGateProvider_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GateGIE_Object_count();
// The number of statically-created instance objects
 
GateGIE_Handle GateGIE_Object_get(GateGIE_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GateGIE_Handle GateGIE_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GateGIE_Handle GateGIE_Object_next(GateGIE_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GateGIE_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GateGIE_Handle_label(GateGIE_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GateGIE_Handle_name(GateGIE_Handle handle);
// The name of this instance object
 
XDCscript usage meta-domain sourced in ti/mcu/msp430/runtime/GateGIE.xdc
var GateGIE = xdc.useModule('ti.mcu.msp430.runtime.GateGIE');
module-wide constants & types
module-wide config parameters
module-wide functions
per-instance config parameters
    var params = new GateGIE.Params// Instance config-params object;
per-instance creation
    var inst = GateGIE.create// Create an instance-object(params);
 
 
const GateGIE.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const GateGIE.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GateGIE.Q_PREEMPTING

Preempting quality

XDCscript usage meta-domain
const GateGIE.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
metaonly config GateGIE.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
GateGIE.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GateGIE.queryMeta()  // module-wide

Configuration time test for a particular gate quality

XDCscript usage meta-domain
GateGIE.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
Instance Config Parameters

XDCscript usage meta-domain
var params = new GateGIE.Params;
// Instance config-params object
Instance Creation

XDCscript usage meta-domain
var params = new GateGIE.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GateGIE.create(params);
// Create an instance-object
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
generated on Mon, 02 May 2011 23:06:49 GMT