metaonly module ti.catalog.msp430.peripherals.interrupt.Interrupt_Controller |
![](../../../../../Arrow_up.png) |
MSP430 Interrupt_Controller
var Interrupt_Controller = xdc.useModule('ti.catalog.msp430.peripherals.interrupt.Interrupt_Controller');
module-wide functions
per-instance config parameters
Interrupt_Controller.addPeripheralsMap() // module-wide |
![](../../../../../Arrow_up.png) |
Create a map of all peripherals available on a device
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
The config parameter
peripherals is by default undefined in an
xdc.platform.ICpuDataSheet instance. This function gathers
all instance configuration parameters that are of the type
xdc.platform.IPeripheral into the map
peripherals.
Interrupt_Controller.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
XDCscript usage |
meta-domain |
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
Interrupt_Controller.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
XDCscript usage |
meta-domain |
Interrupt_Controller.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Interrupt_Controller.Params;
// Instance config-params object
params.baseAddr = UInt undefined;
//
params.name = String undefined;
// Specific peripheral name given by the device
params.numInterrupts = UInt undefined;
//
params.owner = String undefined;
// String specifying the entity that manages the peripheral
config Interrupt_Controller.baseAddr // instance |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Interrupt_Controller.Params;
...
params.baseAddr = UInt undefined;
config Interrupt_Controller.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
XDCscript usage |
meta-domain |
var params = new Interrupt_Controller.Params;
...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config Interrupt_Controller.numInterrupts // instance |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Interrupt_Controller.Params;
...
params.numInterrupts = UInt undefined;
config Interrupt_Controller.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
XDCscript usage |
meta-domain |
var params = new Interrupt_Controller.Params;
...
params.owner = String undefined;
generated on Tue, 01 Feb 2011 01:40:40 GMT