metaonly module ti.catalog.msp430.peripherals.special_function.IE1

MSP430 Interrupt Enable Register 1

XDCscript usage meta-domain sourced in ti/catalog/msp430/peripherals/special_function/IE1.xdc
var IE1 = xdc.useModule('ti.catalog.msp430.peripherals.special_function.IE1');
module-wide constants & types
    values of type IE1.NMIE_t// 
        const IE1.NMIE_OFF;
        const IE1.NMIE;
    values of type IE1.OFIE_t// 
        const IE1.OFIE_OFF// Interrupt not enabled;
        const IE1.OFIE// Interrupt enabled;
    values of type IE1.WDTIE_t// 
        const IE1.WDTIE_OFF;
        const IE1.WDTIE;
        obj.register = String  ...
        obj.regForceSet = Bool  ...
    var obj = new IE1.IE1_t// ;
        obj.NMIE = IE1.NMIE_t  ...
        obj.OFIE = IE1.OFIE_t  ...
        obj.WDTIE = IE1.WDTIE_t  ...
module-wide functions
per-instance config parameters
    var params = new IE1.Params// Instance config-params object;
        NMIE: IE1.NMIE_OFF,
        OFIE: IE1.OFIE_OFF,
        WDTIE: IE1.WDTIE_OFF
    };
        {
            register: "IE1",
            regForceSet: false
        }
    ];
        params.name// Specific peripheral name given by the device = String undefined;
        params.owner// String specifying the entity that manages the peripheral = String undefined;
per-instance functions
    inst.getNMIE// Gets NMIE bit() returns Bool
    inst.getOFIE// Gets OFIE bit() returns Bool
    inst.getWDTIE// Gets WDTIE bit() returns Bool
    inst.setNMIE// Sets NMIE bit(Bool set) returns Bool
    inst.setOFIE// Sets OFIE bit(Bool set) returns Bool
    inst.setWDTIE// Sets WDTIE bit(Bool set) returns Bool
 
enum IE1.NMIE_t
XDCscript usage meta-domain
values of type IE1.NMIE_t
    const IE1.NMIE_OFF;
    const IE1.NMIE;
enum IE1.OFIE_t
XDCscript usage meta-domain
values of type IE1.OFIE_t
    const IE1.OFIE_OFF;
    // Interrupt not enabled
    const IE1.OFIE;
    // Interrupt enabled
enum IE1.WDTIE_t
XDCscript usage meta-domain
values of type IE1.WDTIE_t
    const IE1.WDTIE_OFF;
    const IE1.WDTIE;
struct IE1.ForceSetDefaultRegister_t

Force Set Default Register

XDCscript usage meta-domain
var obj = new IE1.ForceSetDefaultRegister_t;
 
    obj.register = String  ...
    obj.regForceSet = Bool  ...
DETAILS
Type to store if each register needs to be forced initialized even if the register is in default state.
SEE
struct IE1.IE1_t
XDCscript usage meta-domain
var obj = new IE1.IE1_t;
 
    obj.NMIE = IE1.NMIE_t  ...
    obj.OFIE = IE1.OFIE_t  ...
    obj.WDTIE = IE1.WDTIE_t  ...
IE1.addPeripheralsMap()  // module-wide

Create a map of all peripherals available on a device

XDCscript usage meta-domain
IE1.addPeripheralsMap(ICpuDataSheet.Instance cds) returns Void
ARGUMENTS
cds — an xdc.platform.ICpuDataSheet instance
DETAILS
The config parameter peripherals is by default undefined in an xdc.platform.ICpuDataSheet instance. This function gathers all instance configuration parameters that are of the type xdc.platform.IPeripheral into the map peripherals.
IE1.getAll()  // module-wide

Find all peripherals of a certain type

XDCscript usage meta-domain
IE1.getAll() returns IPeripheral.Instance[]
DETAILS
The type of the peripherals returned is defined by the type of the caller.
RETURNS
Returns an array of IPeripheral instances
IE1.getRegisters()  // module-wide

Find all registers defined by the peripheral

XDCscript usage meta-domain
IE1.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters

XDCscript usage meta-domain
var params = new IE1.Params;
// Instance config-params object
    params.IE1 = IE1.IE1_t {
    // IE1, Interrupt Enable Register 1
    NMIE: IE1.NMIE_OFF,
    OFIE: IE1.OFIE_OFF,
    WDTIE: IE1.WDTIE_OFF
};
    params.forceSetDefaultRegister = IE1.ForceSetDefaultRegister_t[] [
    // Determine if each Register needs to be forced set or not
    {
        register: "IE1",
        regForceSet: false
    }
];
    params.name = String undefined;
    // Specific peripheral name given by the device
    params.owner = String undefined;
    // String specifying the entity that manages the peripheral
config IE1.IE1  // instance

IE1, Interrupt Enable Register 1

XDCscript usage meta-domain
var params = new IE1.Params;
  ...
params.IE1 = IE1.IE1_t {
    NMIE: IE1.NMIE_OFF,
    OFIE: IE1.OFIE_OFF,
    WDTIE: IE1.WDTIE_OFF
};
config IE1.forceSetDefaultRegister  // instance

Determine if each Register needs to be forced set or not

XDCscript usage meta-domain
var params = new IE1.Params;
  ...
const params.forceSetDefaultRegister = IE1.ForceSetDefaultRegister_t[] [
    {
        register: "IE1",
        regForceSet: false
    }
];
config IE1.name  // instance

Specific peripheral name given by the device

XDCscript usage meta-domain
var params = new IE1.Params;
  ...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such cases, device data sheets give different names to the instances of a same peripheral. For example, the name for a timer module could be TimerA3, and a device that has two such timers can name them TA0 and TA1.
config IE1.owner  // instance

String specifying the entity that manages the peripheral

XDCscript usage meta-domain
var params = new IE1.Params;
  ...
params.owner = String undefined;
IE1.getNMIE()  // instance

Gets NMIE bit

XDCscript usage meta-domain
inst.getNMIE() returns Bool
SEE
IE1.getOFIE()  // instance

Gets OFIE bit

XDCscript usage meta-domain
inst.getOFIE() returns Bool
SEE
IE1.getWDTIE()  // instance

Gets WDTIE bit

XDCscript usage meta-domain
inst.getWDTIE() returns Bool
SEE
IE1.setNMIE()  // instance

Sets NMIE bit

XDCscript usage meta-domain
inst.setNMIE(Bool set) returns Bool
SEE
IE1.setOFIE()  // instance

Sets OFIE bit

XDCscript usage meta-domain
inst.setOFIE(Bool set) returns Bool
SEE
IE1.setWDTIE()  // instance

Sets WDTIE bit

XDCscript usage meta-domain
inst.setWDTIE(Bool set) returns Bool
SEE
generated on Tue, 18 Jan 2011 00:04:40 GMT