Utils.assembleMemoryMap() // module-wide |
|
Combine the device and the external memory map into a platform map
XDCscript usage |
meta-domain |
Utils.assembleMemoryMap(Any cpu, Any plat, Any noCheck) returns Any
ARGUMENTS
cpu
an xdc.platform.IExeContext object
plat
a platform instance
noCheck
if true, and a custom memory map is defined, the
function does not check if the custom memory map fits
into the available physical memory
DETAILS
This function combines memory maps and also applies memory map name
changes requested through renameMap.
RETURNS
platform memory map
Utils.checkDefaults() // module-wide |
|
Check if dataMemory, codeMemory and stackMemory are set correctly
XDCscript usage |
meta-domain |
Utils.checkDefaults(Any inst, Any memMap) returns Any
ARGUMENTS
inst
an xdc.platform.IPlatform instance
memMap
a map of xdc.platform.IPlatform.Memory objects
DETAILS
The xdc.platform.IPlatform instance parameters 'dataMemory',
'codeMemory', and 'stackMemory' are strings. This function verifies
that those strings correspond to names of the memory objects in the
supplied memory map.
RETURNS
'true' if checked parameters are valid, 'false'
otherwise
Utils.checkFit() // module-wide |
|
Check if a memory map fits into available physical memory
XDCscript usage |
meta-domain |
Utils.checkFit(Any realMemMap, Any customMemMap) returns Any
ARGUMENTS
realMemMap
a map of xdc.platform.IPlatform.Memory
objects containing physical memory map as
defined in datasheets for the device and the
platform
customMemMap
a map of xdc.platform.IPlatform.Memory
objects containing user defined memory map,
which must fit within boundaries of 'realMemMap'
DETAILS
A custom memory map segment can be spread over multiple physical
memories or multiple custom memory map segments can be located in
one physical memory. However, code/data restrictions must be followed.
A custom memory segment with the parameter 'space' set to "code/data",
which is the default value if the parameter was not specified, can fit
only into "code/data" physical memories. Custom memory segments with
'space' set to "code" can fit into "code" and "code/data" memories, and
custom memory segments with 'space' set to "data" can fit into "data"
and "code/data" physical memories.
RETURNS
'true', if customMemMap fits within realMemMap,
and 'false' otherwise
Utils.checkOverlap() // module-wide |
|
Check if there is an overlap among memory objects in a memory map
XDCscript usage |
meta-domain |
Utils.checkOverlap(Any memMap) returns Any
ARGUMENTS
memMap
a map of xdc.platform.IPlatform.Memory objects
RETURNS
a string with names of Memory objects that overlap
Utils.getCpuDataSheet() // module-wide |
|
Get the specified cpu data sheet object
XDCscript usage |
meta-domain |
Utils.getCpuDataSheet(Any cpuDesc) returns Any
ARGUMENTS
cpuDesc
an xdc.platform.IExeContext.Cpu object identifying
the CPU device
RETURNS
an xdc.platform.ICpuDataSheet.Instance object that
corresponds to the specified cpuDesc
THROWS
Error exceptions are thrown for fatal errors