struct Executable.Attrs |
![](../../Arrow_up.png) |
Optional attributes for an Executable instance
XDCscript usage |
meta-domain |
var obj = new Executable.Attrs;
obj.profile = String ...
// target options profile
obj.aopts = String ...
// asm options for objs added to this exe
obj.copts = String ...
// C/C++ options for objs added to this exe
obj.cfgcopts = String ...
// C/C++ options for the C config file
obj.defs = String ...
// definitions for objs added to this exe
obj.incs = String ...
// include opts for objs added to this exe
obj.lopts = String ...
// linker options for this exe
obj.tcopts = String ...
// tconf options for this exe
obj.xsopts = String ...
// xs options for this exe
obj.cpuId = String ...
// optional id of CPU on platform
obj.rtsName = String ...
// optional run time support package name
obj.cpuArgs = Any ...
// optional register settings
obj.cfgScript = String ...
// optional name of config script
obj.cfgHome = String ...
// optional home package of config model
obj.cfgArgs = String ...
// optional arguments passed to cfgScript
obj.cfgArgsEncoded = Bool ...
// if true, cfgArgs is encoded via escape()
obj.exportExe = Bool ...
// export executable's exe file?
obj.exportCfg = Bool ...
// export executable's config script?
obj.exportSrc = Bool ...
// if true, export exe sources to releases
// releases that this exe is a part of
// test attrs for tests added to this exe
obj.linkTemplate = String ...
// linker command file template for this exe
obj.isRom = Bool ...
// if true, exe is a ROMable sub-assembly
FIELDS
cfgArgs
This string may contain any expression that can be
assigned to a JavaScript property. It is evaluated in
the configuration domain after the platform package is
imported and just prior to running the executable's
configuration script. Its value (after evaluation) is
assigned to Program.build.cfgArgs; so, program
configuration scripts can use this property to adjust their
behavior based on values specified in a build script.
For example, a package's build script might build an
executable for each possible level of a "trace" value:
for (t = 0; t < NUM_TRACE_LEVELS; t++) {
:
Pkg.addExecutable("myExe" + t, targ, plat, {
cfgArgs: "{traceLevel: " + t + "}",
cfgScript: "myExe.cfg"
});
}
In this case, the configuration script myExe.cfg can
reference the "trace level" set in the build script by
referencing the Program.build.cfgArgs object directly:
if (Program.build.cfgArgs.traceLevel == 1) {
:
}
cfgArgsEncoded
This boolean flag indicates whether the
string cfgArgs should be treated as an encoded string (via ECMA-262
escape()) or not. If this field is true, the string is treated
as an encoded string and is decoded via unescape() prior to
interpretation.
incs
This string contains include path options used by
the compiler (or assembler) to locate include files; e.g.,
"-I ../../include -I ../c55xx". Note that the syntax of
this string may be target dependent.
defs
This string contains options used by the
compiler (or assembler) to define macros; e.g.,
"-D_C6xxx -DDEBUG=1". Note that the syntax of
this string may be target dependent.
aopts
This string contains options used by the assembler
to produce object files; e.g., "-mP1". Note that the syntax
of this string may be target dependent.
copts
This string contains options used by the C/C++
compiler to produce object files; e.g., "-o3 -mi1". Note
that the syntax of this string may be target dependent.
cfgcopts
This string contains options used by the C/C++
compiler to compile the generated C config file. If cfgopts
is not specified, either explicitly or through
Pkg.attrs.cfgcopts, the options specified in copts are
used instead.
lopts
This string contains options used by the linker
produce object files; e.g., "-l mylib.lib". Note
that the syntax of this string may be target dependent.
tcopts
This string contains options passed to tconf.
Deprecated, use xsopts instead.
xsopts
This string contains options passed to xs
when running configuration scripts; e.g., to turn on the
reporting of warnings this string can be set to "-js -w",
or to define the name-value pair "FOO=bar" available via
the environment hash-table xsopts should be set to
"-DFOO=bar".
cfgHome
This string names the package that is bound to
the Configuration Model's $homepkg. This home package
is automatically loaded as part of configuration and, as
a result, may contribute libraries to the configuration.
If this parameter is not specified, the package containing
the configuration script is used as the home package. This
ensures that the results of a configuration script are
independent of the package building the configuration. In
most cases, the build package is the package containing the
configuration script and this distinction is not important.
But there are times when it is important to control the home
package; e.g., when an external tool generates a
configuration script from information supplied by another
package or when a configuration script in not in any package.
cfgScript
This string names the program configuration
script used to create the files necessary to create the
executable. If cfgScript is not specified, the configuration
script is assumed to be <name>.cfg, where <name> is the
base name of the executable. If cfgScript is set to null,
the executable is assumed to be a "legacy" application that
defines main() directly and does not require any
xdc.runtime support.
If this string is set to a non-null value, and does not have
an extension, then the extension ".cfg" is automatically
added.
If the specified configuration file does not exist in the
package where the executable is being built and
the name does not begin with "./", it is searched
for along the package path. Thus, it is possible to use
configuration scripts in other packages to build executables;
e.g., to use the configuration script "myExe.cfg" from a
ti.bios.examples.hello package, cfgScript should be set
to "ti/bios/examples/hello/myExe.cfg".
The package containing the specified configuration script is
imported prior to running the configuration script and this
package is used to set xdc.$homepkg; thus, configuration
scripts that use xdc.$homepkg will configure the same
executable independent of the package building the executable.
profile
This string names a profile defined by the
executable's target. The profile specifies a set of compiler,
linker, and archiver options that are to be used when
producing the executable. Note that these tool options are
in addition to any options specified via aopts, copts,
etc.
If this field is not set or set to
null, the value of
xdc.bld.PackageContents.attrs.profile is used. If
xdc.bld.PackageContents.attrs.profile is not
specified or equal to
null, the
"release" profile is used.
cpuId
This string is used to uniquely identify the
particular CPU on a platform that will run the executable; on
platforms that contain a single CPU, this string is ignored.
rtsName
This string names a RunTime Support (RTS) package that
will be implicitly loaded prior to running the executable's
configuration script. If this field is set to null, then
no RTS package will be loaded. If this field is not set (or
set to undefined), the RTS package specified by this
executable's target will be used (see
xdc.bld.ITarget.rts) .
cpuArgs
This field is a hash-table of name-value pairs
interpreted by the CPU as register settings that exist at the
time that the executable is loaded; e.g., it is possible to
specify a non-reset value for the PMST register on a C54xx
CPU by setting this parameter to {PMST: 0xffff}.
exportCfg
If this field is set to true, the configuration
script will be part of the releases named in the releases
array. If it is unspecified (or set to null) and the
release specifies that configurations are to be exported,
the configuration script will be part of the release. In
all other cases, the configuration is not part of the
release.
exportSrc
If this field is set to true, the sources
specified via xdc.bld.Executable.addObjects()
will be part of the releases named in the releases
array. If it is unspecified (or set to null) and the
release specifies that sources are to be exported,
the sources will be part of the release. In
all other cases, the sources are not added to the
release.
exportExe
If this field is set to true, the executable
will be part of the releases named in the releases
array. If it is unspecified (or set to null) and the
release specifies that configurations are to be exported,
the executable will be part of the release. In
all other cases, the executable is not part of the
release.
releases
This array contains releases that will contain the
executable. Thus, a single executable can be part of any set
of releases. Each executable is always added to the
package's "default release" in addition to any releases
specified in the releases array.
linkTemplate
If this field is set, it defines the linker
command file template to be used to link this executable.
This specification may, however, be overridden by the
configuration script (see
xdc.cfg.Program.linkTemplate).
As with configuration scripts, if the specified file does not
exist in the package where the executable is being built and
the name does not begin with "./", it is searched for along
the package path. Thus, it is possible to use templates in
other packages to build executables; e.g., to use the linker
command file "myExe.cmd" from the ti.bios.examples.hello
package, linkTemplate should be set to
"ti/bios/examples/hello/myExe.cmd".
DETAILS
Unspecified attributes are "inherited" from
xdc.bld.PackageContents.attrs;
i.e., if one of fields in this structure is unspecified *and* this
field's name matches a field name in
xdc.bld.PackageContents.attrs, then this field's value
defaults to the value in specified by
xdc.bld.PackageContents.attrs. This mechanism makes it
possible to establish package-wide default values for any of the
"inherited" attributes.
Suppose, for example, that you want all executable files in this
package to be built with the 'release' profile, but one particular file
must be built with 'debug' (because it is a source example). The
following build script fragment shows how this can be accomplished:
Pkg.attrs.profile = 'release';
var exe = Pkg.addExecutable('example', ..., {profile: 'debug'});
SEE
Instance Config Parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Executable.Params;
// Instance config-params object
// This executable's optional attributes
params.name = String undefined;
// Base name of the executable
params.platform = String undefined;
// The name of the platform that will run this executable
// The target (on a platform) that executable should be built for
config Executable.attrs // instance |
![](../../Arrow_up.png) |
This executable's optional attributes
XDCscript usage |
meta-domain |
var params = new Executable.Params;
...
DETAILS
These attributes are "inherited" by all objects added to this
executable; i.e., any object attribute that is undefined but is
defined here will be assigned the value from these attributes.
Similarly, any unspecified attributes that also appear in
xdc.bld.PackageContents.Attrs are inherited from
xdc.bld.PackageContents.attrs.
SEE
config Executable.name // instance |
![](../../Arrow_up.png) |
Base name of the executable
XDCscript usage |
meta-domain |
var params = new Executable.Params;
...
params.name = String undefined;
DETAILS
This name is used to construct the final executable file name as
follows:
where
<name> is name and
<target_suffix> is the suffix defined
by each target that the file is built for. See NOTE in
xdc.bld for filename rules.
Note: if the same executable is to be built for different platforms
(having the same target), then name must "encode" the platform's
name.
config Executable.platform // instance |
![](../../Arrow_up.png) |
The name of the platform that will run this executable
XDCscript usage |
meta-domain |
var params = new Executable.Params;
...
params.platform = String undefined;
DETAILS
Platforms are modeled as packages that have a module called
"Platform"; thus the platform name is really a package name.
config Executable.target // instance |
![](../../Arrow_up.png) |
The target (on a platform) that executable should be built for
XDCscript usage |
meta-domain |
var params = new Executable.Params;
...
DETAILS
This parameter is used to determine the target to use for any
objects added to the executable.
During configuration, the executable's platform package can
validate that the target is compatible with the configuration of
the platform; the target object is accessible via the expression
Program.build.target.
Executable.addObjects() // instance |
![](../../Arrow_up.png) |
Add specified object to be built and linked into this executable
XDCscript usage |
meta-domain |
inst.
addObjects(
String[] names,
Object.Attrs objAttrs)
returns Void
ARGUMENTS
names
array of base names of the sources of object files
to be created and linked into the executable.
See NOTE in xdc.bld for filename rules.
objAttrs
optional xdc.bld.Object.Attrs for the
array of objects added; all objects named by names
will be given the attributes objAttrs.
DETAILS
All objects added to the executable are built with the symbol
xdc_cfg__header__ defined to be the name of the executable-specific
C header generated by the program configuration tool. This symbol
is used by the
xdc/cfg/global.h header to include the generated
header file; see
xdc.cfg.Program.global. Thus, it is
possible to portably include configuration specific definitions in a
source file that is used in many different configurations.
For example, a portable main.c might be structured as follows:
#include <xdc/std.h>
#include <ti/bios/include/log.h>
#include <xdc/cfg/global.h> // include declaration of trace
int main(int argc, char *argv[])
{
LOG_printf(trace, "hello world");
:
}
EXAMPLES
1. Locate a source file whose name starts with "hello" with
an extension supported by the executable's target, compile it
and link it into the executable myExe:
myExe.addObjects(["hello"]);
If hello.c exists, compile and add to myExe, if hello.asm exists
assemble and add to myExe, etc. If no such file is located,
a warning is emitted.
2. Compile hello.c and add to the executable myExe:
myExe.addObjects(["hello.c"]);
3. Names may include sub-directory prefixes. In this case, the
source will be located in a sub-directory of the current
package. The following statement declares that the file
"foo/hello.c" should be compiled and linked into the executable
myExe:
myExe.addObjects(["foo/hello.c"]);
As in the previous examples, the extension ".c" is optional.
In case an extension is not supplied, each extension
understood by the target will be tried until a source file
is located.
4. It is also possible to supply file specific compilation
options.
myExe.addObjects(["fir.c", "iir.c"], {defs: "-D_DEBUG"});
In this case, both files fir.c and iir.c will be compiled
with the "-D_DEBUG" flag. Any setting of attrs.defs in the
executable or package is overridden by this definition.
RETURNS
void
THROWS
Error exceptions are thrown for fatal errors
SEE
Executable.addTest() // instance |
![](../../Arrow_up.png) |
Add specified test to executable
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
A test encapsulates an executable and a set of arguments passed to
the executable when it is run.
Tests are run by naming the goal "<test_name>.test" on the xdc
command line; <test_name> is the test's name.
Multiple tests may have the same name; in this case, it is possible
to run all tests using the single goal "<test_name>.test"
RETURNS
the
xdc.bld.Test instance object created
THROWS
Error exceptions are thrown for fatal errors