struct IPackage.BuildAttrs |
![](../Arrow_up.png) |
Package-level attributes from the Build Object Model (BOM)
metaonly struct BuildAttrs {
String libraries[];
// array of archive names produced by this pkg
// desriptors for elements in libraries
Any getLibs;
// getLibs function defined by build script
};
FIELDS
getLibs
the JavaScript function that should be used when
the package participates in a program configuration
script. This field contains the function specified
by a package's build script
libraries
an array of archive names created by this package.
Each name is a package-relative file name of an
archive within the package.
libDesc
a map of library descriptors. This map is indexed
by names that appear in the libraries array.
DETAILS
This structure defines a set of package-level attributes that are
carried forward from the Build Model into the Configuration Model.
struct IPackage.LibDesc |
![](../Arrow_up.png) |
Library properties from the Build Object Model (BOM)
metaonly struct LibDesc {
String target;
// target name
String suffix;
// suffix property of the named target
};
FIELDS
target
target for which the library was built.
suffix
the suffix associated with the named target.
DETAILS
This structure defines library properties that are
carried forward from the Build Model into the Configuration Model.
config IPackage.build // module-wide |
![](../Arrow_up.png) |
The package information from the Build Object Model (BOM)
READONLY
This parameter is set when the package is first loaded
and should not be modified by any other script.
config IPackage.packageBase // module-wide |
![](../Arrow_up.png) |
The absolute path to the package's "base" directory
config String packageBase;
DETAILS
This parameter contains an absolute path to the directory
containing the package's build script (package.bld). For example,
if the package ti.bios is located in c:/packages/ti/bios, then
packageBase equals c:/packages/ti/bios/.
To be robust, clients should not assume that this string ends with a
directory separator.
READONLY
This parameter is set when the package is first loaded
and should not be modified by any other script.
config IPackage.packageRepository // module-wide |
![](../Arrow_up.png) |
The absolute path to the repository containing the package
config String packageRepository;
DETAILS
This parameter contains an absolute path to the directory
containing the full directory namespace of the package. For
example, if the package ti.bios is located in c:/packages/ti/bios,
then packageRepository equals c:/packages/.
To be robust, clients should not assume that this string ends with a
directory separator.
READONLY
This parameter is set when the package is first loaded
and should not be modified by any other script.
config IPackage.profile // module-wide |
![](../Arrow_up.png) |
The profile requested by a configuration script
DETAILS
This parameter is set by configuration scripts to convey additional
information to the package about the libraries being requested from
this package; in particular, it names a specific profile supported by
this package (see
xdc.bld.ITarget.profiles).
Package
getLibs() functions should refer to this parameter
in lieu of the program's
build.profile. This allows configuration
scripts to selectively request debug or release libraries on a per
package basis, for example.
function getLibs(prog)
{
if (this.profile == "debug") {
...
}
}
If this parameter is not set by the configuration script, it is
initialized to
xdc.cfg.Program.build.profile prior to
generating and configuration files; i.e., the package's
getLibs() function can assume that this field is always
set and defaults to the profile used to build the executable.
IPackage.close() // module-wide |
![](../Arrow_up.png) |
Close this package after user scripts complete
DETAILS
This function is called to allow the package to modify its state
based on the results of the user's script. It can optionally
redefine configuration parameters or even throw exceptions to
prevent the configuration step from completing, for example.
Other packages and modules, including the modules in the package, can
change the configuration parameters of any module in the package, after
this function was called. Therefore, this function cannot be used to
validate state of the package and of the whole configuration.
Validation should be done in
validate().
For all packages A and B, if A requires B, then package A is
closed before package B.
The default implementation of this function is a nop.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
immediately after the program's configuration script
has completed and before validation is started.
RETURNS
Returns nothing.
THROWS
Error exceptions are thrown for fatal errors.
NOTE
This function can be called in any model, so any access to
global variables specific to a particular object model should happen
only if the function is called in the context of that model. For
example, the variable
Program is a global variable in the
Configuration Model (
xdc.cfg.Program). Any access to it
should happen after a check that the current model is the
Configuration Model:
if (xdc.om.$name == "cfg") {
print(Program.build.target.name);
}
For additional information about
xdc.om, see
xdc.om
in the
XDCscript Language Reference.
IPackage.exit() // module-wide |
![](../Arrow_up.png) |
Exit this package after the model has been successfully validated
DETAILS
The default implementation of this function is a nop.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
immediately after the program's configuration script
has completed and after generation has completed.
RETURNS
Returns nothing.
THROWS
Error exceptions are thrown for fatal errors.
NOTE
This function can be called in any model, so any access to
global variables specific to a particular object model should happen
only if the function is called in the context of that model. For
example, the variable
Program is a global variable in the
Configuration Model (
xdc.cfg.Program). Any access to it
should happen after a check that the current model is the
Configuration Model:
if (xdc.om.$name == "cfg") {
print(Program.build.target.name);
}
For additional information about
xdc.om, see
xdc.om
in the
XDCscript Language Reference.
IPackage.getLibs() // module-wide |
![](../Arrow_up.png) |
Get the libraries necessary to use this package
ARGUMENTS
prog
the configuration model program object
(xdc.cfg.Program) after the program's
configuration script has completed.
DETAILS
This function is called during the configuration model's generation
phase (after a program's configuration script completes and all
imported packages are closed) and is responsible for returning a list
of libraries (or object files) that are needed to link the program
being configured.
If the package produces one (or no) library for the target for which
the executable is being built, the default implementation of this
function simply returns the name of this library (or null).
If the package produces more than one library for the given target, the
default implementation of this function returns the following library
name:
lib/<package_name>.a<target_suffix>
where
<package_name> is the name of the package (e.g., "ti.bios")
and
<target_suffix> is the
xdc.bld.ITarget.suffix property
of the target used to build the executable.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
after the program's configuration script has completed.
- Program
-
The Configuration model program object
(xdc.cfg.Program) after the program's configuration
script has completed.
RETURNS
Returns a string of ';' delimited object (or library) file
names that are added to the list of things to link to
create the program. The file names are absolute or
relative to the package's base. All white space is
treated as part of the file name. If the files named do
not exist, a fatal error occurs and configuration
terminates.
If null or empty (""), then no libraries or objects are
required for this package.
THROWS
Error exceptions are thrown for fatal errors.
IPackage.getSects() // module-wide |
![](../Arrow_up.png) |
Get package-specific linker section data
DETAILS
This function is called during the configuration model's generation
phase (after a program's configuration script completes) and is
responsible for returning a template file name that is used to
generate package-specific linker command file statements.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
after the program's configuration script has completed.
- Program
-
The Configuration model program object
(xdc.cfg.Program) after program's configuration
script has completed and all packages have validated the
correctness of the configuration.
RETURNS
Returns the path name of template file. The path name
must relative to the package path or an absolute path.
If null is returned, no data is generated.
The template is evaluated in a context where the this
pointer is the package object.
THROWS
Error exceptions are thrown for fatal errors.
IPackage.init() // module-wide |
![](../Arrow_up.png) |
Initialize this package when first imported
DETAILS
This function is called to initialize the package within any
model. It is called just once (when the package is first imported)
so there is no need to explicitly check for prior invocation.
The default implementation of this function is a nop.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
before any model-specific user script runs (e.g. a program's
configuration script),
after the package's package.xs script is run and all
the package's modules are created, and before the
package is added to xdc.om.$packages (the Object Model's
package array)
RETURNS
Returns nothing.
THROWS
Error exceptions are thrown for fatal errors.
NOTE
This function can be called in any model, so any access to
global variables specific to a particular object model should happen
only if the function is called in the context of that model. For
example, the variable
Program is a global variable in the
Configuration Model (
xdc.cfg.Program). Any access to it
should happen after a check that the current model is the
Configuration Model:
if (xdc.om.$name == "cfg") {
print(Program.build.target.name);
}
For additional information about
xdc.om, see
xdc.om
in the
XDCscript Language Reference.
IPackage.validate() // module-wide |
![](../Arrow_up.png) |
Validate this package after the model's state is "sealed"
DETAILS
This function is called to validate the package's state in the
curent model. It can verify semantic constraints and optionally
throw exceptions to prevent the configuration step from completing.
For example, a package that needs to assert incompatibility with
certain versions of prerequisite packages can check the versions in
this function and throw an exception if they are known to be
incompatible with the current package.
This method must not modify the model.
The default implementation of this function is a nop.
CONTEXT
- this
-
The current package's xdc.IPackage.Module object
immediately after the program's configuration script
has completed and before generation started.
RETURNS
Returns nothing.
THROWS
Error exceptions are thrown for fatal errors.
NOTE
This function can be called in any model, so any access to
global variables specific to a particular object model should happen
only if the function is called in the context of that model. For
example, the variable
Program is a global variable in the
Configuration Model (
xdc.cfg.Program). Any access to it
should happen after a check that the current model is the
Configuration Model:
if (xdc.om.$name == "cfg") {
print(Program.build.target.name);
}
For additional information about
xdc.om, see
xdc.om
in the
XDCscript Language Reference.