package xdc.tools.cdoc.sg |
|
Interactive Package Documentation Browser
package xdc.tools.cdoc.sg {
// Interactive Package Documentation Browser
}
USAGE
xs xdc.tools.cdoc.sg [unit-name ...] [-Pr rdir ...]
This tool is used to interactively browse package documentation for
all packages found in the specified repositories rdir .... If no
repositories are specified after the optional -Pr flag, the
repositories in the current package path are used.
If one or more "unit-names" are specified, the corresponding package,
module, or interface reference pages are opened during startup.
This utility is invoked via the XDC xs command, where the
alias xs is defined as follows:
and $XDCROOT is the installation directory of the XDC toolset.
generated on Tue, 24 Aug 2010 15:39:20 GMT