This module's configuration parameters are initialized by
a "startup" script that is run prior to running a package's build
script (
package.bld). This script (often named "
config.bld") is
responsible for specifying the the
xdc.bld.ITarget.rootDir
configuration parameter of all targets that appear in the
targets array; the
rootDir configuration parameter specifies
the absolute path to the installation directory of the compiler used to
build for the specified target. Typically one startup script is used to
establish an environment for multiple packages.
Note: it does not matter if you do not have tools for all the targets
mentioned in the startup script; if you do not build for a target,
its setting in the startup script is irrelevant.
The startup script may configure this module as a function of the
following global variables that exist before this script runs:
enum BuildEnvironment.HostOS |
![](../../Arrow_up.png) |
An enumeration of all supported development hosts
XDCscript usage |
meta-domain |
values of type BuildEnvironment.HostOS
const BuildEnvironment.WINDOWS;
// Win32 Intel development host
const BuildEnvironment.SOLARIS;
// SUN OS 5.x development host
const BuildEnvironment.LINUX;
// Linux development host
SEE
config BuildEnvironment.hostOS // module-wide |
![](../../Arrow_up.png) |
Enumerated constant that identifies the host OS that is executing
the build script
XDCscript usage |
meta-domain |
DETAILS
Note that host OS at the time the makefiles are created may be
different from the host OS at the time sources are compiled!
config BuildEnvironment.hostOSName // module-wide |
![](../../Arrow_up.png) |
The name of the development host
XDCscript usage |
meta-domain |
const BuildEnvironment.hostOSName = String computed value;
DETAILS
One of the strings: "Windows", "Solaris", "Linux". This name is
name of the host OS that is executing the package's build script.
config BuildEnvironment.excludeTargets // module-wide |
![](../../Arrow_up.png) |
A set of targets to exclude from the set specified by
useTargets
XDCscript usage |
meta-domain |
BuildEnvironment.excludeTargets = String undefined;
DETAILS
This string parameter is a single regular expression used to exclude
targets from the set specified by useTargets (or XDCTARGETS).
If
targets is initialized by the build model's
configuration script (i.e., has length > 0) this parameter is
ignored.
If this string is
null or
undefined, nothing is excluded from
list specified by
useTargets or the environment variable
XDCTARGETS.
SEE
config BuildEnvironment.nativeTarget // module-wide |
![](../../Arrow_up.png) |
A target that defines the "native" target
XDCscript usage |
meta-domain |
DETAILS
This parameter allows build scripts to refer to the "native"
target without explicitly naming the target.
For example, a package.bld script may add a library via:
Pkg.addLibrary("lib", Build.nativeTarget);
In addition, it is possible to use
"native" in
XDCTARGETS or
useTargets to specify that
nativeTarget be added to the
targets array.
Thus, it is possible to use the following command on *any* host to
build for that host:
If this parameter is not set by the build model's configuration
script, it is initialized to an appropriate default native target:
config BuildEnvironment.platformTable // module-wide |
![](../../Arrow_up.png) |
A map of platform instance names to the parameters used to
create them
XDCscript usage |
meta-domain |
BuildEnvironment.platformTable = Any[string] [ ];
DETAILS
This map allows one to define platform instances that require
non-default parameter settings. It also provides a way to
publish a set of platforms to be shared among multiple build
scripts.
EXAMPLES
The following fragment defines a platform instance named
"ti.platforms.sim6xxx:big" that corresponds to a platform instance
created by the ti.platforms.sim6xxx.Platform module with the
parameters {endian: "big"}:
Build.platformTable["ti.platforms.sim6xxx:big"] = {endian: "big"};
The following fragment redefines the default platform instance for
the platform package ti.platforms.sim6xxx by specifying alternative
instance creation parameters.
Build.platformTable["ti.platforms.sim6xxx"] = {
endian: "little", verbose: false, ftpath: "c:/ftsuite_1_5",
};
Some platforms are "software abastractions" that can emulate a large
number different physical platforms. In the example below, the
ti.platforms.sim6xxx platform package is capable of simulating
any TMS320C6xxx device. This particular platform package uses the
name of the instance to determine the specific device that it should
emulate. So, the fragment below specifies a platform instance named
"ti.platforms.sim6xxx:TMS320C6416" that emulates the TMS320C6416
device, in little endian mode.
Build.platformTable["ti.platforms.sim6xxx:TMS320C6416"] = {
endian: "little"
};
Software platform packages, such as the ti.platforms.generic, can
even go as far as emulating any device from any "catalog" of
devices. In this example, we use the ti.platforms.generic
platform package to define an instance named
ti.platforms.generic:c6416 that corresponds to a platform
containing the TMS320C6416 device specified in the ti.catalog.c6000
package of devices.
Build.platformTable["ti.platforms.generic:c6416"] = {
deviceName: "TMS320C6416",
catalogName: "ti.catalog.c6000",
};
SEE
config BuildEnvironment.targets // module-wide |
![](../../Arrow_up.png) |
Array of all targets that are supported for the current build
XDCscript usage |
meta-domain |
DETAILS
This array may be explicitly initialized by the build model's
initial configuration script (by default, "config.bld"). For
example, the following fragment specifies that just the
ti.targets.C64 target should be used:
// get the ti.targets.C64 module
var C64 = xdc.module('ti.targets.C64');
// add the ti.target.C64 module to BuildEnvironment.targets array
Build.targets[Build.targets.length++] = C64;
Alternatively, this array can be implicitly initialized via the
XDCTARGETS environment variable or the
useTargets
and
excludeTargets strings. The
targets array
is implicitly initialized if and only if the length of this array is
0 after the build model's configuration script completes.
All targets that are in this array *must* have their
xdc.bld.ITarget.rootDir property set.
SEE
config BuildEnvironment.useTargets // module-wide |
![](../../Arrow_up.png) |
The set of targets to use if the targets array
is empty
XDCscript usage |
meta-domain |
BuildEnvironment.useTargets = String undefined;
DETAILS
useTargets is a string of white space separated target names
(i.e., names of modules that implement
xdc.bld.ITarget) or
regular expression patterns matching target names.
If the
Build.targets array is empty at the end of the
build model's configuration script, targets specified by this string
are added to the build model's
targets array.
In addition to module names, the distinguished string
"native" is interpreted as an alias for the target
specified by the
nativeTarget configuration
parameter.
Special values:
- undefined
-
use the environment variable XDCTARGETS;
- null
-
initialize the targets array to be empty; and
- ""
-
use all TI targets (i.e., "ti.targets\..*").
SEE
BuildEnvironment.getReleaseDescs() // module-wide |
![](../../Arrow_up.png) |
Return a description of all releases for the specified package
XDCscript usage |
meta-domain |
BuildEnvironment.
getReleaseDescs(
String pname)
returns Release.Desc[]
ARGUMENTS
pname
name of the package to get the release
information from
DETAILS
This function allows a "package of packages" to select appropriate
releases from another package based on information provided by that
package.
RETURNS
array of
xdc.bld.Release.Desc
structures that describe the releases specified
by
pname's build script
THROWS
XDCException exceptions are thrown for fatal
errors. The following error codes are
reported in the exception message:
- xdc.bld.PACKAGE_NOT_BUILT
-
This error is reported when a consumer tries to
use a package that has not been built. Ensure that
the required package has been built by the xdc
tool.
- xdc.bld.INVALID_PACKAGE
-
This error is reported when a consumer tries to
use a corrupted package. Try rebuilding the
package causing the problem.
SEE