typedef IClock.IPeripheralArray |
![](../../../../../Arrow_up.png) |
typedef IClock.StringArray |
![](../../../../../Arrow_up.png) |
typedef String StringArray[];
struct IClock.ForceSetDefaultRegister_t |
![](../../../../../Arrow_up.png) |
Force Set Default Register
metaonly struct ForceSetDefaultRegister_t {
String register;
Bool regForceSet;
};
DETAILS
Type to store if each register needs to be forced initialized
even if the register is in default state.
SEE
IClock.addPeripheralsMap() // module-wide |
![](../../../../../Arrow_up.png) |
Create a map of all peripherals available on a device
ARGUMENTS
DETAILS
The config parameter
peripherals is by default undefined in an
xdc.platform.ICpuDataSheet instance. This function gathers
all instance configuration parameters that are of the type
xdc.platform.IPeripheral into the map
peripherals.
IClock.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
IClock.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
RETURNS
Returns an array of register names
config IClock.ACLKHz // instance |
![](../../../../../Arrow_up.png) |
Stores ACLK as frequency in float
readonly config Float ACLKHz;
config IClock.DCOCLKHz // instance |
![](../../../../../Arrow_up.png) |
Stores the DCO clock frequency in float
readonly config Float DCOCLKHz = 1000000;
config IClock.MCLKHz // instance |
![](../../../../../Arrow_up.png) |
Stores MCLK as frequency in float
readonly config Float MCLKHz;
config IClock.SMCLKHz // instance |
![](../../../../../Arrow_up.png) |
Stores SMCLK as frequency in float
readonly config Float SMCLKHz;
config IClock.baseAddr // instance |
![](../../../../../Arrow_up.png) |
Address of the peripheral's control register
DETAILS
A peripheral's registers are commonly accessed through a structure
that defines the offsets of a particular register from the lowest
address mapped to a peripheral. That lowest address is specified by
this parameter.
config IClock.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config IClock.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
IClock.computeDCOCLKHz() // instance |
![](../../../../../Arrow_up.png) |
Initialize to the nearest available DCO clock frequency
Void computeDCOCLKHz(Float DCOCLKHz);