From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Package-Object.$spec
Package specification object
Contents |
Synopsis
| «pkg».$spec |
where «pkg» is a package object.
Description
The $spec property of package object is an object that provides access to various properties of the package derived from the package's specification (package.xdc). The $spec property is a LiveConnect instance of the Java class xdc.services.spec.Pkg.
See also
xdc.services.spec | Client documentation for xdc.services.spec |
XDCscript - Module-Object.$spec | Module specification object |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved