From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
XDCscript - Module-Object.$spec
Module specification object
Contents |
Synopsis
| «Mod».$spec |
where «Mod» is a module object.
Description
The $spec property of module object is an object that provides access to various properties of the module derived from the module's specification («Mod».xdc). The $spec property is a LiveConnect instance of the Java class xdc.services.spec.Unit.
See also
xdc.services.spec | Client documentation for xdc.services.spec |
XDCscript - Package-Object.$spec | Package specification object |
![]() | [printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved