A logger is responsible for recording, transmitting, or otherwise
handling
Log Events generated by clients of the
Log module. The
Log module uses modules that implement the
ILogger interface to record the log events. Most application code will
use the
Log module instead of directly calling the specific
ILogger
module implementation.
All logger implementations must inherit from this interface. The
derived implementations must implement the functions defined in this
interface but may also add additional configuration parameters and
functions.
Events may be defined with a detail level, but the Log interface does not
inherently provide support for filtering of events based on detail level.
Instead, this is left to the ILogger implementation. ILogger
implementations which wish to support filtering based on detail level
should implement the IFilterLogger interface, which extends the ILogger
interface to include APIs for getting and setting the current filter level.
metaonly config ILogger.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly ILogger.getMetaArgs() // module-wide |
|
Returns any meta data needed to support RTA
metaonly function getMetaArgs(inst, instNum);
DETAILS
This meta data should be returned in the form of a structure which
can be converted into XML. This data is added to the RTA XML file
during the application's configuration, and can be accessed later
through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The
instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of
the ILogger's static instances.
ILogger.disable() // instance |
|
Disable a log
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
ILogger.enable() // instance |
|
Enable a log
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
ILogger.write0() // instance |
|
Process a log event with 0 arguments
DETAILS
Same as write4 except with 0 arguments rather than 4.
SEE
ILogger.write1() // instance |
|
Process a log event with 1 arguments
DETAILS
Same as write4 except with 1 arguments rather than 4.
SEE
ILogger.write2() // instance |
|
Process a log event with 2 arguments
DETAILS
Same as write4 except with 2 arguments rather than 4.
SEE
ILogger.write4() // instance |
|
Process a log event with up to 4 arguments
ARGUMENTS
evt
event to be logged
mid
module ID of the module which logged the event
a1
arbitrary argument passed by caller
DETAILS
The
evt argument is of type Log.Event, which encodes the
Log.EventId, the
Diags.Mask, and the
Diags.EventLevel of the event. The event ID can be obtained
via
Types.getEventId(evt), the Diags mask can be obtained via
Diags.getMask(evt), and the event level can be obtained via
Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the
event.
The event information can be used by the logger to handle different
events specially. For example, the event ID can be used to compare
against other known Log.Events.
if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
:
}
The Diags mask and event level can be used for filtering of events
based on event level (see
IFilterLogger), or even routing
events to separate loggers based on diags category (see, for example,
LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but
are generally not recorded by the logger because they are not needed in
decoding and displaying the event. A more suitable value to record is a
Types.Event, which encodes the event ID and module ID. For
example, the
Log.EventRec type stores a
Types.Event
in its record definition. A
Types.Event can be created using
the
Types.makeEvent API given the event ID and module ID.
The event ID value of
0 is used to indicate an event triggered by a
call to one of the
Log_print[0-6] methods. These
methods take a format string rather than a
Log_Event argument and,
as a result, the event ID encoded in
evt is
0 and the parameter
a1 is the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Log_EventId id = Log_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted
according to the message format string associated with evt.
SEE
ILogger.write8() // instance |
|
Process a log event with up to 8 arguments
Void write8(
Log.Event evt,
Types.ModuleId mid,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8);
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE