enum WDTPlus.WDTCNTCL_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTCNTCL_t
const WDTPlus.WDTCNTCL_OFF;
const WDTPlus.WDTCNTCL;
enum WDTPlus.WDTHOLD_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTHOLD_t
const WDTPlus.WDTHOLD_OFF;
const WDTPlus.WDTHOLD;
enum WDTPlus.WDTIS0_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTIS0_t
const WDTPlus.WDTIS0_OFF;
const WDTPlus.WDTIS0;
enum WDTPlus.WDTIS1_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTIS1_t
const WDTPlus.WDTIS1_OFF;
const WDTPlus.WDTIS1;
enum WDTPlus.WDTNMIES_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTNMIES_t
const WDTPlus.WDTNMIES_OFF;
const WDTPlus.WDTNMIES;
enum WDTPlus.WDTNMI_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTNMI_t
const WDTPlus.WDTNMI_OFF;
const WDTPlus.WDTNMI;
enum WDTPlus.WDTPW_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTPW_t
const WDTPlus.WDTPW_OFF;
const WDTPlus.WDTPW;
enum WDTPlus.WDTSSEL_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTSSEL_t
const WDTPlus.WDTSSEL_OFF;
const WDTPlus.WDTSSEL;
enum WDTPlus.WDTTMSEL_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type WDTPlus.WDTTMSEL_t
const WDTPlus.WDTTMSEL_OFF;
const WDTPlus.WDTTMSEL;
struct WDTPlus.WDTCTL_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var obj = new WDTPlus.WDTCTL_t;
// WDT+ password
// Watchdog timer+ hold. This bit stops the watchdog timer+. Setting
WDTHOLD = 1 when the WDT+ is not in use conserves power.
0 Watchdog timer+ is not stopped
1 Watchdog timer+ is stopped
// Watchdog timer+ NMI edge select. This bit selects the interrupt edge for the
NMI interrupt when WDTNMI = 1. Modifying this bit can trigger an NMI. Modify
this bit when WDTIE = 0 to avoid triggering an accidental NMI.
0 NMI on rising edge
1 NMI on falling edge
// Watchdog timer+ NMI select. This bit selects the function for the RST/NMI pin.
0 Reset function
1 NMI function
// Watchdog timer+ mode select
0 Watchdog mode
1 Interval timer mode
// Watchdog timer+ counter clear. Setting WDTCNTCL = 1 clears the count
value to 0000h. WDTCNTCL is automatically reset.
0 No action
1 WDTCNT = 0000h
// Watchdog timer+ clock source select
0 SMCLK
1 ACLK
// Watchdog timer+ interval select. These bits select the watchdog timer+
interval to set the WDTIFG flag and/or generate a PUC.
00 Watchdog clock source /32768
01 Watchdog clock source /8192
10 Watchdog clock source /512
11 Watchdog clock source /64
// Watchdog timer+ interval select. These bits select the watchdog timer+
interval to set the WDTIFG flag and/or generate a PUC.
00 Watchdog clock source /32768
01 Watchdog clock source /8192
10 Watchdog clock source /512
11 Watchdog clock source /64
WDTPlus.addPeripheralsMap() // module-wide |
![](../../../../../Arrow_up.png) |
Create a map of all peripherals available on a device
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
The config parameter
peripherals is by default undefined in an
xdc.platform.ICpuDataSheet instance. This function gathers
all instance configuration parameters that are of the type
xdc.platform.IPeripheral into the map
peripherals.
WDTPlus.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
XDCscript usage |
meta-domain |
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
WDTPlus.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
XDCscript usage |
meta-domain |
WDTPlus.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new WDTPlus.Params;
// Instance config-params object
// WDTCTL, Watchdog Timer+ Register
};
params.baseAddr = UInt undefined;
// Address of the peripheral's control register
params.name = String undefined;
// Specific peripheral name given by the device
params.owner = String undefined;
// String specifying the entity that manages the peripheral
config WDTPlus.WDTCTL // instance |
![](../../../../../Arrow_up.png) |
WDTCTL, Watchdog Timer+ Register
XDCscript usage |
meta-domain |
var params = new WDTPlus.Params;
...
};
config WDTPlus.baseAddr // instance |
![](../../../../../Arrow_up.png) |
Address of the peripheral's control register
XDCscript usage |
meta-domain |
var params = new WDTPlus.Params;
...
params.baseAddr = UInt undefined;
DETAILS
A peripheral's registers are commonly accessed through a structure
that defines the offsets of a particular register from the lowest
address mapped to a peripheral. That lowest address is specified by
this parameter.
config WDTPlus.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
XDCscript usage |
meta-domain |
var params = new WDTPlus.Params;
...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config WDTPlus.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
XDCscript usage |
meta-domain |
var params = new WDTPlus.Params;
...
params.owner = String undefined;
Instance Creation |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new WDTPlus.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object