enum OA_3.OAADC0_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type OA_3.OAADC0_t
const OA_3.OAADC0_OFF;
const OA_3.OAADC0;
enum OA_3.OAADC1_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type OA_3.OAADC1_t
const OA_3.OAADC1_OFF;
const OA_3.OAADC1;
enum OA_3.OAFBR_t |
![](../../../../../Arrow_up.png) |
OAx feedback resistor select
XDCscript usage |
meta-domain |
values of type OA_3.OAFBR_t
const OA_3.OAFBR_0;
const OA_3.OAFBR_1;
const OA_3.OAFBR_2;
const OA_3.OAFBR_3;
const OA_3.OAFBR_4;
const OA_3.OAFBR_5;
const OA_3.OAFBR_6;
const OA_3.OAFBR_7;
enum OA_3.OAFC_t |
![](../../../../../Arrow_up.png) |
OAx function control
XDCscript usage |
meta-domain |
values of type OA_3.OAFC_t
const OA_3.OAFC_0;
const OA_3.OAFC_1;
const OA_3.OAFC_2;
const OA_3.OAFC_3;
const OA_3.OAFC_4;
const OA_3.OAFC_5;
const OA_3.OAFC_6;
const OA_3.OAFC_7;
enum OA_3.OANEXT_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type OA_3.OANEXT_t
const OA_3.OANEXT_OFF;
const OA_3.OANEXT;
enum OA_3.OAN_t |
![](../../../../../Arrow_up.png) |
Inverting input selection
XDCscript usage |
meta-domain |
values of type OA_3.OAN_t
const OA_3.OAN_0;
// OAxI0
const OA_3.OAN_1;
// OAxI1
const OA_3.OAN_2;
// OAxIA (see the device-specific data sheet for connected signal)
const OA_3.OAN_3;
// OAxIB (see the device-specific data sheet for connected signal)
enum OA_3.OAPM_t |
![](../../../../../Arrow_up.png) |
Slew rate select
XDCscript usage |
meta-domain |
values of type OA_3.OAPM_t
const OA_3.OAPM_0;
// OAx Power mode select: Off, output high Z
const OA_3.OAPM_1;
// OAx Power mode select: Slow
const OA_3.OAPM_2;
// OAx Power mode select: Medium
const OA_3.OAPM_3;
// OAx Power mode select: Fast
enum OA_3.OAP_t |
![](../../../../../Arrow_up.png) |
Non-inverting input selection
XDCscript usage |
meta-domain |
values of type OA_3.OAP_t
const OA_3.OAP_0;
// OAxI0
const OA_3.OAP_1;
// OAxI1
const OA_3.OAP_2;
// OAxIA (see the device-specific data sheet for connected signal)
const OA_3.OAP_3;
// OAxIB (see the device-specific data sheet for connected signal)
enum OA_3.OARRIP_t |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
values of type OA_3.OARRIP_t
const OA_3.OARRIP_OFF;
const OA_3.OARRIP;
struct OA_3.OAxCTL0_t |
![](../../../../../Arrow_up.png) |
Opamp Control Register 0 Definition
XDCscript usage |
meta-domain |
var obj = new OA_3.OAxCTL0_t;
// Inverting input select. These bits select the input signal for the OA inverting
input.
00 OAxI0
01 OAxI1
10 OAxIA (see the device-specific data sheet for connected signal)
11 OAxIB (see the device-specific data sheet for connected signal)
// Non-inverting input select. These bits select the input signal for the OA
non-inverting input.
00 OAxI0
01 OA0I1
10 OAxIA (see the device-specific data sheet for connected signal)
11 OAxIB (see the device-specific data sheet for connected signal)
// Slew rate select. These bits select the slew rate vs. current consumption
for the OA.
00 Off, output high Z
01 Slow
10 Medium
11 Fast
// OA output select. These bits, together with the OAFCx bits, control the
routing of the OAx output when OAPMx > 0.
When OAFCx = 0:
00 OAxOUT connected to external pins and ADC input A1, A3, or A5
01 OAxOUT connected to external pins and ADC input A12, A13, or A14
10 OAxOUT connected to external pins and ADC input A1, A3, or A5
11 OAxOUT connected to external pins and ADC input A12, A13, or A14
When OAFCx > 0:
00 OAxOUT used for internal routing only
01 OAxOUT connected to external pins and ADC input A12, A13, or A14
10 OAxOUT connected to external pins and ADC input A1, A3, or A5
11 OAxOUT connected internally to ADC input A12, A13 , or A14.
External A12, A13, or A14 pin connections are disconnected from the
ADC
// OA output select. These bits, together with the OAFCx bits, control the
routing of the OAx output when OAPMx > 0.
When OAFCx = 0:
00 OAxOUT connected to external pins and ADC input A1, A3, or A5
01 OAxOUT connected to external pins and ADC input A12, A13, or A14
10 OAxOUT connected to external pins and ADC input A1, A3, or A5
11 OAxOUT connected to external pins and ADC input A12, A13, or A14
When OAFCx > 0:
00 OAxOUT used for internal routing only
01 OAxOUT connected to external pins and ADC input A12, A13, or A14
10 OAxOUT connected to external pins and ADC input A1, A3, or A5
11 OAxOUT connected internally to ADC input A12, A13 , or A14.
External A12, A13, or A14 pin connections are disconnected from the
ADC
SEE
struct OA_3.OAxCTL1_t |
![](../../../../../Arrow_up.png) |
Opamp Control Register 1 Definition
XDCscript usage |
meta-domain |
var obj = new OA_3.OAxCTL1_t;
// OAx feedback resistor select
000 Tap 0 - 0R/16R
001 Tap 1 - 4R/12R
010 Tap 2 - 8R/8R
011 Tap 3 - 10R/6R
100 Tap 4 - 12R/4R
101 Tap 5 - 13R/3R
110 Tap 6 - 14R/2R
111 Tap 7 - 15R/1R
// OAx function control. This bit selects the function of OAx
000 General purpose opamp
001 Unity gain buffer for three-opamp differential amplifier
010 Unity gain buffer
011 Comparator
100 Non-inverting PGA amplifier
101 Cascaded non-inverting PGA amplifier
110 Inverting PGA amplifier
111 Differential amplifier
// OAx inverting input externally available. This bit, when set, connects the
inverting OAx input to the external pin when the integrated resistor network
is used.
0 OAx inverting input not externally available
1 OAx inverting input externally available
// OAx reverse resistor connection in comparator mode
0 RTOP is connected to AVSS and RBOTTOM is connected to AVCC when
OAFCx = 3
1 RTOP is connected to AVCC and RBOTTOM is connected to AVSS when
OAFCx = 3
SEE
OA_3.addPeripheralsMap() // module-wide |
![](../../../../../Arrow_up.png) |
Create a map of all peripherals available on a device
XDCscript usage |
meta-domain |
ARGUMENTS
DETAILS
The config parameter
peripherals is by default undefined in an
xdc.platform.ICpuDataSheet instance. This function gathers
all instance configuration parameters that are of the type
xdc.platform.IPeripheral into the map
peripherals.
OA_3.getAll() // module-wide |
![](../../../../../Arrow_up.png) |
Find all peripherals of a certain type
XDCscript usage |
meta-domain |
DETAILS
The type of the peripherals returned is defined by the type of the
caller.
RETURNS
Returns an array of IPeripheral instances
OA_3.getRegisters() // module-wide |
![](../../../../../Arrow_up.png) |
Find all registers defined by the peripheral
XDCscript usage |
meta-domain |
OA_3.getRegisters() returns String[]
RETURNS
Returns an array of register names
Instance Config Parameters |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
// Instance config-params object
// OA0 control register 0
};
// OA0 control register 1
};
// OA1 control register 0
};
// OA1 control register 1
};
// OA2 control register 0
};
// OA2 control register 1
};
params.name = String undefined;
// Specific peripheral name given by the device
params.owner = String undefined;
// String specifying the entity that manages the peripheral
config OA_3.OA0CTL0 // instance |
![](../../../../../Arrow_up.png) |
OA0 control register 0
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.OA0CTL1 // instance |
![](../../../../../Arrow_up.png) |
OA0 control register 1
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.OA1CTL0 // instance |
![](../../../../../Arrow_up.png) |
OA1 control register 0
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.OA1CTL1 // instance |
![](../../../../../Arrow_up.png) |
OA1 control register 1
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.OA2CTL0 // instance |
![](../../../../../Arrow_up.png) |
OA2 control register 0
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.OA2CTL1 // instance |
![](../../../../../Arrow_up.png) |
OA2 control register 1
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
};
config OA_3.name // instance |
![](../../../../../Arrow_up.png) |
Specific peripheral name given by the device
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
params.name = String undefined;
DETAILS
Devices can have more than one peripheral of the same type. In such
cases, device data sheets give different names to the instances of a
same peripheral. For example, the name for a timer module could be
TimerA3, and a device that has two such timers can name them TA0
and TA1.
config OA_3.owner // instance |
![](../../../../../Arrow_up.png) |
String specifying the entity that manages the peripheral
XDCscript usage |
meta-domain |
var params = new OA_3.Params;
...
params.owner = String undefined;
Instance Creation |
![](../../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = OA_3.create(params);
// Create an instance-object
OA_3.getNumberOfOA() // instance |
![](../../../../../Arrow_up.png) |
Returns the number of available OA
XDCscript usage |
meta-domain |
inst.getNumberOfOA() returns UChar