const SyncNull_NO_WAIT |
![](../../../Arrow_up.png) |
Used to specify no waiting
#define SyncNull_NO_WAIT (UInt)0
const SyncNull_Q_BLOCKING |
![](../../../Arrow_up.png) |
Blocking quality
#define SyncNull_Q_BLOCKING (Int)1
DETAILS
Implementations with this "quality" may cause the calling thread to
block;
const SyncNull_WAIT_FOREVER |
![](../../../Arrow_up.png) |
Used to wait forever
#define SyncNull_WAIT_FOREVER (UInt)~(0)
enum SyncNull_WaitStatus |
![](../../../Arrow_up.png) |
Error codes returned by ISync_wait
typedef enum SyncNull_WaitStatus {
SyncNull_WaitStatus_ERROR,
SyncNull_WaitStatus_TIMEOUT,
SyncNull_WaitStatus_SUCCESS
} SyncNull_WaitStatus;
Module-Wide Built-Ins |
![](../../../Arrow_up.png) |
// Get this module's unique id
Bool SyncNull_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SyncNull_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SyncNull_Module_getMask();
// Returns the diagnostics mask for this module
Void SyncNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
![](../../../Arrow_up.png) |
typedef struct SyncNull_Object SyncNull_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct SyncNull_Struct SyncNull_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
![](../../../Arrow_up.png) |
typedef struct SyncNull_Params {
// Instance config-params structure
// Common per-instance configs
} SyncNull_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
Instance Creation |
![](../../../Arrow_up.png) |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
Instance Deletion |
![](../../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
SyncNull_query() // instance |
![](../../../Arrow_up.png) |
Query for a particular quality
ARGUMENTS
handle
handle of a previously-created SyncNull instance object
qual
quality
RETURNS
TRUE or FALSE.
DETAILS
FALSE is returned if quality not supported.
SyncNull_signal() // instance |
![](../../../Arrow_up.png) |
Called at completion of an activity
ARGUMENTS
handle
handle of a previously-created SyncNull instance object
DETAILS
This function is non-blocking. It is also required that the underlying
sync be binary in nature.
This function does not take an Error.Block intentionally because
it can be called from ISR context.
SyncNull_wait() // instance |
![](../../../Arrow_up.png) |
Called to wait/poll for completion of an activity
ARGUMENTS
handle
handle of a previously-created SyncNull instance object
timeout
Timeout in microseconds
eb
Hist Pointer to Error.Block
RETURNS
Refer to description above
DETAILS
This function can block. Non-blocking implementations should return
WaitStatus_TIMEOUT to indicate a timeout.
Instance Convertors |
![](../../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
![](../../../Arrow_up.png) |
Int SyncNull_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object