interface xdc.runtime.knl.IGateThreadSupport

Interface for OS specific back-end. [EXPERIMENTAL]

The xdc.runtime.knl package contains modules that provide typical OS services. These xdc.runtime.knl modules require proxies to be bound to an OS specific delegate. This specifies the interface to be implemented by the OS specific delegate for xdc.runtime.knl.GateThread module. [ more ... ]
XDCspec summary sourced in xdc/runtime/knl/IGateThreadSupport.xdc
interface IGateThreadSupport {  ...
    // inherits xdc.runtime.IModule
instance:  ...
XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
package xdc.runtime.knl;
 
interface IGateThreadSupport inherits IGateProvider {
module-wide constants & types
    const Int Q_BLOCKING// Blocking quality = 1;
    const Int Q_PREEMPTING// Preempting quality = 2;
module-wide config parameters
module-wide functions
 
 
 
instance:
per-instance creation
per-instance functions
    IArg enter// Enter this gate( );
    Void leave// Leave this gate( IArg key );
}
C synopsis target-domain
DETAILS
The xdc.runtime.knl package contains modules that provide typical OS services. These xdc.runtime.knl modules require proxies to be bound to an OS specific delegate. This specifies the interface to be implemented by the OS specific delegate for xdc.runtime.knl.GateThread module.
The implementation of IGateThreadSupport should try to implement a gate that supports priority inversion.
See xdc.runtime.knl for more details.
 
const IGateThreadSupport.Q_BLOCKING

Blocking quality

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
const Int Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const IGateThreadSupport.Q_PREEMPTING

Preempting quality

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
const Int Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
metaonly config IGateThreadSupport.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
IGateThreadSupport.query( )  // module-wide

Runtime test for a particular gate quality

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
Bool query( Int qual );
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
metaonly IGateThreadSupport.queryMeta( )  // module-wide

Configuration time test for a particular gate quality

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
metaonly Bool queryMeta( Int qual );
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
per-instance object types

C synopsis target-domain
typedef struct IGateThreadSupport_Object *IGateThreadSupport_Handle;
// Client reference to an abstract instance object
 
per-instance config parameters

XDCscript usage meta-domain
var params = new IGateThreadSupport.Params;
// Instance config-params object
C synopsis target-domain
typedef struct IGateThreadSupport_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} IGateThreadSupport_Params;
 
per-instance creation

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
create( );
// Create an instance-object
 
IGateThreadSupport.enter( )  // per-instance

Enter this gate

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
IArg enter( );
 
DETAILS
Each gate provider can implement mutual exclusion using different algorithms; e.g., disabling all scheduling, disabling the scheduling of all threads below a specified "priority level", suspending the caller when the gate has been entered by another thread and re-enabling it when the the other thread leaves the gate. However, in all cases, after this method returns that caller has exclusive access to the data protected by this gate.
A thread may reenter a gate without blocking or failing.
RETURNS
Returns a "key" that is used to leave this gate; this value is used to restore thread preemption to the state that existed just prior to entering this gate.
 
IGateThreadSupport.leave( )  // per-instance

Leave this gate

XDCspec declarations sourced in xdc/runtime/knl/IGateThreadSupport.xdc
Void leave( IArg key );
 
ARGUMENTS
key — the value returned by a matching call to enter
DETAILS
This method is only called by threads that have previously entered this gate via enter. After this method returns, the caller must not access the data structure protected by this gate (unless the caller has entered the gate more than once and other calls to leave remain to balance the number of previous calls to enter).
 
per-instance convertors

C synopsis target-domain
IGateProvider_Handle IGateThreadSupport_Handle_upCast( IGateThreadSupport_Handle handle );
// unconditionally move one level up the inheritance hierarchy
 
IGateThreadSupport_Handle IGateThreadSupport_Handle_downCast( IGateProvider_Handle handle );
// conditionally move one level down the inheritance hierarchy; NULL upon failure
generated on Fri, 25 Jun 2010 00:01:29 GMT