metaonly module xdc.bld.Test |
![](../../Arrow_left.png) |
![](../../Arrow_up.png) |
![](../../Arrow_right.png) |
Model of a test
Each Test instance represents a pair consisting of an executable and
command line arguments for that executable. Each pair uniquely
identifies an output sequence (the result of running the executable
with the specified arguments) that can be compared to a known valid
result. Executables that have non-deterministic execution behavior
(e.g., multi-threaded apps) must ensure that the output is independent
of these variations.
[
more ... ]
metaonly module Test { ...
instance: ...
XDCscript usage |
meta-domain |
var Test = xdc.useModule('xdc.bld.Test');
module-wide constants & types
per-instance config parameters
metaonly module Test {
module-wide constants & types
};
instance:
per-instance config parameters
}
DETAILS
Each Test instance represents a pair consisting of an executable and
command line arguments for that executable. Each pair uniquely
identifies an output sequence (the result of running the executable
with the specified arguments) that can be compared to a known valid
result. Executables that have non-deterministic execution behavior
(e.g., multi-threaded apps) must ensure that the output is independent
of these variations.
Test instances are created via the Executable.addTest() function;
this ensures that each test is associated with a containing executable.
Test instances do not have unique names. However, each test does have
a "group" name which is optionally specified via Test.Attrs. If the
"group" name is not specified, it defaults to the name of the containing
executable. To run any group of tests (which may consist of one or more
executable and command-line pairs) it is sufficient to run
the following command:
xdc <test_group_name>.test
where <test_group_name> is the name of the test group to run.
Each Executable instance (created via PackageContents.addExecutable())
implicitly adds a test whose "group" name is the name of the executable
and whose arguments are empty (i.e., argc == 0). Thus, it is possible
to run any executable that can be built using the following command:
where <exe_name> is the name of the executable. Note that if you add a
test to the executable (without specifying a unique groupName), the
command above will run the executable more than once; it will run once
for every test associated with the executable.
struct Test.Attrs |
![](../../Arrow_up.png) |
Optional attributes for a test instance
XDCscript usage |
meta-domain |
var obj = new Test.Attrs;
obj.args = String ...
// arguments passed to the exe for this test
obj.execCmd = String ...
// exec command for this test
obj.execArgs = String ...
// arguments to the exec command itself
obj.groupName = String ...
// name of a group of related tests
obj.refOutput = String ...
// name of a reference output file
obj.refExitCode = Int ...
// expected exit code (default = 0)
FIELDS
args
this is a string of arguments (which may contain
embedded strings) that are passed to the executable
being run.
execCmd
this string names the "loader" which is responsible
for running the executable with the arguments
specified by the args field. If this field is
null or undefined, the command used to run
the executable is determined by the executable's
configuration script; see
xdc.cfg.Program.execCmd.
execArgs
this is a string of arguments passed to the
"loader" to control how this loader manages the
execution of the executable being run.
groupName
the name of the group of tests that this test is a
a member of.
refOutput
the name of a "reference" text file that is used
to validate the output generated by running
the executable with the specified arguments. If
the exit status of the executable is 0 and the
output of the executable differs from the
contents of refOutput, the test fails. If this
comparison fails, the output of the executable is
saved to a temporary file to allow analysis of the
failure. The temporary file's name is:
".tmp,{exeName},{id}", where {exeName} is the
name of the executable and {id} is a test
id number.
If refOutput is not defined (or set to null)
no comparison is made; only the exit status of the
executable is used to determine the success or
failure of the test.
refExitCode
the expected exit status of the executable.
If refExitCode is not defined (or set to null)
an exit status of 0 is assumed.
DETAILS
Unspecified attributes are "inherited" from
Executable.Attrs;
i.e., if one of fields in this structure is unspecified *and* this
field's name matches a field name in
Executable.Attrs, then
this field's value defaults to the value in specified by
Executable.Attrs. This mechanism makes it possible to establish
executable-specific default values for any of the "inherited"
attributes.
SEE
per-instance config parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Test.Params;
// Instance config-params object
// Optional attributes for this test instance
config Test.attrs // per-instance |
![](../../Arrow_up.png) |
Optional attributes for this test instance
XDCscript usage |
meta-domain |
var params = new Test.Params;
...
DETAILS
Default values for each of the fields in attrs:
- groupName
-
name of the program "containing" this test
- execCmd
-
the first non-null value in:
prog.attrs.test.exec,
xdc.cfg.Program.execCmd,
prog.platform.getExecCmd().
- execArgs
-
the first non-null value in:
prog.attrs.test.execArgs,
"".
- args
-
the first non-null value in:
prog.attrs.test.args,
"".
generated on Sat, 12 Jun 2010 05:51:50 GMT