metaonly module xdc.tools.path.sg.Main |
![](../../../../Arrow_up.png) |
Graphical interface to path tool
This graphical interactive tool displays the packages located along any
specified package repository path.
[
more ... ]
metaonly module Main { ...
instance: ...
XDCscript usage |
meta-domain |
var Main = xdc.useModule('xdc.tools.path.sg.Main');
module-wide config parameters
'[--packagepath PATH]'
];
module-wide functions
per-instance config parameters
per-instance functions
metaonly module Main inherits ICmd {
module-wide config parameters
'[--packagepath PATH]'
];
module-wide functions
instance:
per-instance config parameters
per-instance functions
}
USAGE
xs xdc.tools.path.sg [--packagepath PATH]
DETAILS
This graphical interactive tool displays the packages located along any
specified package repository path.
At startup, this tool shows the packages located along the current package
path; i.e.,
$XDCPATH;$XDCROOT/packages;^
where $XDCPATH is the value of the the user settable prefix of the
package path, $XDCROOT is the installation directory of the XDC tools,
and ^ is the repository of the package in the current working directory
(if it exists). To specify a package path other than the current package
path, use the --packagepath option. Only semicolon delimited canonical
paths should be specifed as arguments with the --packagepath option.
Environment variables such as $XDCROOT and special designators such as
'^' should not be used.
BUGS
This tool scans all packages available along the current
package path before displaying the user interface. So, a repository in
the package path that contains a large number of sub-directories, such
as '/', causes very long delays before the user interface is displayed.
While it is easy to see that you should not put '/' in the package path,
it is less obvious that installing a package at '/' has the same effect.
config Main.usage // module-wide |
![](../../../../Arrow_up.png) |
Usage for this command
XDCscript usage |
meta-domain |
Main.usage = String[] [
'[--packagepath PATH]'
];
Main.exec( ) // module-wide |
![](../../../../Arrow_up.png) |
'xs' script entry point
XDCscript usage |
meta-domain |
Main.exec( Any args ) returns Any
Main.main( ) // module-wide |
![](../../../../Arrow_up.png) |
'xs' shell entry point
XDCscript usage |
meta-domain |
Main.main( Any args ) returns Any
per-instance config parameters |
![](../../../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Main.Params;
// Instance config-params object
params.pathArg = String null;
// package path to scan for packages
config Main.pathArg // per-instance |
![](../../../../Arrow_up.png) |
package path to scan for packages
XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.pathArg = String null;
Main.run( ) // per-instance |
![](../../../../Arrow_up.png) |
Underlying implementation
XDCscript usage |
meta-domain |
generated on Thu, 25 Feb 2010 19:25:08 GMT