From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Command Line Tools
Command line tools overview
Contents |
This reference provides an overview of the command-line tools provided for creating and working with packages. In addition, it provides a brief description of the most frequently used commands.
Core commands
XDCtools requires just two "core" commands shown in the table below.
Command - xdc | eXpanDed C package build command |
Command - xs | XDCscript interpreter |
XDCscript commands
In addition to the core commands above, many of the basic tools are implemented as packages containing XDCscript utilities. Each of the commands shown in the table below is run using the xs utility above.
Command - xdc.tools.cdoc | Package documentation tool |
Command - xdc.tools.cdoc.sg | Interactive package documentation tool |
Command - xdc.tools.check | Repository compatibility check tool |
Command - xdc.tools.closure | Closure tool |
Command - xdc.tools.configuro | Target content configuration tool |
Command - xdc.tools.path | Package path display tool |
Command - xdc.tools.path.sg | Interactive Package Path browser tool |
Command - xdc.tools.repoman | Repository management tool |
Command - xdc.tools.repoman.sg | Interactive repository management tool |
Utility commands
Finally, the commands above use a few "utility" commands that are useful in their own right. These last tools are most useful within makefiles or shell scripts.
Command - xdcdir | eXpanDed C print package name or repository |
Command - xdclpf | eXpanDed C package file list command |
Command - xdcpkg | eXpanDed C package list command |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved