From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC

Command - xdc.tools.path

Package path display tool

Contents

Synopsis

 
xs xdc.tools.path [options ...]

For a complete description of this tool's options, see its Cdoc reference page xdc.tools.path.

Description

The path tool displays the packages located along the specified package path. Both textual and graphical versions of this tool are provided. The textual tool is xdc.tools.path and the graphical tool is xdc.tools.path.sg.

By default, the path tool displays a list of all packages found in the repositories referenced by the package path.

For example, output for the xdc.tools.cdoc.sg package is similar to this:

Package Name: xdc.tools.cdoc.sg
Repository: C:\xdc_2_94_01\packages
Release Name: xdc_tools_cdoc_sg
Label: default
Compatibility Key: 1, 0, 0, 62
Date: 04/25/2007 19:07

The following command-line options are available:

-n
Display only the names of the packages.
-p
Echo only the current package path.
-d
Display information about the packages in the specified repository
only. For example:
xs xdc.tools.path -d C:/CCStudio_v3.3/bios_5_31/packages

See also

Command - xdc.tools.path.sg Interactive Package Path browser tool
xdc.tools.path Client documentation for xdc.tools.path

[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference