The information in this interface is read-only, defined by the chip's
data sheet, and is obtained by naming a module in a package that
implements this interface.
Data sheets are created by platforms as part of creating an "execution
context" (see
xdc.platform.IPlatform.getExeContext). This
execution context includes the CPU's memory map as well as any external
memory provided by the platform itself, for example.
per-instance config parameters |
|
XDCscript usage |
meta-domain |
var params = new ICpuDataSheet.Params;
// Instance config-params object
params.cpuCore = String undefined;
// A string identifying the CPU Core
params.cpuCoreRevision = String undefined;
// A string that uniquely identifies a revision of the core
params.dataWordSize = Int undefined;
// The size of an int on the target in 8-bit bytes
params.minDataUnitSize = Int undefined;
// The minimum addressable data unit size in 8-bit bytes
params.minProgUnitSize = Int undefined;
// The minimum addressable program unit size in 8-bit bytes
config ICpuDataSheet.cpuCore // per-instance |
|
A string identifying the CPU Core
DETAILS
This uniquely identifies the instruction set that the CPU can
decode and execute.
config ICpuDataSheet.cpuCoreRevision // per-instance |
|
A string that uniquely identifies a revision of the core
config String cpuCoreRevision;
config ICpuDataSheet.dataWordSize // per-instance |
|
The size of an int on the target in 8-bit bytes
config ICpuDataSheet.minDataUnitSize // per-instance |
|
The minimum addressable data unit size in 8-bit bytes
config Int minDataUnitSize;
config ICpuDataSheet.minProgUnitSize // per-instance |
|
The minimum addressable program unit size in 8-bit bytes
config Int minProgUnitSize;
per-instance creation |
|
create( String revision );
// Create an instance-object
ARGUMENTS
revision
a string that identifies revision of the CPU to be
created.
DETAILS
A "data sheet" for a CPU allows one to get specific attributes
for a CPU programatically; e.g., the memory map of the CPU.
Notice that we don't specify CPU registers when we create a
a data-sheet; registers are provided as necessary to the other
functions defined in this interface. This allows one to more easily
get memory maps for several different setting of the registers,
for example.
ICpuDataSheet.getMemoryMap( ) // per-instance |
|
Get the memory map that corresponds to the values of the specified
registers
function getMemoryMap( registers );
ARGUMENTS
registers
a hash of named registers to values at the time
an executable is to be loaded (for example)
DETAILS
If a register is not specified and this register can affect the
memory map, the register is assumed to be set to its reset
value (the value of the register immediately after a CPU reset).
RETURNS
Returns an array of
xdc.platform.IPlatform.Memory
objects that represent the memory visible to an
executable running on the CPU.
ICpuDataSheet.getRegisterSet( ) // per-instance |
|
The set of valid register names for this CPU
function getRegisterSet( );
DETAILS
This function returns the complete set of register names that may be
passed to the
getMemoryMap() function. This function is
only used to enable one to write a "requires contract" for the
getMemoryMap() function.
RETURNS
Returns an array of valid register names (strings) for
this device; only names from this array are valid keys
for the registers argument to
getMemoryMap().