module xdc.runtime.knl.SyncSemThread

A ISync implementation based on a SemThread. [EXPERIMENTAL]

This module implements the ti.sdo.utils.ISync interface using the xdc.runtime.knl.SemThread module.
XDCspec summary sourced in xdc/runtime/knl/SyncSemThread.xdc
module SyncSemThread {  ...
    // inherits xdc.runtime.IModule
instance:  ...
C synopsis target-domain
#include <xdc/runtime/knl/SyncSemThread.h>
module-wide constants & types
 
module-wide built-ins
per-instance object types
 
per-instance config parameters
        IInstance_Params *instance;
 
per-instance creation
per-instance deletion
per-instance functions
per-instance convertors
per-instance built-ins
 
XDCscript usage meta-domain
var SyncSemThread = xdc.useModule('xdc.runtime.knl.SyncSemThread');
module-wide constants & types
 
        const SyncSemThread.WaitStatus_ERROR;
        const SyncSemThread.WaitStatus_TIMEOUT;
        const SyncSemThread.WaitStatus_SUCCESS;
module-wide config parameters
per-instance config parameters
    var params = new SyncSemThread.Params// Instance config-params object;
per-instance creation
    var inst = SyncSemThread.create// Create an instance-object( params );
 
XDCspec declarations sourced in xdc/runtime/knl/SyncSemThread.xdc
package xdc.runtime.knl;
 
module SyncSemThread inherits ISync {
module-wide constants & types
    const UInt NO_WAIT// Used to specify no waiting = 0;
    const Int Q_BLOCKING// Blocking quality = 1;
    const UInt WAIT_FOREVER// Used to wait forever = ~(0);
 
        WaitStatus_ERROR,
        WaitStatus_TIMEOUT,
        WaitStatus_SUCCESS
    };
module-wide config parameters
 
 
instance:
per-instance creation
per-instance functions
    Bool query// Query for a particular quality( Int qual );
}
 
const SyncSemThread.NO_WAIT

Used to specify no waiting

XDCscript usage meta-domain
const SyncSemThread.NO_WAIT = 0;
C synopsis target-domain
#define SyncSemThread_NO_WAIT (UInt)0
 
 
const SyncSemThread.Q_BLOCKING

Blocking quality

XDCscript usage meta-domain
const SyncSemThread.Q_BLOCKING = 1;
C synopsis target-domain
#define SyncSemThread_Q_BLOCKING (Int)1
 
DETAILS
Implementations with this "quality" may cause the calling thread to block;
 
const SyncSemThread.WAIT_FOREVER

Used to wait forever

XDCscript usage meta-domain
const SyncSemThread.WAIT_FOREVER = ~(0);
C synopsis target-domain
#define SyncSemThread_WAIT_FOREVER (UInt)~(0)
 
 
enum SyncSemThread.WaitStatus

Error codes returned by Semaphore_pend

XDCscript usage meta-domain
values of type SyncSemThread.WaitStatus
    const SyncSemThread.WaitStatus_ERROR;
    const SyncSemThread.WaitStatus_TIMEOUT;
    const SyncSemThread.WaitStatus_SUCCESS;
C synopsis target-domain
typedef enum SyncSemThread_WaitStatus {
    SyncSemThread_WaitStatus_ERROR,
    SyncSemThread_WaitStatus_TIMEOUT,
    SyncSemThread_WaitStatus_SUCCESS
} SyncSemThread_WaitStatus;
 
 
metaonly config SyncSemThread.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
SyncSemThread.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
module-wide built-ins

C synopsis target-domain
Types_ModuleId SyncSemThread_Module_id( );
// Get this module's unique id
 
Bool SyncSemThread_Module_startupDone( );
// Test if this module has completed startup
 
IHeap_Handle SyncSemThread_Module_heap( );
// The heap from which this module allocates memory
 
Bool SyncSemThread_Module_hasMask( );
// Test whether this module has a diagnostics mask
 
Bits16 SyncSemThread_Module_getMask( );
// Returns the diagnostics mask for this module
 
Void SyncSemThread_Module_setMask( Bits16 mask );
// Set the diagnostics mask for this module
 
per-instance object types

C synopsis target-domain
typedef struct SyncSemThread_Object SyncSemThread_Object;
// Opaque internal representation of an instance object
 
typedef SyncSemThread_Object *SyncSemThread_Handle;
// Client reference to an instance object
 
typedef struct SyncSemThread_Struct SyncSemThread_Struct;
// Opaque client structure large enough to hold an instance object
 
SyncSemThread_Handle SyncSemThread_handle( SyncSemThread_Struct *structP );
// Convert this instance structure pointer into an instance handle
 
SyncSemThread_Struct *SyncSemThread_struct( SyncSemThread_Handle handle );
// Convert this instance handle into an instance structure pointer
 
per-instance config parameters

XDCscript usage meta-domain
var params = new SyncSemThread.Params;
// Instance config-params object
C synopsis target-domain
typedef struct SyncSemThread_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
} SyncSemThread_Params;
 
Void SyncSemThread_Params_init( SyncSemThread_Params *params );
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
per-instance creation

XDCscript usage meta-domain
var params = new SyncSemThread.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = SyncSemThread.create( params );
// Create an instance-object
C synopsis target-domain
SyncSemThread_Handle SyncSemThread_create( const SyncSemThread_Params *params, Error_Block *eb );
// Allocate and initialize a new instance object and return its handle
 
Void SyncSemThread_construct( SyncSemThread_Struct *structP, const SyncSemThread_Params *params, Error_Block *eb );
// Initialize a new instance object inside the provided structure
ARGUMENTS
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
 
per-instance deletion

C synopsis target-domain
Void SyncSemThread_delete( SyncSemThread_Handle *handleP );
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void SyncSemThread_destruct( SyncSemThread_Struct *structP );
// Finalize the instance object inside the provided structure
 
SyncSemThread.query( )  // per-instance

Query for a particular quality

C synopsis target-domain
Bool SyncSemThread_query( SyncSemThread_Handle handle, Int qual );
 
ARGUMENTS
handle — handle of a previously-created SyncSemThread instance object
qual — quality
RETURNS
TRUE or FALSE.
DETAILS
FALSE is returned if quality not supported.
 
SyncSemThread.signal( )  // per-instance

Called at completion of an activity

C synopsis target-domain
Void SyncSemThread_signal( SyncSemThread_Handle handle );
 
ARGUMENTS
handle — handle of a previously-created SyncSemThread instance object
DETAILS
This function is non-blocking. It is also required that the underlying sync be binary in nature.
This function does not take an Error.Block intentionally because it can be called from ISR context.
 
SyncSemThread.wait( )  // per-instance

Called to wait/poll for completion of an activity

C synopsis target-domain
Int SyncSemThread_wait( SyncSemThread_Handle handle, UInt timeout, Error_Block *eb );
 
ARGUMENTS
handle — handle of a previously-created SyncSemThread instance object
timeout — Timeout
eb — Hist Pointer to Error.Block
RETURNS
Refer to description above
DETAILS
This function can block. Non-blocking implementations should return false to indicate a timeout.
 
per-instance convertors

C synopsis target-domain
ISync_Handle SyncSemThread_Handle_upCast( SyncSemThread_Handle handle );
// unconditionally move one level up the inheritance hierarchy
 
SyncSemThread_Handle SyncSemThread_Handle_downCast( ISync_Handle handle );
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
per-instance built-ins

C synopsis target-domain
Int SyncSemThread_Object_count( );
// The number of statically-created instance objects
 
SyncSemThread_Handle SyncSemThread_Object_get( SyncSemThread_Object *array, Int i );
// The handle of the i-th statically-created instance object (array == NULL)
 
SyncSemThread_Handle SyncSemThread_Object_first( );
// The handle of the first dynamically-created instance object, or NULL
 
SyncSemThread_Handle SyncSemThread_Object_next( SyncSemThread_Handle handle );
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle SyncSemThread_Object_heap( );
// The heap used to allocate dynamically-created instance objects
 
Types_Label *SyncSemThread_Handle_label( SyncSemThread_Handle handle, Types_Label *buf );
// The label associated with this instance object
 
String SyncSemThread_Handle_name( SyncSemThread_Handle handle );
// The name of this instance object
generated on Fri, 09 Oct 2009 20:09:14 GMT