interface xdc.runtime.knl.ISemaphore |
|
|
|
Interface implemented by all front-end semaphore providers.
SemThread and SemProcess. [EXPERIMENTAL]
Semaphores can be used for synchronization and mutual exclusion.
[
more ... ]
interface ISemaphore { ...
instance: ...
interface ISemaphore {
module-wide constants & types
};
};
module-wide config parameters
instance:
per-instance config parameters
per-instance functions
}
#include <xdc/runtime/knl/ISemaphore.h>
per-instance object types
per-instance config parameters
DETAILS
Semaphores can be used for synchronization and mutual exclusion.
pend() is used to wait for a semaphore. The timeout parameter allows the
caller to wait until a timeout, wait indefinitely, or not wait at all.
The return value indicates whether or not the wait was successful.
post() is used to signal a semaphore. If no thread is waiting on the
semaphore, then post() increments the semaphore count (for binary
semaphores, the count is always 0 or 1).
getCount() returns the count of the semaphore.
reset() sets the semaphore count to a given value. There should be no
threads waiting on the semaphore when reset() is called.
const ISemaphore.FOREVER |
|
Used as the timeout value to specify wait forever
const UInt FOREVER = ~(0);
enum ISemaphore.Mode |
|
Types of semaphores
enum Mode {
Mode_COUNTING,
// Counting semaphore
Mode_BINARY
// Binary Semaphore
};
enum ISemaphore.PendStatus |
|
Error codes returned by Semaphore_pend
enum PendStatus {
PendStatus_ERROR,
PendStatus_TIMEOUT,
PendStatus_SUCCESS
};
metaonly config ISemaphore.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
per-instance object types |
|
typedef struct ISemaphore_Object *ISemaphore_Handle;
// Client reference to an abstract instance object
per-instance config parameters |
|
XDCscript usage |
meta-domain |
var params = new ISemaphore.Params;
// Instance config-params object
// Semaphore mode. Default is COUNTING
typedef struct ISemaphore_Params {
// Instance config-params structure
// Common per-instance configs
// Semaphore mode. Default is COUNTING
} ISemaphore_Params;
config ISemaphore.mode // per-instance |
|
Semaphore mode. Default is COUNTING
DETAILS
When mode is BINARY , the semaphore has only two states, available
and unavailable. When mode is COUNTING, the semaphore keeps track of
number of times a semaphore is posted.
ISemaphore.pend( ) // per-instance |
|
Wait for the semaphore to become available
ARGUMENTS
timeout
timeout in microseconds
eb
error block
DETAILS
RETURNS
refer to description above
ISemaphore.post( ) // per-instance |
|
Increment the semaphore count
ARGUMENTS
eb
error block
RETURNS
true for success, false for error in error block
generated on Fri, 09 Oct 2009 20:09:13 GMT