module xdc.runtime.knl.Cache

Cache Module [EXPERIMENTAL]

The Cache module provide APIs to allow applications to maintain cache coherency. [ more ... ]
XDCspec summary sourced in xdc/runtime/knl/Cache.xdc
module Cache {  ...
// inherits xdc.runtime.IModule
C synopsis target-domain
XDCscript usage meta-domain
var Cache = xdc.useModule('xdc.runtime.knl.Cache');
local proxy modules
        Cache.Proxy.delegate$ = ICacheSupport.Module null
module-wide config parameters
 
XDCspec declarations sourced in xdc/runtime/knl/Cache.xdc
package xdc.runtime.knl;
 
module Cache {
local proxy modules
    proxy Proxy inherits ICacheSupport;
module-wide config parameters
module-wide functions
    Bool inv// Invalidate range of memory for all cache(s)( Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb );
    Bool wb// Writes back a range of memory from all cache(s)( Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb );
    Bool wbInv// Write back and invalidate range of memory( Ptr blockPtr, SizeT byteCnt, Bool wait, Error.Block *eb );
}
DETAILS
The Cache module provide APIs to allow applications to maintain cache coherency.
This module will use an OS specific delegate (back-end) to manipulate the cache. This module has a module wide config parameter Proxy which needs to be bound to an OS specific delegate before this module can be used.
Here is an example showing how the proxy is bound to an BIOS 6.x specific delegate var Cache = xdc.useModule('xdc.runtime.knl.Cache'); Cache.Proxy = xdc.useModule('ti.sysbios.xdcruntime.CacheSupport');
Typically the package containing the delegates have a Settings module that will bind all xdc.runtime.knl proxies. The following example sets up all the xdc.runtime.knl proxies.
xdc.useModule("ti.sysbios.xdcruntime.Settings");
 
proxy Cache.Proxy

ICacheSupport proxy

XDCscript usage meta-domain
Cache.Proxy = ICacheSupport.Module null
// some delegate module inheriting the ICacheSupport interface
    Cache.Proxy.delegate$ = ICacheSupport.Module null
    // explicit access to the currently bound delegate module
 
DETAILS
Cache will use this proxy to access the cache hardware using OS specific APIs.
 
metaonly config Cache.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
Cache.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
Cache.inv( )  // module-wide

Invalidate range of memory for all cache(s)

C synopsis target-domain
Bool Cache_inv( Ptr blockPtr, SizeT byteCnt, Bool wait, Error_Block *eb );
 
ARGUMENTS
blockPtr — start address of range to be invalidated
byteCnt — number of bytes to be invalidated
wait — wait until the operation is completed
eb — error block
DETAILS
Invalidate the range of memory within the specified starting address and byte count. The range of addresses operated on gets quantized to whole cache lines in each cache. All lines in range are invalidated for all cache types.
RETURNS
true for success; false for error.
 
Cache.wait( )  // module-wide

Wait for a previous cache operation to complete

C synopsis target-domain
Bool Cache_wait( Error_Block *eb );
 
ARGUMENTS
eb — error block
DETAILS
Wait for the cache wb/wbInv/inv operation to complete. A cache operation is not truly complete until it has worked its way through all buffering and all memory writes have landed in the source memory.
RETURNS
true for success; false for error.
 
Cache.wb( )  // module-wide

Writes back a range of memory from all cache(s)

C synopsis target-domain
Bool Cache_wb( Ptr blockPtr, SizeT byteCnt, Bool wait, Error_Block *eb );
 
ARGUMENTS
blockPtr — start address of range to be invalidated
byteCnt — number of bytes to be invalidated
wait — wait until the operation is completed
eb — error block
DETAILS
Writes back the range of memory within the specified starting address and byte count. The range of addresses operated on gets quantized to whole cache lines in each cache. All lines within the range are left valid in all caches and the data within the range will be written back to the source memory.
RETURNS
true for success; false for error.
 
Cache.wbInv( )  // module-wide

Write back and invalidate range of memory

C synopsis target-domain
Bool Cache_wbInv( Ptr blockPtr, SizeT byteCnt, Bool wait, Error_Block *eb );
 
ARGUMENTS
blockPtr — start address of range to be invalidated
byteCnt — number of bytes to be invalidated
wait — wait until the operation is completed
eb — error block
DETAILS
Writes back and invalidates the range of memory within the specified starting address and byte count. The range of addresses operated on gets quantized to whole cache lines in each cache. All lines within the range are written back to the source memory and then invalidated for all cache types.
RETURNS
true for success; false for error.
 
module-wide built-ins

C synopsis target-domain
Types_ModuleId Cache_Module_id( );
// Get this module's unique id
 
Bool Cache_Module_startupDone( );
// Test if this module has completed startup
 
IHeap_Handle Cache_Module_heap( );
// The heap from which this module allocates memory
 
Bool Cache_Module_hasMask( );
// Test whether this module has a diagnostics mask
 
Bits16 Cache_Module_getMask( );
// Returns the diagnostics mask for this module
 
Void Cache_Module_setMask( Bits16 mask );
// Set the diagnostics mask for this module
generated on Fri, 09 Oct 2009 20:09:13 GMT