Release instances define a container object that represents all files that
are part of a release of a package. A release may, for example, include
just the files necessary to support a particular ISA even though the
package as a whole can support multiple ISAs.
Each Release instance is realized as a tar file containing the files
that are part of a release of a package.
typedef Release.DescArray |
![](../../Arrow_up.png) |
An array of release descriptors
struct Release.Attrs |
![](../../Arrow_up.png) |
Optional Release attributes
XDCscript usage |
meta-domain |
var obj = new Release.Attrs;
obj.archiver = String ...
// "tar" or "zip"; defaults to "tar"
obj.compress = Bool ...
// if true, compress package archive
obj.exportDoc = Bool ...
// if true, export generated docs
obj.exportExe = Bool ...
// if true, export program executables
obj.exportCfg = Bool ...
// if true, export program cfg scripts
obj.exportSrc = Bool ...
// if true, export all package sources
obj.exportAll = Bool ...
// if true, export all files in package
obj.relScript = String ...
// release files post-processing script
obj.prefix = String ...
// prefix for name of install of archive
obj.label = String ...
// uninterpreted label for this release
FIELDS
exportCfg
If this field is set to true, configuration
scripts will be part of the release. If it is unspecified
(or set to null), program configuration scripts will not
be added to this release.
exportDoc
If this field is set to true, generated
documentation will be part of the release.
exportSrc
If this field is set to true, sources
used to produce object files will be part of the release.
If it is unspecified (or set to null), no sources will
be part of this release.
exportExe
If this field is set to true, executables
will be part of the release. If it is unspecified (or set
to null), executables will not be part of this release.
exportAll
If this field is set to true, all files
in this package that are not known to be generated are in
the release. If it is unspecified (or set to null), these
files will not be added to this release.
Note that the set of files specified by exportAll is
determined at the time the package's makefile is generated.
If one of these files is subsequently removed before the
release is built, the build of the release will fail; a file
required by the release no longer exists. If the file is
not really required for the release, you must trigger a
rebuild for the generated makefiles; either touch
package.bld or remove the generated makefile and re-build
the release.
relScript
If this field is non-null, the string names a
"release script" that is run to post-process the
files that are part of a release. Like
configuration scripts, the string names a script
file that is searched for first in the in package's
base directory, and then along the package path. See
Manifest for more information about release scripts
and what they can do.
label
This string allows one to "tag" each release with a
label that can be used by other tools to select appropriate
releases. For example, the label might contain customer names.
This label is not interpreted by the XDC tools. It is simply
recorded in the package's build model XML file
(
package/package.bld.xml) and retrieved via
xdc.bld.BuildEnvironment.getReleaseDescs()
prefix
This string allows one to "export" each release to a
location outside of the package. prefix is prepended
to the name of the release name to form the name of the
release archive.
For example, setting prefix to "../" implies that a
release named "exports/foo" generates an archive file named
foo.tar in the directory "../exports".
prefix must be a relative path that is relative to the
package's "base" directory; i.e., the directory containing the
package's specification file
package.xdc. If it is not
specified (or set to
null) the current setting of
xdc.bld.PackageContents.releasePrefix is used.
compress
If this field is set to true, the release
archive file will be compressed; otherwise, the
archive will not be compressed. Archives are compressed
via gzip; compressed archives are .tar.gz files.
archiver
This field names the archiver to use when creating a
release. Two archivers are currently supported:
"tar" and "zip". If the archiver is set to "zip"
the Attrs.compress field is implicitly set to
true.
DETAILS
Unspecified attributes are "inherited" from
xdc.bld.PackageContents.Attrs; i.e., if one of fields in
this structure is unspecified *and* this field's name matches a field
name in
xdc.bld.PackageContents.Attrs, then
this field's value defaults to the value in specified by
xdc.bld.PackageContents.attrs. This mechanism makes it
possible to establish package-wide default values for any of the
"inherited" attributes.
However, elements added to a release can "override" these attributes.
For example, when an executable is added to a release and the
executable's attributes specify
'exportSrc = false', the release
will not contain the executable's sources (even if the release's
attrs.exportSrc attribute is set to
true).
SEE
struct Release.Desc |
![](../../Arrow_up.png) |
A description of a release
XDCscript usage |
meta-domain |
var obj = new Release.Desc;
obj.name = String ...
// the name used to create the release
obj.aname = String ...
// the file name of the archive
obj.label = String ...
// the label given to the release
DETAILS
This structure provides information about a release that can be
used to select from multiple releases provided by a package.
SEE
per-instance config parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new Release.Params;
// Instance config-params object
// This instance's attributes
params.name = String undefined;
// The name of the release
params.otherFiles = String[] undefined;
// Additional files to add to this release
config Release.attrs // per-instance |
![](../../Arrow_up.png) |
This instance's attributes
XDCscript usage |
meta-domain |
var params = new Release.Params;
...
DETAILS
Unless explicitly specified, these attributes are "inherited" from
the package's attributes (
xdc.bld.PackageContents.attrs)
SEE
config Release.name // per-instance |
![](../../Arrow_up.png) |
The name of the release
XDCscript usage |
meta-domain |
var params = new Release.Params;
...
params.name = String undefined;
DETAILS
This name is the base name of the generated tar file containing all
files that make up the release. For example, if the name of the
release is "foo" then the file "foo.tar" (located in the same
directory as package.bld) is a tar file containing the release files.
Note that each package has at least one release defined, the default
release. The default release's name is the name of the package with
'.'s replaced with '_'s. For example, the default release name for
the package "foo.bar" is "foo_bar" and the generated tar file is
named "foo_bar.tar".
config Release.otherFiles // per-instance |
![](../../Arrow_up.png) |
Additional files to add to this release
XDCscript usage |
meta-domain |
var params = new Release.Params;
...
params.otherFiles = String[] undefined;
DETAILS
This is an array of arbitrary files that are to be included
in this release of the package.
Only those files that are not already directly (or indirectly) named
by adding programs or libraries to this release need to appear in
this array.