From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
FAQ-080713-9
How is the RTSC-Pedia organized, and what sorts of documents exist
Contents |
At its top-most level, the RTSC-Pedia comprises four major document binders which in turn hold the multiple dozens of documents and sub-documents available at this site:
- The documents in this binder address many of the why's, what's, and how's of RTSCbut from a "10,000 foot" perspective that does not necessarily expose many of the low-level details involved in using the XDCtools product for day-to-day RTSC programming tasks. Use these documents for overall orientation within the world of RTSC.
- The documents in this binder teach the core aspects of the RTSC programming modelbut from an "on-the-ground" perspective where programmer's can, if they wish, use the XDCtools product to build and execute live examples. Use these documents to systematically learn (new) programming idioms introduced within the world of RTSC.
- The documents in this binder pragmatically describe all facets of the XDCtools productfrom installation and getting-started to programming and trouble-shooting. Use these documents once you've downloaded XDCtools and have begun working with the product on a day-to-day basis.
- The documents in this binder systematically define each element bundled with the XDCtools productfrom basic commands to the most advanced aspect of the programming model. Use these documents as definitive references for programming capabilities introduced elsewhere.
See also
FAQ-080713-7 | If I'm only consuming RTSC content, what should I read next |
FAQ-080713-8 | I also want to produce RTSC content, what should I read next |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved