This logger processes log events as they are generated and routes
them through the
System_printf() function.
The final disposition of the log event is dependent on which system
provider has been assigned to the
System.SupportProxy configuration parameter.
Note that the log events are processed within the runtime context
of the
Log_write() or
Log_print() function
that generated the event. It is important to account for the processing
overhead and stack usage imposed on the runtime context. The cost of
this processing is defined by the implementation of the system provider.
Configuration example: The following XDC configuration statements
create a logger instance, assign it as the default logger for all
modules, and enable
USER1 logging in all modules of the package
my.pkg. See the
Diags.setMaskMeta() function
for details on specifying the module names.
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
var LoggerSysParams = new LoggerSys.Params();
Defaults.common$.logger = LoggerSys.create(LoggerSysParams);
Diags.setMaskMeta("my.pkg.%", Diags.USER1, Diags.RUNTIME_ON);
proxy LoggerSys.TimestampProxy |
![](../../Arrow_up.png) |
User supplied time-stamp proxy
XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
DETAILS
This proxy allows
LoggerSys to use a timestamp server different
from the server used by
xdc.runtime.Timestamp. However, if
not supplied by a user, this proxy defaults to whichever timestamp
server is used by
Timestamp.
metaonly config LoggerSys.common$ // module-wide |
![](../../Arrow_up.png) |
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
module-wide built-ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool LoggerSys_Module_startupDone( );
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LoggerSys_Module_hasMask( );
// Test whether this module has a diagnostics mask
Bits16 LoggerSys_Module_getMask( );
// Returns the diagnostics mask for this module
Void LoggerSys_Module_setMask( Bits16 mask );
// Set the diagnostics mask for this module
per-instance object types |
![](../../Arrow_up.png) |
typedef struct LoggerSys_Object LoggerSys_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct LoggerSys_Struct LoggerSys_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
per-instance config parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new LoggerSys.Params;
// Instance config-params object
typedef struct LoggerSys_Params {
// Instance config-params structure
// Common per-instance configs
} LoggerSys_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
per-instance creation |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params =
new LoggerSys.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = LoggerSys.create( params );
// Create an instance-object
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
The logger instance will route all log events it receives to
the
System.printf function.
per-instance deletion |
![](../../Arrow_up.png) |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
LoggerSys.write4( ) // per-instance |
![](../../Arrow_up.png) |
Process a log event with up to 4 arguments
ARGUMENTS
handle
handle of a previously-created LoggerSys instance object
evt
event to be logged
a1
arbitrary argument passed by caller
This parameter, along with a2, a3, and a4 are parameters
that are to be interpreted according to the message format string
associated with evt.
DETAILS
At the time this method is called,
evt encodes two values: the
module ID of the module that "triggered" a
Log.Event
and the
Log.EventId of the event. The module ID can
be obtained via
Types.getModuleId(evt)
and the event ID can be obtained via
Types.getEventId(evt).
The event ID can be used to compare against other known
Log.Events.
if (Log_getEventId(MY_EVENT) == Types_getEventId(evt)) {
:
}
The event ID value of
0 is used to indicate an event triggered
by a call to one of the
Log_print[0-6]
methods. These methods take a
format string rather than a
Log_Event argument and, as a result,
the event ID encoded in
evt is
0 and the parameter
a1 is
the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Types_EventId id = Types_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
SEE
LoggerSys.write8( ) // per-instance |
![](../../Arrow_up.png) |
Process a log event with up to 8 arguments
Void LoggerSys_write8(
LoggerSys_Handle handle,
Types_Event evt,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8 );
ARGUMENTS
handle
handle of a previously-created LoggerSys instance object
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
per-instance convertors |
![](../../Arrow_up.png) |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
per-instance built-ins |
![](../../Arrow_up.png) |
Int LoggerSys_Object_count( );
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object