metaonly interface xdc.platform.IExeContext

Execution environment interface between a platform and an executable

This interface describes the execution environment provided by a platform as seen by an executable on a particular CPU at the time it is loaded. [ more ... ]
XDCspec summary sourced in xdc/platform/IExeContext.xdc
metaonly interface IExeContext {  ...
instance:  ...
XDCspec declarations sourced in xdc/platform/IExeContext.xdc
DETAILS
This interface describes the execution environment provided by a platform as seen by an executable on a particular CPU at the time it is loaded.
Execution contexts are created by platforms via xdc.platform.IPlatform.getExeContext(). Execution contexts are created implicitly just prior to executing a program's configuration script. This execution context is made available to the configuration script as the global read-only Program.cpu configuration parameter; see xdc.cfg.Program.
 
struct IExeContext.Cpu

CPU attributes necessary to create an execution context

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
metaonly struct Cpu {
    String id;
    // unique id within the platform
    String catalogName;
    // name of catalog package
    String deviceName;
    // module name within catalog package
    String revision;
    // revision of specified device
    Float clockRate;
    // clock rate in MHz of CPU on board
};
 
DETAILS
Attributes that uniquely identify the CPU responsible for executing an executable image.
 
per-instance config parameters

XDCscript usage meta-domain
var params = new IExeContext.Params;
// Instance config-params object
    params.attrs = ICpuDataSheet.Instance undefined;
    // The CPU "data-sheet" attributes
    params.board = IPlatform.Board undefined;
    // The board-level attributes
    params.catalogName = String undefined;
    // The name of the package containing the module named by deviceName
    params.clockRate = Float undefined;
    // The clock rate in MHz of the CPU
    params.deviceName = String undefined;
    // The name of a CPU device within the catalog package catalogName
    params.id = String undefined;
    // The CPU's unique id within the platform
    params.memoryMap = IPlatform.Memory[string] undefined;
    // The memory map seen by executables at the time they are loaded
    params.revision = String "";
    // The revision of the CPU
 
config IExeContext.attrs  // per-instance

The CPU "data-sheet" attributes

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config ICpuDataSheet.Instance attrs;
 
DETAILS
This "data sheet" allows one to get information about the CPU that runs the run the executable associated with this execution context.
Multi-CPU platforms provide multiple execution contexts; each context is associated with a single CPU on the platform.
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.board  // per-instance

The board-level attributes

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
readonly config IPlatform.Board board;
 
DETAILS
This parameter defines the static attributes of the board containing the CPU that runs the executable.
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.catalogName  // per-instance

The name of the package containing the module named by deviceName

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config String catalogName;
 
DETAILS
This string names a package containing one or more modules that implements the xdc.platform.ICpuDataSheet interface.
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.clockRate  // per-instance

The clock rate in MHz of the CPU

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config Float clockRate;
 
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.deviceName  // per-instance

The name of a CPU device within the catalog package catalogName

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config String deviceName;
 
DETAILS
This string names a module in the catalog package, specified by catalogName, that represents the CPU that runs the executable; i.e., it implements the xdc.platform.ICpuDataSheet interface.
 
config IExeContext.id  // per-instance

The CPU's unique id within the platform

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config String id;
 
DETAILS
This id is the string used to identify a specific CPU within the platform that provides this execution context.
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.memoryMap  // per-instance

The memory map seen by executables at the time they are loaded

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config IPlatform.Memory memoryMap[string];
 
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
 
config IExeContext.revision  // per-instance

The revision of the CPU

XDCspec declarations sourced in xdc/platform/IExeContext.xdc
config String revision = "";
 
READONLY
This parameter is set by the platform and is readonly for configuration scripts.
generated on Sat, 01 Aug 2009 01:23:34 GMT