From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - Proxy-Object.delegate$
Module that implements the proxy's interface
Contents |
Synopsis
| var Mod = xdc.module("«moduleName»"); var ProxyMod = Mod.«ProxyName».delegate$; |
Description
The delegate$ property of a proxy object is the module that implements the interface provided by the proxy. This property is typically used to enable configuration script to set the underlying implementation module's configuration parameters.
Example
The following script disables the "entry" trace of the underlying implementation of the System.SupportProxy proxy.
| /* get the System module's SystemSupport proxy's implementing module */ var System = xdc.module("xdc.runtime.System"); var SupportMod = System.SupportProxy.delegate$; /* disable entry trace for this module */ var Diags = xdc.useModule("xdc.runtime.Diags"); SupportMod.common$.diags_ENTRY = Diags.ALWAYS_OFF; |