interface xdc.runtime.ILogger |
![](../../Arrow_left.png) |
![](../../Arrow_up.png) |
![](../../Arrow_right.png) |
Interface to service Log events
A logger is responsible for recording, transmitting, or otherwise
handling
Log Events generated by clients of the
Log module. The
Log module uses modules that implement the
ILogger interface to record the log events. Most application code will
use the
Log module instead of directly calling the specific
ILogger
module implementation.
[
more ... ]
interface ILogger { ...
instance: ...
interface ILogger {
module-wide config parameters
instance:
per-instance functions
}
#include <xdc/runtime/ILogger.h>
per-instance object types
per-instance config parameters
DETAILS
A logger is responsible for recording, transmitting, or otherwise
handling
Log Events generated by clients of the
Log module. The
Log module uses modules that implement the
ILogger interface to record the log events. Most application code will
use the
Log module instead of directly calling the specific
ILogger
module implementation.
All logger implementations must inherit from this interface. The
derived implementations must implement the functions defined in this
interface but may also add additional configuration parameters and
functions.
metaonly config ILogger.common$ // module-wide |
![](../../Arrow_up.png) |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
per-instance object types |
![](../../Arrow_up.png) |
typedef struct ILogger_Object *ILogger_Handle;
// Client reference to an abstract instance object
per-instance config parameters |
![](../../Arrow_up.png) |
XDCscript usage |
meta-domain |
var params = new ILogger.Params;
// Instance config-params object
typedef struct ILogger_Params {
// Instance config-params structure
// Common per-instance configs
} ILogger_Params;
ILogger.write4( ) // per-instance |
![](../../Arrow_up.png) |
Process a log event with up to 4 arguments
Void write4(
Types.Event evt,
IArg a1,
IArg a2,
IArg a3,
IArg a4 );
ARGUMENTS
evt
event to be logged
a1
arbitrary argument passed by caller
This parameter, along with a2, a3, and a4 are parameters
that are to be interpreted according to the message format string
associated with evt.
DETAILS
At the time this method is called,
evt encodes two values: the
module ID of the module that "triggered" a
Log.Event
and the
Log.EventId of the event. The module ID can
be obtained via
Types.getModuleId(evt)
and the event ID can be obtained via
Types.getEventId(evt).
The event ID can be used to compare against other known
Log.Events.
if (Log_getEventId(MY_EVENT) == Types_getEventId(evt)) {
:
}
The event ID value of
0 is used to indicate an event triggered
by a call to one of the
Log_print[0-6]
methods. These methods take a
format string rather than a
Log_Event argument and, as a result,
the event ID encoded in
evt is
0 and the parameter
a1 is
the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Types_EventId id = Types_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
SEE
ILogger.write8( ) // per-instance |
![](../../Arrow_up.png) |
Process a log event with up to 8 arguments
Void write8(
Types.Event evt,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8 );
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
generated on Thu, 25 Jun 2009 21:46:14 GMT