metaonly config Defaults.common$ // module-wide |
![](../../Arrow_up.png) |
Defaults inherited by all target modules
XDCscript usage |
meta-domain |
fxntab: true,
gate: null,
gateParams: null,
instanceHeap: null,
instanceSection: null,
logger: null,
namedInstance: false,
namedModule: true,
romPatchTable: false
};
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
This structure defines the default values for the configuration
parameters shared by all modules in a system. Unless otherwise
noted, setting one of the fields defined below will set the
corresponding value for all modules in the system which have not
been explicitly set; i.e., it will establish a default value for
the parameter.
DIAGS_ASSERT
Enables asserts at runtime. Default is ALWAYS_ON
DIAGS_ENTRY
Enables entry trace for all functions. Default is ALWAYS_OFF
DIAGS_EXIT
Enables exit trace for all functions. Default is ALWAYS_OFF
DIAGS_INTERNAL
Enables internal asserts. Default is ALWAYS_OFF. When set to
ALWAYS_ON, requires diags_ASSERT to be ALWAYS_ON.
DIAGS_LIFECYCLE
Enables lifecycle logs. These logs are written during creates
and deletes. Default is ALWAYS_OFF.
DIAGS_USER
Each diags_USER field controls a separate user-defined
logging level. Default is ALWAYS_OFF for all diags_USER fileds.
GATE
Default gate used by all modules which are declared as being
@Gated.
By default, this parameter points to an instance of
GateNull,
which means there is no protection.
GATEPARAMS
The default parameters used to create gates at runtime. See
Types.Common$.gateParams. Default is
null.
INSTANCEHEAP
Specify heap to be used for module instances. Default is
null.
If
instanceHeap is
null, instances will be allocated from
the heap specified by
Memory.defaultHeapInstance.
INSTANCESECTION
Specify section to be used to place module instances. Default is
null.
LOGGER
Default logger used by modules to write logs. By default there is
no logger.
MEMORYPOLICY
Used to specify type of application. Types.STATIC_POLICY is used when
all objects are created statically. Types.CREATE_POLICY is used when
the application creates objects at runtime. Types.DELETE_POLICY is
used when the application creates and deletes objects at runtime. This
helps eliminate unwanted create and delete code.
NAMEDINSTANCE
This parameter should be set to true if space needs to be allocated in
instance objects for instance names. Allocating space for a name
allows object view tools to display the names. The runtime functions
Mod_Handle_name() and Mod_Handle_label() defined for each module
Mod can be used to retrieve the name at runtime.
NAMEDMODULE
This field allows the name of the module to be retained on the target.
Setting this to false will save space but will also prevent
the target from being able to display the module names appearing
in Log events and Errors.
Setting
namedModule to
false causes all modules, except for
Memory and
Main to be unnamed by default. To
eliminate the string names for these modules you must explicitly
set their
common$.namedModule parameters to
false; without these
two names, target-side display of error messages is somewhat cryptic.
ROMPATCHTABLE
Specify whether modules that are allocated to ROM are patchable.
metaonly Defaults.getCommon( ) // module-wide |
![](../../Arrow_up.png) |
Get a specified common parameter from a module
XDCscript usage |
meta-domain |
ARGUMENTS
eb
module whose parameter is queried
param
string naming the queried parameter
DETAILS
Get the value of a member of the structure common$ based on
defaults and the current value of the parameter.
RETURNS
Returns the value of the parameter named param from the module
mod.
module-wide built-ins |
![](../../Arrow_up.png) |
// Get this module's unique id
Bool Defaults_Module_startupDone( );
// Test if this module has completed startup
// The heap from which this module allocates memory