![]() |
![]() |
Functions | |
int | Sock6New (int Family, int Type, int Protocol, int RxBufSize, int TxBufSize, HANDLE *phSock) |
int | Sock6Bind (HANDLE h, PSA pName) |
int | Sock6Recv (HANDLE h, char *pBuf, INT32 size, int flags, PSA pPeer, INT32 *pRetSize) |
int | Sock6Send (HANDLE h, char *pBuf, INT32 size, int flags, INT32 *pRetSize) |
int | Sock6Connect (HANDLE h, PSA pName) |
void | Sock6IntAbort (SOCK6 *ps) |
int | Sock6Close (HANDLE h) |
int | Sock6Disconnect (HANDLE h) |
int | Sock6Check (HANDLE h, int IoType) |
int | Sock6Status (HANDLE h, int request, int *results) |
int | Sock6Shutdown (HANDLE h, int how) |
int | Sock6GetName (HANDLE h, PSA pSockName, PSA pPeerName) |
int | Sock6Listen (HANDLE h, int maxcon) |
int | Sock6Accept (HANDLE h, HANDLE *phSock) |
int | Sock6Set (HANDLE hSock, int Type, int Prop, void *pbuf, int size) |
int | Sock6Get (HANDLE hSock, int Type, int Prop, void *pbuf, int *psize) |
int Sock6Accept | ( | HANDLE | h, | |
HANDLE * | phSock | |||
) |
Description
The function accepts connections on a socket which is listening for connections to arrive.
[in] | h | Socket Handle which is listening for connections. |
[out] | phSock | Socket Handle which is created after accepting the connection. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Bind | ( | HANDLE | h, | |
PSA | pName | |||
) |
Description
The function binds an address and port to the socket.
[in] | h | Socket Handle passed. |
[in] | pName | IPv6 Address and Port Information to which the socket will be bound. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Check | ( | HANDLE | h, | |
int | IoType | |||
) |
Description
The function is called to determine if there is any operation pending on the socket.
[in] | h | Socket Handle which needs to be checked. |
[in] | IoType | Type of operation which is pending. |
1 | - Operation is pending | |
0 | - Operation is not pending |
int Sock6Close | ( | HANDLE | h | ) |
Description
The function closes an IPv6 Socket.
[in] | h | Socket Handle which is to be closed. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Connect | ( | HANDLE | h, | |
PSA | pName | |||
) |
Description
The function connects the socket.
[in] | h | Socket Handle which is to be connected. |
[in] | pName | Socket Address Information to which the socket will be connected. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Disconnect | ( | HANDLE | h | ) |
Description
The function disconnects an IPv6 Socket. This is not the same as close; since the socket is not cleaned up.
[in] | h | Socket Handle which is to be disconnected. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Get | ( | HANDLE | hSock, | |
int | Type, | |||
int | Prop, | |||
void * | pbuf, | |||
int * | psize | |||
) |
Description
The function is used to get the socket parameters
[in] | hSock | Handle to the socket. |
[in] | Type | Socket Level which is to be configured.
|
[in] | Prop | The Property which needs to be configured. |
[out] | pbuf | Data buffer where the value of property will be stored. |
[out] | psize | Size of the Data buffer |
Success | - 0 | |
Error | - Non Zero |
int Sock6GetName | ( | HANDLE | h, | |
PSA | pSockName, | |||
PSA | pPeerName | |||
) |
Description
The function gets information about the Local and Peer to which the socket has been connected.
[in] | h | Socket Handle for which the information is required. |
[out] | pSockName | Local Information is populated in this. |
[out] | pPeerName | Peer Information is populated in this. |
Always | returns 0. |
void Sock6IntAbort | ( | SOCK6 * | ps | ) |
Description
The function cleans up the internal memory for the V6 Socket.
[in] | ps | Pointer to the SOCK6 Object which will be cleaned up. |
Not | Applicable. |
int Sock6Listen | ( | HANDLE | h, | |
int | maxcon | |||
) |
Description
The function listens on STREAM sockets waiting for connections to arrive
[in] | h | Socket Handle on which connections are being listened for. |
[in] | maxcon | Maximum number of connections that can be accepted. |
Success | - 0 | |
Error | - Non Zero |
int Sock6New | ( | int | Family, | |
int | Type, | |||
int | Protocol, | |||
int | RxBufSize, | |||
int | TxBufSize, | |||
HANDLE * | phSock | |||
) |
Description
The function creates a new IPv6 Socket.
[in] | Family | Socket Family. Only AF_INET6 is supported. |
[in] | Type | The type of socket being created
|
[in] | Protocol | Valid Values are 0, IPPROTO_UDP and IPPROTO_TCP. |
[in] | RxBufSize | Receive buffer size of the V6 Socket. |
[in] | TxBufSize | Transmit buffer size of the V6 Socket. |
[out] | phSock | Socket Handle which is returned. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Recv | ( | HANDLE | h, | |
char * | pBuf, | |||
INT32 | size, | |||
int | flags, | |||
PSA | pPeer, | |||
INT32 * | pRetSize | |||
) |
Description
The function receives data from a socket.
[in] | h | Socket Handle from where data has to be read. |
[in] | pBuf | Data Buffer where data has to be copied after it is read from the socket. |
[in] | size | Size of the data buffer passed. |
[in] | flags | Flags |
[in] | pPeer | Peer Information from where the packet was received. |
[in] | pRetSize | Total number of data bytes actually received. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Send | ( | HANDLE | h, | |
char * | pBuf, | |||
INT32 | size, | |||
int | flags, | |||
INT32 * | pRetSize | |||
) |
Description
The function send data out from a socket.
[in] | h | Socket Handle from where data has to be send out |
[in] | pBuf | Data Buffer which contains the data to be sent out. |
[in] | size | Size of the data buffer passed. |
[in] | flags | Flags |
[in] | pRetSize | Total number of data bytes actually sent out. |
Success | - 0 | |
Error | - Non Zero |
int Sock6Set | ( | HANDLE | hSock, | |
int | Type, | |||
int | Prop, | |||
void * | pbuf, | |||
int | size | |||
) |
Description
The function is used to set the socket parameters
[in] | hSock | Handle to the socket. |
[in] | Type | Socket Level which is to be configured.
|
[in] | Prop | The Property which needs to be configured. |
[in] | pbuf | Data buffer where the value of property is present |
[in] | size | Size of the Data buffer |
Success | - 0 | |
Error | - Non Zero |
int Sock6Shutdown | ( | HANDLE | h, | |
int | how | |||
) |
Description
The function shuts down the V6 socket.
[in] | h | Socket Handle which is to be shutdown. |
[out] | how |
|
Always | returns 0. |
int Sock6Status | ( | HANDLE | h, | |
int | request, | |||
int * | results | |||
) |
Description
The function returns the socket status.
[in] | h | Socket Handle which needs to be checked. |
[in] | request | Type of request |
[out] | results | Result buffer which has the result of the request. |
Success | - 0 | |
Error | - Non Zero |