![]() |
![]() |
TI-RTOS Drivers
tidrivers_full_2_20_01_10
|
SDSPIUSCIA Hardware attributes. More...
#include <SDSPIUSCIA.h>
Data Fields | |
uint32_t | baseAddr |
uint8_t | clockSource |
uint8_t | portSCK |
uint32_t | pinSCK |
uint8_t | portMISO |
uint32_t | pinMISO |
uint8_t | portMOSI |
uint32_t | pinMOSI |
uint8_t | portCS |
uint32_t | pinCS |
SDSPIUSCIA Hardware attributes.
The SDSPIUSCIA configuration structure describes to the SDSPIUSCIA driver implementation hardware specifies on which SPI peripheral, GPIO Pins and Ports are to be used.
The SDSPIUSCIA driver uses this information to:
These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For TivaWare these definitions are found in:
An example configuration structure could look as the following:
uint32_t SDSPIUSCIA_HWAttrs::baseAddr |
SPI Peripheral's base address
uint8_t SDSPIUSCIA_HWAttrs::clockSource |
SPIUSCI Clock source
uint8_t SDSPIUSCIA_HWAttrs::portSCK |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIA_HWAttrs::pinSCK |
SPI SCK pin
uint8_t SDSPIUSCIA_HWAttrs::portMISO |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIA_HWAttrs::pinMISO |
SPI MISO pin
uint8_t SDSPIUSCIA_HWAttrs::portMOSI |
SPI port uses for the SCK, MISO, and MOSI pins
uint32_t SDSPIUSCIA_HWAttrs::pinMOSI |
SPI MOSI pin
uint8_t SDSPIUSCIA_HWAttrs::portCS |
GPIO Port used for the chip select
uint32_t SDSPIUSCIA_HWAttrs::pinCS |
GPIO Pin used for the chip select