![]() |
![]() |
TI-RTOS Drivers
tidrivers_full_2_20_01_10
|
Power global configuration. More...
#include <PowerCC3200.h>
Data Fields | |
Power_PolicyInitFxn | policyInitFxn |
Power_PolicyFxn | policyFxn |
void(* | enterLPDSHookFxn )(void) |
Hook function called before entering LPDS. More... | |
void(* | resumeLPDSHookFxn )(void) |
Hook function called when resuming from LPDS. More... | |
bool | enablePolicy |
bool | enableGPIOWakeupLPDS |
bool | enableGPIOWakeupShutdown |
bool | enableNetworkWakeupLPDS |
uint32_t | wakeupGPIOSourceLPDS |
The GPIO source for wakeup from LPDS. More... | |
uint32_t | wakeupGPIOTypeLPDS |
The GPIO trigger type for wakeup from LPDS. More... | |
void(* | wakeupGPIOFxnLPDS )(unsigned int argument) |
Function to be called when the configured GPIO triggers wakeup from LPDS. More... | |
unsigned int | wakeupGPIOFxnLPDSArg |
The argument to be passed to wakeupGPIOFxnLPDS() More... | |
uint32_t | wakeupGPIOSourceShutdown |
The GPIO sources for wakeup from shutdown. More... | |
uint32_t | wakeupGPIOTypeShutdown |
The GPIO trigger type for wakeup from shutdown. More... | |
uint32_t | ramRetentionMaskLPDS |
SRAM retention mask for LPDS. More... | |
bool | keepDebugActiveDuringLPDS |
Keep debug interface active during LPDS. More... | |
uint32_t | ioRetentionShutdown |
IO retention mask for Shutdown. More... | |
PowerCC3200_ParkInfo * | pinParkDefs |
Pointer to an array of pins to be parked during LPDS. More... | |
uint32_t | numPins |
Number of pins to be parked during LPDS. More... | |
Power global configuration.
Power_PolicyInitFxn PowerCC3200_ConfigV1::policyInitFxn |
Init function for power policy
Power_PolicyFxn PowerCC3200_ConfigV1::policyFxn |
The power policy function
void(* PowerCC3200_ConfigV1::enterLPDSHookFxn) (void) |
Hook function called before entering LPDS.
This function is called after any notifications are complete, and before any pins are parked, just before entry to LPDS.
void(* PowerCC3200_ConfigV1::resumeLPDSHookFxn) (void) |
Hook function called when resuming from LPDS.
This function is called early in the wake sequence, before any notification functions are run.
bool PowerCC3200_ConfigV1::enablePolicy |
Determines whether to run the power policy function
bool PowerCC3200_ConfigV1::enableGPIOWakeupLPDS |
Enable GPIO as a wakeup source for LPDS
bool PowerCC3200_ConfigV1::enableGPIOWakeupShutdown |
Enable GPIO as a wakeup source for shutdown
bool PowerCC3200_ConfigV1::enableNetworkWakeupLPDS |
Enable Network activity as a wakeup source for LPDS
uint32_t PowerCC3200_ConfigV1::wakeupGPIOSourceLPDS |
The GPIO source for wakeup from LPDS.
Only one of the following GPIOs {2,4,11,13,17,24,26} can be the wakeup source for LPDS. The following values are taken from the driverlib prcm.h file.
Value can be one of the following (defined in driverlib/prcm.h): PRCM_LPDS_GPIO2, PRCM_LPDS_GPIO4, PRCM_LPDS_GPIO11, PRCM_LPDS_GPIO13, PRCM_LPDS_GPIO17, PRCM_LPDS_GPIO24, PRCM_LPDS_GPIO26
uint32_t PowerCC3200_ConfigV1::wakeupGPIOTypeLPDS |
The GPIO trigger type for wakeup from LPDS.
Value can be one of the following (defined in driverlib/prcm.h): PRCM_LPDS_LOW_LEVEL, PRCM_LPDS_HIGH_LEVEL, PRCM_LPDS_FALL_EDGE, PRCM_LPDS_RISE_EDGE
void(* PowerCC3200_ConfigV1::wakeupGPIOFxnLPDS) (unsigned int argument) |
Function to be called when the configured GPIO triggers wakeup from LPDS.
During LPDS the internal GPIO module is powered off, and special periphery logic is used instead to detect the trigger and wake the device. No GPIO interrupt service routine will be triggered in this case (even if an ISR is configured, and used normally to detect GPIO interrupts when not in LPDS). This function can be used in lieu of a GPIO ISR, to take specific action upon LPDS wakeup.
A value of NULL indicates no GPIO wakeup function will be called.
An argument for this wakeup function can be specified via wakeupGPIOFxnLPDSArg.
Note that this wakeup function will be called as one of the last steps in Power_sleep(), after all notifications have been sent out, and after pins have been restored to their previous (non-parked) states.
unsigned int PowerCC3200_ConfigV1::wakeupGPIOFxnLPDSArg |
The argument to be passed to wakeupGPIOFxnLPDS()
uint32_t PowerCC3200_ConfigV1::wakeupGPIOSourceShutdown |
The GPIO sources for wakeup from shutdown.
Any one of the following GPIOs {2,4,11,13,17,24,26} can be a wakeup source for shutdown. The following values are taken from the driverlib prcm.h file
Value can be one or more of the following (defined in driverlib/prcm.h): PRCM_HIB_GPIO2, PRCM_HIB_GPIO4, PRCM_HIB_GPIO11, PRCM_HIB_GPIO13, PRCM_HIB_GPIO17, PRCM_HIB_GPIO24, PRCM_HIB_GPIO26
uint32_t PowerCC3200_ConfigV1::wakeupGPIOTypeShutdown |
The GPIO trigger type for wakeup from shutdown.
Value can be one of the following (defined in driverlib/prcm.h): PRCM_HIB_LOW_LEVEL, PRCM_HIB_HIGH_LEVEL, PRCM_HIB_FALL_EDGE, PRCM_HIB_RISE_EDGE
uint32_t PowerCC3200_ConfigV1::ramRetentionMaskLPDS |
SRAM retention mask for LPDS.
Value can be a mask of the following (defined in driverlib/prcm.h): PRCM_SRAM_COL_1, PRCM_SRAM_COL_2, PRCM_SRAM_COL_3, PRCM_SRAM_COL_4
bool PowerCC3200_ConfigV1::keepDebugActiveDuringLPDS |
Keep debug interface active during LPDS.
This Boolean controls whether the debug interface will be left active when LPDS is entered. For best power savings this flag should be set to false. Setting the flag to true will enable better debug capability, but will prevent full LPDS, and will result in increased power consumption.
uint32_t PowerCC3200_ConfigV1::ioRetentionShutdown |
IO retention mask for Shutdown.
Value can be a mask of the following (defined in driverlib/prcm.h): PRCM_IO_RET_GRP_0, PRCM_IO_RET_GRP_1, PRCM_IO_RET_GRP_2 PRCM_IO_RET_GRP_3
PowerCC3200_ParkInfo* PowerCC3200_ConfigV1::pinParkDefs |
Pointer to an array of pins to be parked during LPDS.
A value of NULL will disable parking of any pins during LPDS
uint32_t PowerCC3200_ConfigV1::numPins |
Number of pins to be parked during LPDS.