![]() |
![]() |
TI-RTOS Drivers
tidrivers_full_2_20_01_10
|
![]() |
Macros | |
#define | I2C_STATUS_SUCCESS 0 |
Successful status code returned by I2C_control(). More... | |
#define | I2C_STATUS_ERROR -1 |
Generic error status code returned by I2C_control(). More... | |
#define | I2C_STATUS_UNDEFINEDCMD -2 |
An error status code returned by I2C_control() for undefined command codes. More... | |
I2C_STATUS_* macros are general status codes returned by I2C_control()
I2CCC26XX_STATUS_* macros are command codes only defined in the I2CCC26XX.h driver implementation and need to:
I2CCC3200_STATUS_* macros are command codes only defined in the I2CCC3200.h driver implementation and need to:
I2CEUSCIB_STATUS_* macros are command codes only defined in the I2CEUSCIB.h driver implementation and need to:
I2CMSP432_STATUS_* macros are command codes only defined in the I2CMSP432.h driver implementation and need to:
I2CTiva_STATUS_* macros are command codes only defined in the I2CTiva.h driver implementation and need to:
I2CUSCIB_STATUS_* macros are command codes only defined in the I2CUSCIB.h driver implementation and need to:
#define I2C_STATUS_SUCCESS 0 |
Successful status code returned by I2C_control().
I2C_control() returns I2C_STATUS_SUCCESS if the control code was executed successfully.
#define I2C_STATUS_ERROR -1 |
Generic error status code returned by I2C_control().
I2C_control() returns I2C_STATUS_ERROR if the control code was not executed successfully.
#define I2C_STATUS_UNDEFINEDCMD -2 |
An error status code returned by I2C_control() for undefined command codes.
I2C_control() returns I2C_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.