![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_20_00_08
|
I2CCC26XX Hardware attributes. More...
#include <I2CCC26XX.h>
Data Fields | |
I2CBaseAddrType | baseAddr |
unsigned long | powerMngrId |
int | intNum |
uint8_t | intPriority |
I2C Peripheral's interrupt priority. More... | |
uint32_t | swiPriority |
I2C SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file. More... | |
uint8_t | sdaPin |
uint8_t | sclPin |
I2CCC26XX Hardware attributes.
These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For cc26xxware these definitions are found in:
intPriority is the I2C peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities.
A sample structure is shown below:
I2CBaseAddrType I2CCC26XX_HWAttrsV1::baseAddr |
I2C Peripheral's base address
unsigned long I2CCC26XX_HWAttrsV1::powerMngrId |
I2C Peripheral's power manager ID
int I2CCC26XX_HWAttrsV1::intNum |
I2C Peripheral's interrupt vector
uint8_t I2CCC26XX_HWAttrsV1::intPriority |
I2C Peripheral's interrupt priority.
The CC26xx uses three of the priority bits, meaning ~0 has the same effect as (7 << 5).
(7 << 5) will apply the lowest priority.
(1 << 5) will apply the highest priority.
Setting the priority to 0 is not supported by this driver.
HWI's with priority 0 ignore the HWI dispatcher to support zero-latency interrupts, thus invalidating the critical sections in this driver.
uint32_t I2CCC26XX_HWAttrsV1::swiPriority |
I2C SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is 15 by default. The maximum can be reduced to save RAM by adding or modifying Swi.numPriorities in the kernel configuration file.
uint8_t I2CCC26XX_HWAttrsV1::sdaPin |
I2C SDA pin mapping
uint8_t I2CCC26XX_HWAttrsV1::sclPin |
I2C SCL pin mapping