CC26xx Driver Library
uart.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: uart.c
3 * Revised: 2015-11-16 19:41:47 +0100 (Mon, 16 Nov 2015)
4 * Revision: 45094
5 *
6 * Description: Driver for the UART.
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/uart.h>
40 
41 //*****************************************************************************
42 //
43 // Handle support for DriverLib in ROM:
44 // This section will undo prototype renaming made in the header file
45 //
46 //*****************************************************************************
47 #if !defined(DOXYGEN)
48  #undef UARTFIFOLevelGet
49  #define UARTFIFOLevelGet NOROM_UARTFIFOLevelGet
50  #undef UARTConfigSetExpClk
51  #define UARTConfigSetExpClk NOROM_UARTConfigSetExpClk
52  #undef UARTConfigGetExpClk
53  #define UARTConfigGetExpClk NOROM_UARTConfigGetExpClk
54  #undef UARTDisable
55  #define UARTDisable NOROM_UARTDisable
56  #undef UARTCharGetNonBlocking
57  #define UARTCharGetNonBlocking NOROM_UARTCharGetNonBlocking
58  #undef UARTCharGet
59  #define UARTCharGet NOROM_UARTCharGet
60  #undef UARTCharPutNonBlocking
61  #define UARTCharPutNonBlocking NOROM_UARTCharPutNonBlocking
62  #undef UARTCharPut
63  #define UARTCharPut NOROM_UARTCharPut
64  #undef UARTIntRegister
65  #define UARTIntRegister NOROM_UARTIntRegister
66  #undef UARTIntUnregister
67  #define UARTIntUnregister NOROM_UARTIntUnregister
68 #endif
69 
70 //*****************************************************************************
71 //
73 //
74 //*****************************************************************************
75 void
76 UARTFIFOLevelGet(uint32_t ui32Base, uint32_t *pui32TxLevel,
77  uint32_t *pui32RxLevel)
78 {
79  uint32_t ui32Temp;
80 
81  //
82  // Check the arguments.
83  //
84  ASSERT(UARTBaseValid(ui32Base));
85 
86  //
87  // Read the FIFO level register.
88  //
89  ui32Temp = HWREG(ui32Base + UART_O_IFLS);
90 
91  //
92  // Extract the transmit and receive FIFO levels.
93  //
94  *pui32TxLevel = ui32Temp & UART_IFLS_TXSEL_M;
95  *pui32RxLevel = ui32Temp & UART_IFLS_RXSEL_M;
96 }
97 
98 //*****************************************************************************
99 //
101 //
102 //*****************************************************************************
103 void
104 UARTConfigSetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk,
105  uint32_t ui32Baud, uint32_t ui32Config)
106 {
107  uint32_t ui32Div;
108 
109  //
110  // Check the arguments.
111  //
112  ASSERT(UARTBaseValid(ui32Base));
113  ASSERT(ui32Baud != 0);
114 
115  //
116  // Stop the UART.
117  //
118  UARTDisable(ui32Base);
119 
120  //
121  // Compute the fractional baud rate divider.
122  //
123  ui32Div = (((ui32UARTClk * 8) / ui32Baud) + 1) / 2;
124 
125  //
126  // Set the baud rate.
127  //
128  HWREG(ui32Base + UART_O_IBRD) = ui32Div / 64;
129  HWREG(ui32Base + UART_O_FBRD) = ui32Div % 64;
130 
131  //
132  // Set parity, data length, and number of stop bits.
133  //
134  HWREG(ui32Base + UART_O_LCRH) = ui32Config;
135 }
136 
137 //*****************************************************************************
138 //
140 //
141 //*****************************************************************************
142 void
143 UARTConfigGetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk,
144  uint32_t *pui32Baud, uint32_t *pui32Config)
145 {
146  uint32_t ui32Int, ui32Frac;
147 
148  //
149  // Check the arguments.
150  //
151  ASSERT(UARTBaseValid(ui32Base));
152 
153  //
154  // Compute the baud rate.
155  //
156  ui32Int = HWREG(ui32Base + UART_O_IBRD);
157  ui32Frac = HWREG(ui32Base + UART_O_FBRD);
158  *pui32Baud = (ui32UARTClk * 4) / ((64 * ui32Int) + ui32Frac);
159 
160  //
161  // Get the parity, data length, and number of stop bits.
162  //
163  *pui32Config = (HWREG(ui32Base + UART_O_LCRH) &
166 }
167 
168 //*****************************************************************************
169 //
171 //
172 //*****************************************************************************
173 void
174 UARTDisable(uint32_t ui32Base)
175 {
176 
177  //
178  // Check the arguments.
179  //
180  ASSERT(UARTBaseValid(ui32Base));
181 
182  //
183  // Wait for end of TX.
184  //
185  while(HWREG(ui32Base + UART_O_FR) & UART_FR_BUSY)
186  {
187  }
188 
189  //
190  // Disable the FIFO.
191  //
192  HWREG(ui32Base + UART_O_LCRH) &= ~(UART_LCRH_FEN);
193 
194  //
195  // Disable the UART.
196  //
197  HWREG(ui32Base + UART_O_CTL) &= ~(UART_CTL_UARTEN | UART_CTL_TXE |
198  UART_CTL_RXE);
199 }
200 
201 //*****************************************************************************
202 //
204 //
205 //*****************************************************************************
206 int32_t
207 UARTCharGetNonBlocking(uint32_t ui32Base)
208 {
209  //
210  // Check the arguments.
211  //
212  ASSERT(UARTBaseValid(ui32Base));
213 
214  //
215  // See if there are any characters in the receive FIFO.
216  //
217  if(!(HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE))
218  {
219  //
220  // Read and return the next character.
221  //
222  return(HWREG(ui32Base + UART_O_DR));
223  }
224  else
225  {
226  //
227  // There are no characters, so return a failure.
228  //
229  return(-1);
230  }
231 }
232 
233 //*****************************************************************************
234 //
236 //
237 //*****************************************************************************
238 int32_t
239 UARTCharGet(uint32_t ui32Base)
240 {
241  //
242  // Check the arguments.
243  //
244  ASSERT(UARTBaseValid(ui32Base));
245 
246  //
247  // Wait until a char is available.
248  //
249  while(HWREG(ui32Base + UART_O_FR) & UART_FR_RXFE)
250  {
251  }
252 
253  //
254  // Now get the character.
255  //
256  return(HWREG(ui32Base + UART_O_DR));
257 }
258 
259 //*****************************************************************************
260 //
262 //
263 //*****************************************************************************
264 bool
265 UARTCharPutNonBlocking(uint32_t ui32Base, uint8_t ui8Data)
266 {
267  //
268  // Check the arguments.
269  //
270  ASSERT(UARTBaseValid(ui32Base));
271 
272  //
273  // See if there is space in the transmit FIFO.
274  //
275  if(!(HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF))
276  {
277  //
278  // Write this character to the transmit FIFO.
279  //
280  HWREG(ui32Base + UART_O_DR) = ui8Data;
281 
282  //
283  // Success.
284  //
285  return(true);
286  }
287  else
288  {
289  //
290  // There is no space in the transmit FIFO, so return a failure.
291  //
292  return(false);
293  }
294 }
295 
296 //*****************************************************************************
297 //
299 //
300 //*****************************************************************************
301 void
302 UARTCharPut(uint32_t ui32Base, uint8_t ui8Data)
303 {
304  //
305  // Check the arguments.
306  //
307  ASSERT(UARTBaseValid(ui32Base));
308 
309  //
310  // Wait until space is available.
311  //
312  while(HWREG(ui32Base + UART_O_FR) & UART_FR_TXFF)
313  {
314  }
315 
316  //
317  // Send the char.
318  //
319  HWREG(ui32Base + UART_O_DR) = ui8Data;
320 }
321 
322 //*****************************************************************************
323 //
325 //
326 //*****************************************************************************
327 void
328 UARTIntRegister(uint32_t ui32Base, void (*pfnHandler)(void))
329 {
330  //
331  // Check the arguments.
332  //
333  ASSERT(UARTBaseValid(ui32Base));
334 
335  //
336  // Register the interrupt handler.
337  //
338  IntRegister(INT_UART0_COMB, pfnHandler);
339 
340  //
341  // Enable the UART interrupt.
342  //
343  IntEnable(INT_UART0_COMB);
344 }
345 
346 //*****************************************************************************
347 //
349 //
350 //*****************************************************************************
351 void
352 UARTIntUnregister(uint32_t ui32Base)
353 {
354  //
355  // Check the arguments.
356  //
357  ASSERT(UARTBaseValid(ui32Base));
358 
359  //
360  // Disable the interrupt.
361  //
362  IntDisable(INT_UART0_COMB);
363 
364  //
365  // Unregister the interrupt handler.
366  //
367  IntUnregister(INT_UART0_COMB);
368 }
void UARTCharPut(uint32_t ui32Base, uint8_t ui8Data)
Waits to send a character from the specified port.
Definition: uart.c:302
void UARTConfigSetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config)
Sets the configuration of a UART.
Definition: uart.c:104
void UARTIntRegister(uint32_t ui32Base, void(*pfnHandler)(void))
Registers an interrupt handler for a UART interrupt.
Definition: uart.c:328
void UARTDisable(uint32_t ui32Base)
Disables transmitting and receiving.
Definition: uart.c:174
int32_t UARTCharGetNonBlocking(uint32_t ui32Base)
Receives a character from the specified port.
Definition: uart.c:207
#define ASSERT(expr)
Definition: debug.h:74
void UARTConfigGetExpClk(uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config)
Gets the current configuration of a UART.
Definition: uart.c:143
int32_t UARTCharGet(uint32_t ui32Base)
Waits for a character from the specified port.
Definition: uart.c:239
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:200
bool UARTCharPutNonBlocking(uint32_t ui32Base, uint8_t ui8Data)
Sends a character to the specified port.
Definition: uart.c:265
void UARTFIFOLevelGet(uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel)
Gets the FIFO level at which interrupts are generated.
Definition: uart.c:76
void UARTIntUnregister(uint32_t ui32Base)
Unregisters an interrupt handler for a UART interrupt.
Definition: uart.c:352
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:378
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:152
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:318