CC26xx Driver Library
i2c.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: i2c.c
3 * Revised: 2015-11-16 19:41:47 +0100 (Mon, 16 Nov 2015)
4 * Revision: 45094
5 *
6 * Description: Driver for the I2C module
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/i2c.h>
40 
41 //*****************************************************************************
42 //
43 // Handle support for DriverLib in ROM:
44 // This section will undo prototype renaming made in the header file
45 //
46 //*****************************************************************************
47 #if !defined(DOXYGEN)
48  #undef I2CMasterInitExpClk
49  #define I2CMasterInitExpClk NOROM_I2CMasterInitExpClk
50  #undef I2CMasterErr
51  #define I2CMasterErr NOROM_I2CMasterErr
52  #undef I2CIntRegister
53  #define I2CIntRegister NOROM_I2CIntRegister
54  #undef I2CIntUnregister
55  #define I2CIntUnregister NOROM_I2CIntUnregister
56 #endif
57 
58 //*****************************************************************************
59 //
61 //
62 //*****************************************************************************
63 void
64 I2CMasterInitExpClk(uint32_t ui32Base, uint32_t ui32I2CClk,
65  bool bFast)
66 {
67  uint32_t ui32SCLFreq;
68  uint32_t ui32TPR;
69 
70  //
71  // Check the arguments.
72  //
73  ASSERT(I2CBaseValid(ui32Base));
74 
75  //
76  // Must enable the device before doing anything else.
77  //
79 
80  //
81  // Get the desired SCL speed.
82  //
83  if(bFast == true)
84  {
85  ui32SCLFreq = 400000;
86  }
87  else
88  {
89  ui32SCLFreq = 100000;
90  }
91 
92  //
93  // Compute the clock divider that achieves the fastest speed less than or
94  // equal to the desired speed. The numerator is biased to favor a larger
95  // clock divider so that the resulting clock is always less than or equal
96  // to the desired clock, never greater.
97  //
98  ui32TPR = ((ui32I2CClk + (2 * 10 * ui32SCLFreq) - 1) / (2 * 10 * ui32SCLFreq)) - 1;
99  HWREG(I2C0_BASE + I2C_O_MTPR) = ui32TPR;
100 }
101 
102 //*****************************************************************************
103 //
105 //
106 //*****************************************************************************
107 uint32_t
108 I2CMasterErr(uint32_t ui32Base)
109 {
110  uint32_t ui32Err;
111 
112  //
113  // Check the arguments.
114  //
115  ASSERT(I2CBaseValid(ui32Base));
116 
117  //
118  // Get the raw error state.
119  //
120  ui32Err = HWREG(I2C0_BASE + I2C_O_MSTAT);
121 
122  //
123  // If the I2C master is busy, then all the other status bits are invalid,
124  // and there is no error to report.
125  //
126  if(ui32Err & I2C_MSTAT_BUSY)
127  {
128  return(I2C_MASTER_ERR_NONE);
129  }
130 
131  //
132  // Check for errors.
133  //
134  if(ui32Err & (I2C_MSTAT_ERR | I2C_MSTAT_ARBLST))
135  {
137  }
138  else
139  {
140  return(I2C_MASTER_ERR_NONE);
141  }
142 }
143 
144 //*****************************************************************************
145 //
147 //
148 //*****************************************************************************
149 void
150 I2CIntRegister(uint32_t ui32Base, void (*pfnHandler)(void))
151 {
152  uint32_t ui32Int;
153 
154  //
155  // Check the arguments.
156  //
157  ASSERT(I2CBaseValid(ui32Base));
158 
159  //
160  // Get the interrupt number.
161  //
162  ui32Int = INT_I2C_IRQ;
163 
164  //
165  // Register the interrupt handler, returning an error if an error occurs.
166  //
167  IntRegister(ui32Int, pfnHandler);
168 
169  //
170  // Enable the I2C interrupt.
171  //
172  IntEnable(ui32Int);
173 }
174 
175 //*****************************************************************************
176 //
178 //
179 //*****************************************************************************
180 void
181 I2CIntUnregister(uint32_t ui32Base)
182 {
183  uint32_t ui32Int;
184 
185  //
186  // Check the arguments.
187  //
188  ASSERT(I2CBaseValid(ui32Base));
189 
190  //
191  // Get the interrupt number.
192  //
193  ui32Int = INT_I2C_IRQ;
194 
195  //
196  // Disable the interrupt.
197  //
198  IntDisable(ui32Int);
199 
200  //
201  // Unregister the interrupt handler.
202  //
203  IntUnregister(ui32Int);
204 }
static void I2CMasterEnable(uint32_t ui32Base)
Enables the I2C Master block.
Definition: i2c.h:300
#define I2C_MASTER_ERR_NONE
Definition: i2c.h:124
void I2CMasterInitExpClk(uint32_t ui32Base, uint32_t ui32I2CClk, bool bFast)
Initializes the I2C Master block.
Definition: i2c.c:64
#define ASSERT(expr)
Definition: debug.h:74
uint32_t I2CMasterErr(uint32_t ui32Base)
Gets the error status of the I2C Master module.
Definition: i2c.c:108
void IntUnregister(uint32_t ui32Interrupt)
Unregisters the function to be called when an interrupt occurs.
Definition: interrupt.c:200
void I2CIntRegister(uint32_t ui32Base, void(*pfnHandler)(void))
Registers an interrupt handler for the I2C module.
Definition: i2c.c:150
void IntDisable(uint32_t ui32Interrupt)
Disables an interrupt.
Definition: interrupt.c:378
void IntRegister(uint32_t ui32Interrupt, void(*pfnHandler)(void))
Registers a function to be called when an interrupt occurs.
Definition: interrupt.c:152
void I2CIntUnregister(uint32_t ui32Base)
Unregisters an interrupt handler for the I2C module.
Definition: i2c.c:181
void IntEnable(uint32_t ui32Interrupt)
Enables an interrupt.
Definition: interrupt.c:318