CC26xx Driver Library
event.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_event.h>
#include <driverlib/debug.h>

Go to the source code of this file.

Functions

static void EventRegister (uint32_t ui32EventSubscriber, uint32_t ui32EventSource)
 Connects an event to an event subscriber via Event Fabric. More...
 
static void EventSwEventSet (uint32_t ui32SwEvent)
 Sets software event. More...
 
static void EventSwEventClear (uint32_t ui32SwEvent)
 Clears software event. More...
 
static uint32_t EventSwEventGet (uint32_t ui32SwEvent)
 Gets software event status. More...