CC13xx Driver Library
rfc_carrierSense_s Struct Reference

#include <rf_prop_cmd.h>

Data Fields

struct {
   uint8_t   bEnaRssi:1
 If 1, enable RSSI as a criterion. More...
 
   uint8_t   bEnaCorr:1
 If 1, enable correlation as a criterion. More...
 
   uint8_t   operation:1
 0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy More...
 
   uint8_t   busyOp:1
 0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle More...
 
   uint8_t   idleOp:1
 0: Continue on channel Idle
1: End on channel Idle More...
 
   uint8_t   timeoutRes:1
 0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle More...
 
csConf
 
int8_t rssiThr
 RSSI threshold. More...
 
uint8_t numRssiIdle
 Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle. More...
 
uint8_t numRssiBusy
 Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy. More...
 
uint16_t corrPeriod
 Number of RAT ticks for a correlation observation periods. More...
 
struct {
   uint8_t   numCorrInv:4
 Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid. More...
 
   uint8_t   numCorrBusy:4
 Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy. More...
 
corrConfig
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
csEndTrigger
 Trigger classifier for ending the carrier sense. More...
 
ratmr_t csEndTime
 Time used together with csEndTrigger for ending the operation. More...
 

Detailed Description

Definition at line 77 of file rf_prop_cmd.h.

Field Documentation

uint8_t rfc_carrierSense_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 105 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::bEnaCorr

If 1, enable correlation as a criterion.

Definition at line 80 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::bEnaRssi

If 1, enable RSSI as a criterion.

Definition at line 79 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::busyOp

0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle

Definition at line 83 of file rf_prop_cmd.h.

struct { ... } rfc_carrierSense_s::corrConfig
uint16_t rfc_carrierSense_s::corrPeriod

Number of RAT ticks for a correlation observation periods.

Definition at line 96 of file rf_prop_cmd.h.

struct { ... } rfc_carrierSense_s::csConf
ratmr_t rfc_carrierSense_s::csEndTime

Time used together with csEndTrigger for ending the operation.

Definition at line 111 of file rf_prop_cmd.h.

struct { ... } rfc_carrierSense_s::csEndTrigger

Trigger classifier for ending the carrier sense.

uint8_t rfc_carrierSense_s::idleOp

0: Continue on channel Idle
1: End on channel Idle

Definition at line 86 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::numCorrBusy

Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy.

Definition at line 100 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::numCorrInv

Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid.

Definition at line 98 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::numRssiBusy

Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy.

Definition at line 94 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::numRssiIdle

Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle.

Definition at line 92 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::operation

0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy

Definition at line 81 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 108 of file rf_prop_cmd.h.

int8_t rfc_carrierSense_s::rssiThr

RSSI threshold.

Definition at line 91 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::timeoutRes

0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle

Definition at line 88 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 107 of file rf_prop_cmd.h.

uint8_t rfc_carrierSense_s::triggerType

The type of trigger.

Definition at line 104 of file rf_prop_cmd.h.