CC13xx Driver Library
rfc_CMD_PROP_RX_SNIFF_s Struct Reference

Proprietary Mode Receive Command with Sniff Mode. More...

#include <rf_prop_cmd.h>

Data Fields

uint16_t commandNo
 Proprietary Mode Receive Command The command ID number 0x3808. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
struct {
   uint8_t   bFsOff:1
 0: Keep frequency synth on after command
1: Turn frequency synth off after command More...
 
   uint8_t   bRepeatOk:1
 0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly More...
 
   uint8_t   bRepeatNok:1
 0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error More...
 
   uint8_t   bUseCrc:1
 0: Do not check CRC
1: Check CRC More...
 
   uint8_t   bVarLen:1
 0: Fixed length
1: Receive length as first byte More...
 
   uint8_t   bChkAddress:1
 0: No address check
1: Check address More...
 
   uint8_t   endType:1
 0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens More...
 
   uint8_t   filterOp:1
 0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch More...
 
pktConf
 
struct {
   uint8_t   bAutoFlushIgnored:1
 If 1, automatically discard ignored packets from RX queue. More...
 
   uint8_t   bAutoFlushCrcErr:1
 If 1, automatically discard packets with CRC error from RX queue. More...
 
   uint8_t   __pad0__:1
 
   uint8_t   bIncludeHdr:1
 If 1, include the received header or length byte in the stored packet; otherwise discard it. More...
 
   uint8_t   bIncludeCrc:1
 If 1, include the received CRC field in the stored packet; otherwise discard it. More...
 
   uint8_t   bAppendRssi:1
 If 1, append an RSSI byte to the packet in the RX queue. More...
 
   uint8_t   bAppendTimestamp:1
 If 1, append a timestamp to the packet in the RX queue. More...
 
   uint8_t   bAppendStatus:1
 If 1, append a status byte to the packet in the RX queue. More...
 
rxConf
 RX configuration. More...
 
uint32_t syncWord
 Sync word to listen for. More...
 
uint8_t maxPktLen
 Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length. More...
 
uint8_t address0
 Address. More...
 
uint8_t address1
 Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
endTrigger
 Trigger classifier for ending the operation. More...
 
ratmr_t endTime
 Time used together with endTrigger for ending the operation. More...
 
dataQueue_tpQueue
 Pointer to receive queue. More...
 
uint8_t * pOutput
 Pointer to output structure. More...
 
struct {
   uint8_t   bEnaRssi:1
 If 1, enable RSSI as a criterion. More...
 
   uint8_t   bEnaCorr:1
 If 1, enable correlation as a criterion. More...
 
   uint8_t   operation:1
 0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy More...
 
   uint8_t   busyOp:1
 0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle More...
 
   uint8_t   idleOp:1
 0: Continue on channel Idle
1: End on channel Idle More...
 
   uint8_t   timeoutRes:1
 0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle More...
 
csConf
 
int8_t rssiThr
 RSSI threshold. More...
 
uint8_t numRssiIdle
 Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle. More...
 
uint8_t numRssiBusy
 Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy. More...
 
uint16_t corrPeriod
 Number of RAT ticks for a correlation observation periods. More...
 
struct {
   uint8_t   numCorrInv:4
 Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid. More...
 
   uint8_t   numCorrBusy:4
 Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy. More...
 
corrConfig
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
csEndTrigger
 Trigger classifier for ending the carrier sense. More...
 
ratmr_t csEndTime
 Time used together with csEndTrigger for ending the operation. More...
 

Detailed Description

Proprietary Mode Receive Command with Sniff Mode.

Definition at line 636 of file rf_prop_cmd.h.

Field Documentation

uint8_t rfc_CMD_PROP_RX_SNIFF_s::__pad0__

Definition at line 677 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::address0

Address.

Definition at line 687 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::address1

Address (set equal to address0 to accept only one address. If 0xFF, accept 0x00 as well)

Definition at line 688 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendRssi

If 1, append an RSSI byte to the packet in the RX queue.

Definition at line 680 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendStatus

If 1, append a status byte to the packet in the RX queue.

Definition at line 682 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAppendTimestamp

If 1, append a timestamp to the packet in the RX queue.

Definition at line 681 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAutoFlushCrcErr

If 1, automatically discard packets with CRC error from RX queue.

Definition at line 676 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bAutoFlushIgnored

If 1, automatically discard ignored packets from RX queue.

Definition at line 675 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bChkAddress

0: No address check
1: Check address

Definition at line 667 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 646 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaCorr

If 1, enable correlation as a criterion.

Definition at line 703 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bEnaRssi

If 1, enable RSSI as a criterion.

Definition at line 702 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bFsOff

0: Keep frequency synth on after command
1: Turn frequency synth off after command

Definition at line 657 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bIncludeCrc

If 1, include the received CRC field in the stored packet; otherwise discard it.

Definition at line 679 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bIncludeHdr

If 1, include the received header or length byte in the stored packet; otherwise discard it.

Definition at line 678 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bRepeatNok

0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error

Definition at line 661 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bRepeatOk

0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly

Definition at line 659 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bUseCrc

0: Do not check CRC
1: Check CRC

Definition at line 663 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::busyOp

0: Continue carrier sense on channel Busy
1: End carrier sense on channel Busy
For an RX command, the receiver will continue when carrier sense ends, but it will then not end if channel goes Idle

Definition at line 706 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::bVarLen

0: Fixed length
1: Receive length as first byte

Definition at line 665 of file rf_prop_cmd.h.

uint16_t rfc_CMD_PROP_RX_SNIFF_s::commandNo

Proprietary Mode Receive Command The command ID number 0x3808.

Definition at line 637 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::condition
struct { ... } rfc_CMD_PROP_RX_SNIFF_s::corrConfig
uint16_t rfc_CMD_PROP_RX_SNIFF_s::corrPeriod

Number of RAT ticks for a correlation observation periods.

Definition at line 719 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::csConf
ratmr_t rfc_CMD_PROP_RX_SNIFF_s::csEndTime

Time used together with csEndTrigger for ending the operation.

Definition at line 734 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::csEndTrigger

Trigger classifier for ending the carrier sense.

ratmr_t rfc_CMD_PROP_RX_SNIFF_s::endTime

Time used together with endTrigger for ending the operation.

Definition at line 698 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::endTrigger

Trigger classifier for ending the operation.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::endType

0: Packet is received to the end if end trigger happens after sync is obtained
1: Packet reception is stopped if end trigger happens

Definition at line 669 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::filterOp

0: Stop receiver and restart sync search on address mismatch
1: Receive packet and mark it as ignored on address mismatch

Definition at line 671 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::idleOp

0: Continue on channel Idle
1: End on channel Idle

Definition at line 709 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::maxPktLen

Packet length for fixed length, maximum packet length for variable length
0: Unlimited or unknown length.

Definition at line 685 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

Definition at line 654 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::numCorrBusy

Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Invalid to Busy.

Definition at line 723 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::numCorrInv

Number of subsequent correlation tops with maximum corrPeriod RAT ticks between them needed to go from Idle to Invalid.

Definition at line 721 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::numRssiBusy

Number of consecutive RSSI measurements above the threshold needed before the channel is declared Busy.

Definition at line 717 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::numRssiIdle

Number of consecutive RSSI measurements below the threshold needed before the channel is declared Idle.

Definition at line 715 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::operation

0: Busy if either RSSI or correlation indicates Busy
1: Busy if both RSSI and correlation indicates Busy

Definition at line 704 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 649 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::pktConf
rfc_radioOp_t* rfc_CMD_PROP_RX_SNIFF_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 642 of file rf_prop_cmd.h.

uint8_t* rfc_CMD_PROP_RX_SNIFF_s::pOutput

Pointer to output structure.

Definition at line 700 of file rf_prop_cmd.h.

dataQueue_t* rfc_CMD_PROP_RX_SNIFF_s::pQueue

Pointer to receive queue.

Definition at line 699 of file rf_prop_cmd.h.

int8_t rfc_CMD_PROP_RX_SNIFF_s::rssiThr

RSSI threshold.

Definition at line 714 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 653 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::rxConf

RX configuration.

ratmr_t rfc_CMD_PROP_RX_SNIFF_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 643 of file rf_prop_cmd.h.

struct { ... } rfc_CMD_PROP_RX_SNIFF_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_PROP_RX_SNIFF_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 639 of file rf_prop_cmd.h.

uint32_t rfc_CMD_PROP_RX_SNIFF_s::syncWord

Sync word to listen for.

Definition at line 684 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::timeoutRes

0: Timeout with channel state Invalid treated as Busy
1: Timeout with channel state Invalid treated as Idle

Definition at line 711 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 648 of file rf_prop_cmd.h.

uint8_t rfc_CMD_PROP_RX_SNIFF_s::triggerType

The type of trigger.

Definition at line 645 of file rf_prop_cmd.h.