High-Speed Receive Command. More...
#include <rf_hs_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x3842. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More... | |
} | condition |
struct { | |
uint8_t bFsOff:1 | |
0: Keep frequency synth on after command 1: Turn frequency synth off after command More... | |
uint8_t bUseCrc:1 | |
0: Do not receive or check CRC 1: Receive and check CRC More... | |
uint8_t bVarLen:1 | |
0: Fixed length 1: Receive length as first byte More... | |
uint8_t bRepeatOk:1 | |
0: End operation after receiving a packet correctly 1: Go back to sync search after receiving a packet correctly More... | |
uint8_t bRepeatNok:1 | |
0: End operation after receiving a packet with CRC error 1: Go back to sync search after receiving a packet with CRC error More... | |
uint8_t addressMode:2 | |
0: No address check 1: Accept address0 and address1 2: Accept address0 , address1 , and 0x00003: Accept address0 , address1 , 0x0000, and 0xFFFF More... | |
} | pktConf |
struct { | |
uint8_t bAutoFlushCrcErr:1 | |
If 1, automatically remove packets with CRC error from Rx queue. More... | |
uint8_t bIncludeLen:1 | |
If 1, include the received length field in the stored packet; otherwise discard it. More... | |
uint8_t bIncludeCrc:1 | |
If 1, include the received CRC field in the stored packet; otherwise 3scard it. More... | |
uint8_t bAppendStatus:1 | |
If 1, append a status word to the packet in the Rx queue. More... | |
uint8_t bAppendTimestamp:1 | |
If 1, append a timestamp to the packet in the Rx queue. More... | |
} | rxConf |
uint16_t | maxPktLen |
Packet length for fixed length; maximum packet length for variable length. More... | |
uint16_t | address0 |
Address. More... | |
uint16_t | address1 |
Address (set equal to address0 to accept only one address) More... | |
uint8_t | __dummy0 |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | endTrigger |
Trigger classifier for ending the operation. More... | |
ratmr_t | endTime |
Time used together with endTrigger for ending the operation. More... | |
dataQueue_t * | pQueue |
Pointer to receive queue. More... | |
rfc_hsRxOutput_t * | pOutput |
Pointer to output structure. More... | |
High-Speed Receive Command.
Definition at line 108 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::__dummy0 |
Definition at line 153 of file rf_hs_cmd.h.
uint16_t rfc_CMD_HS_RX_s::address0 |
Address.
Definition at line 151 of file rf_hs_cmd.h.
uint16_t rfc_CMD_HS_RX_s::address1 |
Address (set equal to address0
to accept only one address)
Definition at line 152 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::addressMode |
0: No address check
1: Accept address0
and address1
2: Accept address0
, address1
, and 0x0000
3: Accept address0
, address1
, 0x0000, and 0xFFFF
Definition at line 138 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bAppendStatus |
If 1, append a status word to the packet in the Rx queue.
Definition at line 147 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bAppendTimestamp |
If 1, append a timestamp to the packet in the Rx queue.
Definition at line 148 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bAutoFlushCrcErr |
If 1, automatically remove packets with CRC error from Rx queue.
Definition at line 144 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 117 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bFsOff |
0: Keep frequency synth on after command
1: Turn frequency synth off after command
Definition at line 128 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bIncludeCrc |
If 1, include the received CRC field in the stored packet; otherwise 3scard it.
Definition at line 146 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bIncludeLen |
If 1, include the received length field in the stored packet; otherwise discard it.
Definition at line 145 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bRepeatNok |
0: End operation after receiving a packet with CRC error
1: Go back to sync search after receiving a packet with CRC error
Definition at line 136 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bRepeatOk |
0: End operation after receiving a packet correctly
1: Go back to sync search after receiving a packet correctly
Definition at line 134 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bUseCrc |
0: Do not receive or check CRC
1: Receive and check CRC
Definition at line 130 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::bVarLen |
0: Fixed length
1: Receive length as first byte
Definition at line 132 of file rf_hs_cmd.h.
uint16_t rfc_CMD_HS_RX_s::commandNo |
The command ID number 0x3842.
Definition at line 109 of file rf_hs_cmd.h.
struct { ... } rfc_CMD_HS_RX_s::condition |
ratmr_t rfc_CMD_HS_RX_s::endTime |
Time used together with endTrigger
for ending the operation.
Definition at line 162 of file rf_hs_cmd.h.
struct { ... } rfc_CMD_HS_RX_s::endTrigger |
Trigger classifier for ending the operation.
uint16_t rfc_CMD_HS_RX_s::maxPktLen |
Packet length for fixed length; maximum packet length for variable length.
Definition at line 150 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::nSkip |
Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...
Definition at line 125 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 120 of file rf_hs_cmd.h.
struct { ... } rfc_CMD_HS_RX_s::pktConf |
rfc_radioOp_t* rfc_CMD_HS_RX_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 113 of file rf_hs_cmd.h.
rfc_hsRxOutput_t* rfc_CMD_HS_RX_s::pOutput |
Pointer to output structure.
Definition at line 164 of file rf_hs_cmd.h.
dataQueue_t* rfc_CMD_HS_RX_s::pQueue |
Pointer to receive queue.
Definition at line 163 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 124 of file rf_hs_cmd.h.
struct { ... } rfc_CMD_HS_RX_s::rxConf |
ratmr_t rfc_CMD_HS_RX_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 114 of file rf_hs_cmd.h.
struct { ... } rfc_CMD_HS_RX_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_HS_RX_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 110 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 119 of file rf_hs_cmd.h.
uint8_t rfc_CMD_HS_RX_s::triggerType |
The type of trigger.
Definition at line 116 of file rf_hs_cmd.h.