CC13xx Driver Library
prcm.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_ints.h>
#include <inc/hw_prcm.h>
#include <inc/hw_nvic.h>
#include <inc/hw_aon_rtc.h>
#include <driverlib/interrupt.h>
#include <driverlib/debug.h>
#include <driverlib/cpu.h>

Go to the source code of this file.

Macros

#define PRCM_RUN_MODE   0x00000001
 
#define PRCM_SLEEP_MODE   0x00000002
 
#define PRCM_DEEP_SLEEP_MODE   0x00000004
 
#define PRCM_CLOCK_DIV_1   PRCM_GPTCLKDIV_RATIO_DIV1
 
#define PRCM_CLOCK_DIV_2   PRCM_GPTCLKDIV_RATIO_DIV2
 
#define PRCM_CLOCK_DIV_4   PRCM_GPTCLKDIV_RATIO_DIV4
 
#define PRCM_CLOCK_DIV_8   PRCM_GPTCLKDIV_RATIO_DIV8
 
#define PRCM_CLOCK_DIV_16   PRCM_GPTCLKDIV_RATIO_DIV16
 
#define PRCM_CLOCK_DIV_32   PRCM_GPTCLKDIV_RATIO_DIV32
 
#define PRCM_CLOCK_DIV_64   PRCM_GPTCLKDIV_RATIO_DIV64
 
#define PRCM_CLOCK_DIV_128   PRCM_GPTCLKDIV_RATIO_DIV128
 
#define PRCM_CLOCK_DIV_256   PRCM_GPTCLKDIV_RATIO_DIV256
 
#define PRCM_DOMAIN_RFCORE   0x00000001
 
#define PRCM_DOMAIN_SERIAL   0x00000002
 
#define PRCM_DOMAIN_PERIPH   0x00000004
 
#define PRCM_DOMAIN_SYSBUS   0x00000008
 
#define PRCM_DOMAIN_VIMS   0x00000010
 
#define PRCM_DOMAIN_CPU   0x00000020
 
#define PRCM_DOMAIN_TIMER   0x00000040
 
#define PRCM_DOMAIN_CLKCTRL   0x00000080
 
#define PRCM_DOMAIN_MCU   0x00000100
 
#define PRCM_DOMAIN_POWER_OFF   0x00000002
 
#define PRCM_DOMAIN_POWER_ON   0x00000001
 
#define PRCM_DOMAIN_POWER_DOWN_READY   0x00000000
 
#define PRCM_WCLK_NEG_EDGE   0x00000008
 
#define PRCM_WCLK_POS_EDGE   0x00000000
 
#define PRCM_WCLK_SINGLE_PHASE   0x00000000
 
#define PRCM_WCLK_DUAL_PHASE   0x00000002
 
#define PRCM_WCLK_USER_DEF   0x00000004
 
#define I2S_SAMPLE_RATE_16K   0x00000001
 
#define I2S_SAMPLE_RATE_24K   0x00000002
 
#define I2S_SAMPLE_RATE_32K   0x00000004
 
#define I2S_SAMPLE_RATE_48K   0x00000008
 
#define PRCM_PERIPH_TIMER0   0x00000000
 
#define PRCM_PERIPH_TIMER1   0x00000001
 
#define PRCM_PERIPH_TIMER2   0x00000002
 
#define PRCM_PERIPH_TIMER3   0x00000003
 
#define PRCM_PERIPH_SSI0   0x00000100
 
#define PRCM_PERIPH_SSI1   0x00000101
 
#define PRCM_PERIPH_UART0   0x00000200
 
#define PRCM_PERIPH_UART1   0x00000201
 
#define PRCM_PERIPH_I2C0   0x00000300
 
#define PRCM_PERIPH_I2C1   0x00000301
 
#define PRCM_PERIPH_CRYPTO   0x00000400
 
#define PRCM_PERIPH_TRNG   0x00000401
 
#define PRCM_PERIPH_UDMA   0x00000408
 
#define PRCM_PERIPH_GPIO   0x00000500
 
#define PRCM_PERIPH_I2S   0x00000600
 

Functions

void PRCMInfClockConfigureSet (uint32_t ui32ClkDiv, uint32_t ui32PowerMode)
 Configure the infrastructure clock. More...
 
uint32_t PRCMInfClockConfigureGet (uint32_t ui32PowerMode)
 Use this function to get the infrastructure clock configuration. More...
 
static void PRCMMcuPowerOff (void)
 Request a power off of the MCU voltage domain. More...
 
static void PRCMMcuPowerOffCancel (void)
 Cancel a request for a power off of the MCU voltage domain. More...
 
static void PRCMMcuUldoConfigure (uint32_t ui32Enable)
 Assert or de-assert a request for the uLDO. More...
 
static void PRCMGPTimerClockDivisionSet (uint32_t clkDiv)
 Setup the clock division factor for the GP-Timer domain. More...
 
static uint32_t PRCMGPTimerClockDivisionGet (void)
 Get the clock division factor for the GP-Timer domain. More...
 
static void PRCMAudioClockEnable (void)
 Enable the audio clock generation. More...
 
static void PRCMAudioClockDisable (void)
 Disable the audio clock generation. More...
 
void PRCMAudioClockConfigSet (uint32_t ui32ClkConfig, uint32_t ui32SampleRate)
 Configure the audio clock generation. More...
 
void PRCMAudioClockConfigSetOverride (uint32_t ui32ClkConfig, uint32_t ui32MstDiv, uint32_t ui32BitDiv, uint32_t ui32WordDiv)
 Configure the audio clock generation with manual setting of clock divider. More...
 
static void PRCMLoadSet (void)
 Use this function to synchronize the load settings. More...
 
static bool PRCMLoadGet (void)
 Check if any of the load sensitive register has been updated. More...
 
static void PRCMDomainEnable (uint32_t ui32Domains)
 Enable clock domains in the MCU voltage domain. More...
 
static void PRCMDomainDisable (uint32_t ui32Domains)
 Disable clock domains in the MCU voltage domain. More...
 
void PRCMPowerDomainOn (uint32_t ui32Domains)
 Turn power on in power domains in the MCU domain. More...
 
void PRCMPowerDomainOff (uint32_t ui32Domains)
 Turn off a specific power domain. More...
 
static void PRCMRfPowerDownWhenIdle (void)
 Configure RF core to power down when idle. More...
 
void PRCMPeripheralRunEnable (uint32_t ui32Peripheral)
 Enables a peripheral in Run mode. More...
 
void PRCMPeripheralRunDisable (uint32_t ui32Peripheral)
 Disables a peripheral in Run mode. More...
 
void PRCMPeripheralSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in sleep mode. More...
 
void PRCMPeripheralSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in sleep mode. More...
 
void PRCMPeripheralDeepSleepEnable (uint32_t ui32Peripheral)
 Enables a peripheral in deep-sleep mode. More...
 
void PRCMPeripheralDeepSleepDisable (uint32_t ui32Peripheral)
 Disables a peripheral in deep-sleep mode. More...
 
uint32_t PRCMPowerDomainStatus (uint32_t ui32Domains)
 Get the status for a specific power domain. More...
 
static bool PRCMRfReady (void)
 Return the access status of the RF Core. More...
 
static void PRCMSleep (void)
 Put the processor into sleep mode. More...
 
void PRCMDeepSleep (void)
 Put the processor into deep-sleep mode. More...
 
static void PRCMCacheRetentionEnable (void)
 Enable CACHE RAM retention. More...
 
static void PRCMCacheRetentionDisable (void)
 Disable CACHE RAM retention. More...