#include <stdint.h>
#include <stdbool.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_fcfg1.h>
Go to the source code of this file.
Enumerations | |
enum | ProtocolBitVector_t { PROTOCOL_Unknown = 0, PROTOCOLBIT_BLE = 0x02, PROTOCOLBIT_IEEE_802_15_4 = 0x04, PROTOCOLBIT_Proprietary = 0x08 } |
Enumeration identifying the protocols supported. More... | |
enum | PackageType_t { PACKAGE_Unknown = -1, PACKAGE_4x4 = 0, PACKAGE_5x5 = 1, PACKAGE_7x7 = 2, PACKAGE_WAFER = 3, PACKAGE_WCSP = 4 } |
Package type enumeration. More... | |
enum | ChipType_t { CHIP_TYPE_Unknown = -1, CHIP_TYPE_CC1310 = 0, CHIP_TYPE_CC1350 = 1, CHIP_TYPE_CC2620 = 2, CHIP_TYPE_CC2630 = 3, CHIP_TYPE_CC2640 = 4, CHIP_TYPE_CC2650 = 5, CHIP_TYPE_CUSTOM_0 = 6, CHIP_TYPE_CUSTOM_1 = 7 } |
Chip type enumeration. More... | |
enum | ChipFamily_t { FAMILY_Unknown = -1, FAMILY_CC26xx = 0, FAMILY_CC13xx = 1, FAMILY_CC26xx_Liz = 2, FAMILY_CC26xx_Aga = 3, FAMILY_CC26xx_R2 = 4 } |
Chip family enumeration. More... | |
enum | HwRevision_t { HWREV_Unknown = -1, HWREV_1_0 = 10, HWREV_2_0 = 20, HWREV_2_1 = 21, HWREV_2_2 = 22, HWREV_2_3 = 23 } |
HW revision enumeration. More... | |
Functions | |
ProtocolBitVector_t | ChipInfo_GetSupportedProtocol_BV (void) |
Returns bit vector showing supported protocols. More... | |
static bool | ChipInfo_SupportsBLE (void) |
Returns true if the chip supports the BLE protocol. More... | |
static bool | ChipInfo_SupportsIEEE_802_15_4 (void) |
Returns true if the chip supports the IEEE 802.15.4 protocol. More... | |
static bool | ChipInfo_SupportsPROPRIETARY (void) |
Returns true if the chip supports propriatary protocols. More... | |
PackageType_t | ChipInfo_GetPackageType (void) |
Returns package type. More... | |
static bool | ChipInfo_PackageTypeIs4x4 (void) |
Returns true if this is a 4x4mm chip. More... | |
static bool | ChipInfo_PackageTypeIs5x5 (void) |
Returns true if this is a 5x5mm chip. More... | |
static bool | ChipInfo_PackageTypeIs7x7 (void) |
Returns true if this is a 7x7mm chip. More... | |
static bool | ChipInfo_PackageTypeIsWAFER (void) |
Returns true if this is a wafer sale chip (naked die). More... | |
static bool | ChipInfo_PackageTypeIsWCSP (void) |
Returns true if this is a WCSP chip (flip chip). More... | |
static uint32_t | ChipInfo_GetDeviceIdHwRevCode (void) |
Returns the internal chip HW revision code. More... | |
static uint32_t | ChipInfo_GetMinorHwRev (void) |
Returns minor hardware revision number. More... | |
static uint32_t | ChipInfo_GetUserId (void) |
Returns the 32 bits USER_ID field. More... | |
ChipType_t | ChipInfo_GetChipType (void) |
Returns chip type. More... | |
ChipFamily_t | ChipInfo_GetChipFamily (void) |
Returns chip family member. More... | |
static bool | ChipInfo_ChipFamilyIsCC26xx (void) |
Returns true if this chip is member of the CC26xx family. More... | |
static bool | ChipInfo_ChipFamilyIsCC13xx (void) |
Returns true if this chip is member of the CC13xx family. More... | |
static bool | ChipInfo_ChipFamilyIsCC26xx_R2 (void) |
Returns true if this chip is member of the CC26xx_R2 family. More... | |
static bool | ChipInfo_ChipFamilyIsCC26xx_Liz (void) |
Returns true if this chip is member of the CC26xx_Liz family. More... | |
static bool | ChipInfo_ChipFamilyIsCC26xx_Aga (void) |
Returns true if this chip is member of the CC26xx_Aga family. More... | |
HwRevision_t | ChipInfo_GetHwRevision (void) |
Returns chip HW revision. More... | |
static bool | ChipInfo_HwRevisionIs_1_0 (void) |
Returns true if HW revision for this chip is 1.0. More... | |
static bool | ChipInfo_HwRevisionIs_2_0 (void) |
Returns true if HW revision for this chip is 2.0. More... | |
static bool | ChipInfo_HwRevisionIs_GTEQ_2_0 (void) |
Returns true if HW revision for this chip is 2.0 or greater. More... | |
static bool | ChipInfo_HwRevisionIs_2_1 (void) |
Returns true if HW revision for this chip is 2.1. More... | |
static bool | ChipInfo_HwRevisionIs_GTEQ_2_1 (void) |
Returns true if HW revision for this chip is 2.1 or greater. More... | |
static bool | ChipInfo_HwRevisionIs_2_2 (void) |
Returns true if HW revision for this chip is 2.2. More... | |
static bool | ChipInfo_HwRevisionIs_GTEQ_2_2 (void) |
Returns true if HW revision for this chip is 2.2 or greater. More... | |
static bool | ChipInfo_HwRevisionIs_GTEQ_2_3 (void) |
Returns true if HW revision for this chip is 2.3 or greater. More... | |
void | ThisCodeIsBuiltForCC13xxHwRev20AndLater_HaltIfViolated (void) |
Verifies that curent chip is built for CC13xx HwRev 2.0 or later and never returns if violated. More... | |