CC13xx Driver Library
aux_timer.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_ints.h>
#include <inc/hw_memmap.h>
#include <inc/hw_aux_timer.h>
#include <driverlib/debug.h>
#include <driverlib/interrupt.h>

Go to the source code of this file.

Macros

#define AUX_TIMER_CFG_ONE_SHOT   (AUX_TIMER_T0CFG_RELOAD_MAN)
 
#define AUX_TIMER_CFG_PERIODIC   (AUX_TIMER_T0CFG_RELOAD_CONT)
 
#define AUX_TIMER_CFG_ONE_SHOT_EDGE_COUNT   ((AUX_TIMER_T0CFG_RELOAD_MAN) | (AUX_TIMER_T0CFG_MODE_TICK))
 
#define AUX_TIMER_CFG_PERIODIC_EDGE_COUNT   ((AUX_TIMER_T0CFG_RELOAD_CONT) | (AUX_TIMER_T0CFG_MODE_TICK))
 
#define AUX_TIMER_CFG_RISING_EDGE   (AUX_TIMER_T0CFG_TICK_SRC_POL_RISE)
 
#define AUX_TIMER_CFG_FALLING_EDGE   (AUX_TIMER_T0CFG_TICK_SRC_POL_FALL)
 
#define AUX_TIMER_CFG_TICK_SRC_RTC_EVENT   (AUX_TIMER_T0CFG_TICK_SRC_RTC_CH2_EV)
 
#define AUX_TIMER_CFG_TICK_SRC_CMP_A   (AUX_TIMER_T0CFG_TICK_SRC_AUX_COMPA)
 
#define AUX_TIMER_CFG_TICK_SRC_CMP_B   (AUX_TIMER_T0CFG_TICK_SRC_AUX_COMPB)
 
#define AUX_TIMER_CFG_TICK_SRC_TDCDONE   (AUX_TIMER_T0CFG_TICK_SRC_TDC_DONE)
 
#define AUX_TIMER_CFG_TICK_SRC_TIMER0_EVENT   (AUX_TIMER_T1CFG_TICK_SRC_TIMER0_EV)
 
#define AUX_TIMER_CFG_TICK_SRC_TIMER1_EVENT   (AUX_TIMER_T0CFG_TICK_SRC_TIMER1_EV)
 
#define AUX_TIMER_CFG_TICK_SRC_SMPH_RELEASE   (AUX_TIMER_T0CFG_TICK_SRC_SMPH_AUTOTAKE_DONE)
 
#define AUX_TIMER_CFG_TICK_SRC_ADC_DONE   (AUX_TIMER_T0CFG_TICK_SRC_ADC_DONE)
 
#define AUX_TIMER_CFG_TICK_SRC_RTC_4KHZ   (AUX_TIMER_T0CFG_TICK_SRC_RTC_4KHZ)
 
#define AUX_TIMER_CFG_TICK_SRC_OBSMUX0   (AUX_TIMER_T0CFG_TICK_SRC_OBSMUX0)
 
#define AUX_TIMER_CFG_TICK_SRC_OBSMUX1   (AUX_TIMER_T0CFG_TICK_SRC_OBSMUX1)
 
#define AUX_TIMER_CFG_TICK_SRC_AON_SW   (AUX_TIMER_T0CFG_TICK_SRC_AON_SW)
 
#define AUX_TIMER_CFG_TICK_SRC_AON_PROG_WU   (AUX_TIMER_T0CFG_TICK_SRC_AON_PROG_WU)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO0   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO0)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO1   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO1)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO2   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO2)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO3   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO3)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO4   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO4)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO5   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO5)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO6   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO6)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO7   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO7)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO8   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO8)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO9   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO9)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO10   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO10)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO11   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO11)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO12   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO12)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO13   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO13)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO14   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO14)
 
#define AUX_TIMER_CFG_TICK_SRC_AIO15   (AUX_TIMER_T0CFG_TICK_SRC_AUXIO15)
 
#define AUX_TIMER_CFG_TICK_SRC_ACLK_REF   (AUX_TIMER_T0CFG_TICK_SRC_ACLK_REF)
 
#define AUX_TIMER_CFG_TICK_SRC_MCU_EVENT   (AUX_TIMER_T0CFG_TICK_SRC_MCU_EVENT)
 
#define AUX_TIMER_CFG_TICK_SRC_ADC_IRQ   (AUX_TIMER_T0CFG_TICK_SRC_ADC_IRQ)
 
#define AUX_TIMER_0   0x0000FFFF
 
#define AUX_TIMER_1   0x00FF0000
 
#define AUX_TIMER_BOTH   0x00FFFFFF
 
#define AUX_TIMER_PRESCALE_DIV_1   0x00000000
 
#define AUX_TIMER_PRESCALE_DIV_2   0x00000001
 
#define AUX_TIMER_PRESCALE_DIV_4   0x00000002
 
#define AUX_TIMER_PRESCALE_DIV_8   0x00000003
 
#define AUX_TIMER_PRESCALE_DIV_16   0x00000004
 
#define AUX_TIMER_PRESCALE_DIV_32   0x00000005
 
#define AUX_TIMER_PRESCALE_DIV_64   0x00000006
 
#define AUX_TIMER_PRESCALE_DIV_128   0x00000007
 
#define AUX_TIMER_PRESCALE_DIV_256   0x00000008
 
#define AUX_TIMER_PRESCALE_DIV_512   0x00000009
 
#define AUX_TIMER_PRESCALE_DIV_1028   0x0000000A
 
#define AUX_TIMER_PRESCALE_DIV_2048   0x0000000B
 
#define AUX_TIMER_PRESCALE_DIV_4096   0x0000000C
 
#define AUX_TIMER_PRESCALE_DIV_8192   0x0000000D
 
#define AUX_TIMER_PRESCALE_DIV_16384   0x0000000E
 
#define AUX_TIMER_PRESCALE_DIV_32768   0x0000000F
 

Functions

void AUXTimerConfigure (uint32_t ui32Timer, uint32_t ui32Config)
 Configure AUX timer. More...
 
void AUXTimerStart (uint32_t ui32Timer)
 Start AUX timer(s). More...
 
void AUXTimerStop (uint32_t ui32Timer)
 Stop AUX timer(s). More...
 
static void AUXTimerTargetValSet (uint32_t ui32Timer, uint32_t ui32Target)
 Set AUX timer target value. More...
 
static uint32_t AUXTimerTargetValGet (uint32_t ui32Timer)
 Get AUX timer target value. More...
 
void AUXTimerPrescaleSet (uint32_t ui32Timer, uint32_t ui32PrescaleDiv)
 Set AUX timer prescale value. More...
 
uint32_t AUXTimerPrescaleGet (uint32_t ui32Timer)
 Get AUX timer prescale value. More...