CC13xx Driver Library
aon_rtc.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: aon_rtc.c
3 * Revised: 2016-02-29 13:43:37 +0100 (Mon, 29 Feb 2016)
4 * Revision: 45791
5 *
6 * Description: Driver for the AON RTC.
7 *
8 * Copyright (c) 2015 - 2016, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <driverlib/aon_rtc.h>
40 #include <driverlib/cpu.h>
41 
42 //*****************************************************************************
43 //
44 // Handle support for DriverLib in ROM:
45 // This section will undo prototype renaming made in the header file
46 //
47 //*****************************************************************************
48 #if !defined(DOXYGEN)
49  #undef AONRTCCurrentCompareValueGet
50  #define AONRTCCurrentCompareValueGet NOROM_AONRTCCurrentCompareValueGet
51  #undef AONRTCCurrent64BitValueGet
52  #define AONRTCCurrent64BitValueGet NOROM_AONRTCCurrent64BitValueGet
53 #endif
54 
55 
56 //*****************************************************************************
57 //
58 // Get the current value of the RTC counter in a format compatible to the compare registers.
59 //
60 //*****************************************************************************
61 uint32_t
63 {
64  uint32_t ui32CurrentSec ;
65  uint32_t ui32CurrentSubSec ;
66  uint32_t ui32SecondSecRead ;
67 
68  //
69  // Reading SEC both before and after SUBSEC in order to detect if SEC incremented while reading SUBSEC
70  // If SEC incremented, we can't be sure which SEC the SUBSEC belongs to, so repeating the sequence then.
71  //
72  do {
73  ui32CurrentSec = HWREG( AON_RTC_BASE + AON_RTC_O_SEC );
74  ui32CurrentSubSec = HWREG( AON_RTC_BASE + AON_RTC_O_SUBSEC );
75  ui32SecondSecRead = HWREG( AON_RTC_BASE + AON_RTC_O_SEC );
76  } while ( ui32CurrentSec != ui32SecondSecRead );
77 
78  return (( ui32CurrentSec << 16 ) | ( ui32CurrentSubSec >> 16 ));
79 }
80 
81 //*****************************************************************************
82 //
83 // Get the current 64-bit value of the RTC counter.
84 //
85 //*****************************************************************************
86 uint64_t
88 {
89  union {
90  uint64_t returnValue ;
91  uint32_t secAndSubSec[ 2 ] ;
92  } currentRtc ;
93  uint32_t ui32SecondSecRead ;
94 
95  //
96  // Reading SEC both before and after SUBSEC in order to detect if SEC incremented while reading SUBSEC
97  // If SEC incremented, we can't be sure which SEC the SUBSEC belongs to, so repeating the sequence then.
98  //
99  do {
100  currentRtc.secAndSubSec[ 1 ] = HWREG( AON_RTC_BASE + AON_RTC_O_SEC );
101  currentRtc.secAndSubSec[ 0 ] = HWREG( AON_RTC_BASE + AON_RTC_O_SUBSEC );
102  ui32SecondSecRead = HWREG( AON_RTC_BASE + AON_RTC_O_SEC );
103  } while ( currentRtc.secAndSubSec[ 1 ] != ui32SecondSecRead );
104 
105  return ( currentRtc.returnValue );
106 }
uint64_t AONRTCCurrent64BitValueGet(void)
Get the current 64-bit value of the RTC counter.
Definition: aon_rtc.c:87
uint32_t AONRTCCurrentCompareValueGet(void)
Get the current value of the RTC counter in a format that matches RTC compare values.
Definition: aon_rtc.c:62