![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_16_00_08
|
![]() |
Macros | |
#define | Watchdog_STATUS_SUCCESS 0 |
Successful status code returned by Watchdog_control(). More... | |
#define | Watchdog_STATUS_ERROR -1 |
Generic error status code returned by Watchdog_control(). More... | |
#define | Watchdog_STATUS_UNDEFINEDCMD -2 |
An error status code returned by Watchdog_control() for undefined command codes. More... | |
Watchdog_STATUS_* macros are general status codes returned by Watchdog_control()
#define Watchdog_STATUS_SUCCESS 0 |
Successful status code returned by Watchdog_control().
Watchdog_control() returns Watchdog_STATUS_SUCCESS if the control code was executed successfully.
#define Watchdog_STATUS_ERROR -1 |
Generic error status code returned by Watchdog_control().
Watchdog_control() returns Watchdog_STATUS_ERROR if the control code was not executed successfully.
#define Watchdog_STATUS_UNDEFINEDCMD -2 |
An error status code returned by Watchdog_control() for undefined command codes.
Watchdog_control() returns Watchdog_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.