![]() |
![]() |
Defines | |
#define | VICP_VERSION 0x01000000 |
#define | VICP_NUMRESOURCES 6 |
Typedefs | |
typedef enum VICP_Status | VICP_Status |
Status codes for VICP API return values. | |
typedef enum VICP_ResourceType | VICP_ResourceType |
Resource types to be used for all APIs. | |
typedef enum VICP_InterruptLine | VICP_InterruptLine |
Source of VICP resource interrupt. | |
typedef enum VICP_InterruptType | VICP_InterruptType |
Type of ARM interrupt support. | |
Enumerations | |
enum | VICP_Status { VICP_OK = 0, VICP_EFAIL, VICP_ENOCHANNEL, VICP_ENOINIT } |
Status codes for VICP API return values. More... | |
enum | VICP_ResourceType { VICP_IMX0, VICP_IMX1, VICP_MJCP, VICP_NSF, VICP_HDVICP0, VICP_HDVICP1 } |
Resource types to be used for all APIs. More... | |
enum | VICP_InterruptLine { VICP_FIXED, VICP_FLEXIBLE } |
Source of VICP resource interrupt. More... | |
enum | VICP_InterruptType { VICP_IRQ, VICP_FIQ } |
Type of ARM interrupt support. More... | |
Functions | |
int | VICP_init (void) |
VICP initialization API. | |
int | VICP_exit (void) |
VICP finalization API. | |
VICP_Status | VICP_register (VICP_ResourceType resource, VICP_InterruptLine intrLine, VICP_InterruptType intrType) |
Registers resource with requested interrupt type. | |
VICP_Status | VICP_unregister (VICP_ResourceType resource) |
Frees previously requested resource. | |
VICP_Status | VICP_wait (VICP_ResourceType resource) |
Waits for the transfer corresponding to this resource to complete. | |
VICP_Status | VICP_done (VICP_ResourceType resource, int *done) |
Checks if the transfer corresponding to this resource is complete. |
This is the API for the VICP Manager.
#define VICP_VERSION 0x01000000 |
#define VICP_NUMRESOURCES 6 |
typedef enum VICP_Status VICP_Status |
Status codes for VICP API return values.
typedef enum VICP_ResourceType VICP_ResourceType |
Resource types to be used for all APIs.
typedef enum VICP_InterruptLine VICP_InterruptLine |
Source of VICP resource interrupt.
typedef enum VICP_InterruptType VICP_InterruptType |
Type of ARM interrupt support.
enum VICP_Status |
Status codes for VICP API return values.
VICP_OK |
OK |
VICP_EFAIL |
general failure |
VICP_ENOCHANNEL |
no channels available |
VICP_ENOINIT |
VICP_init() not called |
enum VICP_ResourceType |
enum VICP_InterruptLine |
Source of VICP resource interrupt.
enum VICP_InterruptType |
int VICP_init | ( | void | ) |
VICP initialization API.
int VICP_exit | ( | void | ) |
VICP finalization API.
VICP_Status VICP_register | ( | VICP_ResourceType | resource, |
VICP_InterruptLine | intrLine, | ||
VICP_InterruptType | intrType | ||
) |
Registers resource with requested interrupt type.
VICP_Status VICP_unregister | ( | VICP_ResourceType | resource ) |
Frees previously requested resource.
VICP_Status VICP_wait | ( | VICP_ResourceType | resource ) |
Waits for the transfer corresponding to this resource to complete.
VICP_Status VICP_done | ( | VICP_ResourceType | resource, |
int * | done | ||
) |
Checks if the transfer corresponding to this resource is complete.